Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum I am not able to interface JHD162A LCD to any of the PSoC Kits?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 29 subscribers
  • Views 2359 views
  • Users 0 members are here
Related

I am not able to interface JHD162A LCD to any of the PSoC Kits?

gsgill112
gsgill112 over 11 years ago

I have tried the Cypress LCD component as well as a Community component where you can select different pins.

In both the cases I get some junk on display ? I did manage to get the custom component working for a while but now that's also not working.

 

I have been through the LCD component's datasheet like a 1000 times and almost tried all the functions but with no luck ?? Please help !!

 

my main looks like :- >

 

main(){

 

LCD_Start();

LCD_Print_String("Hello");

while(1);

}

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    I think you need to see the low level approach to ensure correct operations. I would checkout this:

    http://www.scribd.com/doc/17686517/JHD162A-LCD-Code

    Especially the Init code with correct delay...

    Your problem is that the display keeps its state during MCU reset. When cold-booting, the initial data mode is 8-bit which you immediately switch to 4-bit which reads data with a pair of EN pulses.

    When you reset the MCU, you do not know whether even or odd number of EN pulses were sent. So you have to somhow reset the display even if it does not have reset pin.

    This can be done by sending 0x33 0x33 (in 8-bit mode it will mean 4-times switch to 8-bit, in 4-bit mode it will mean once or twice switch to 8-bit). Then you can be sure that you always start from the same state.

    Then proceed with regular 0x32 (or 4-bit 0x02 if you have single 4-bit write function), 0x28 to get into 4-bit 2-line mode.

     

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago

    I think you need to see the low level approach to ensure correct operations. I would checkout this:

    http://www.scribd.com/doc/17686517/JHD162A-LCD-Code

    Especially the Init code with correct delay...

    Your problem is that the display keeps its state during MCU reset. When cold-booting, the initial data mode is 8-bit which you immediately switch to 4-bit which reads data with a pair of EN pulses.

    When you reset the MCU, you do not know whether even or odd number of EN pulses were sent. So you have to somhow reset the display even if it does not have reset pin.

    This can be done by sending 0x33 0x33 (in 8-bit mode it will mean 4-times switch to 8-bit, in 4-bit mode it will mean once or twice switch to 8-bit). Then you can be sure that you always start from the same state.

    Then proceed with regular 0x32 (or 4-bit 0x02 if you have single 4-bit write function), 0x28 to get into 4-bit 2-line mode.

     

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 11 years ago in reply to clem57

    @gsgill112

    Are you using this datasheet?

    http://www.itron.com.cn/PDF_file/JHD162A%20SERIES.pdf

     

    Here is someone with same problem and the solution was:

    Unsolved JHD162A LCD Initialization

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gsgill112
    0 gsgill112 over 11 years ago in reply to clem57

    @Clem Martins     The LCD is not the problem, previously I was working with the CharLCd() component in PSoC creator and it pretty much looks like a black box, So I don't know of a way to see the backend code.For the new component I am working I have to incorporate the 0x33 0x33 hack !!Although , I also tried shutting down the power to reset the entire System, as when the LCD boots It doesn't remember the previous stage but that didn't help !!



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gsgill112
    0 gsgill112 over 11 years ago in reply to clem57

    and as far as other platforms are concerned, I have written code for CCS and have also worked with AVR, and have successful results. but I am like very new to PSoC so , Struggling a bit image  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hlipka
    0 hlipka over 11 years ago in reply to gsgill112

    The components are not really a black box. When you have build your project, everything is in 'Generated Code'. Look there in the C file for the LCD component, and you can see what it does.

    When using the CharLCDMP component, make sure you are using the latest version (scroll down on Character LCD (mp) Multi - Port - Cypress ) - the later versions have some bugfixes regarding the timing.