Atmel Xplained Boards
  • Products & Partners
  • Dev Tools
  • Atmel Xplained Boards
  • More
  • Cancel
Atmel Xplained Boards
Forum SAMA5D4 ADC driver - do you know a Linux image that has the driver?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Atmel Xplained Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 6 subscribers
  • Views 3897 views
  • Users 0 members are here
Related

SAMA5D4 ADC driver - do you know a Linux image that has the driver?

Jan Cumps
Jan Cumps over 11 years ago

For the Enchanted Objects Design ChallengeI'm trying to get the ADC Hardware Trigger mechanism working.


I have difficulties with the ADC driver. I am unsure if the 4.7 and 4.6 linux Yocto Poky images have that driver installed.


I have 3 questions :


Is the ADC driver for the sama5d4 included in those Yocto Poky images?

If yes, what's the name of the driver (is it at91_adc)?

If no, is there an image around with the ADC included, or is there a way to get the driver installed on my board running that Yocto Poky image?

 

Here's the blog post that shows what I'm dong: Review 9b: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 2

 

I have issues when the buffer read tool generic_buffer tries to load the driver:

 

Here's where the code fails:

 

    /* Find the device requested */  
    dev_num = find_type_by_name(device_name, "device");  
    if (dev_num < 0) {  
        printf("Failed to find the %s\n", device_name);  
        ret = -ENODEV;  
        goto error_ret;  
    }  
    printf("iio device number being used is %d\n", dev_num); 

 

Error

Failed to find the at91_adc

  • Sign in to reply
  • Cancel

Top Replies

  • noglitch
    noglitch over 11 years ago in reply to Jan Cumps +1 suggested
    Hi, Due to move to DT, the device name has changed. It is now "fc034000.adc" for this device. So, your command line should be: ./generic_buffer -n fc034000.adc -t fc034000.adc-dev0-continuous -l 2 It seems…
  • noglitch
    noglitch over 11 years ago +1 verified
    FYI, I've just updated the Linux4SAM.org page: http://www.at91.com/linux4sam/bin/view/Linux4SAM/IioAdcDriver to reflect the changes in naming brought by a Device Tree system.
  • noglitch
    noglitch over 11 years ago in reply to Jan Cumps +1
    Oh thanks for the typo correction. I use the Linux4SAM 4.7 kernel + rootfs image. I took the generic_buffer.c file in the linux-3.18-at91 kernel and compiled it with a Code Sourcery toolchain (Sourcery…
Parents
  • noglitch
    0 noglitch over 11 years ago

    FYI, I've just updated the Linux4SAM.org page:

    http://www.at91.com/linux4sam/bin/view/Linux4SAM/IioAdcDriver

    to reflect the changes in naming brought by a Device Tree system.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 11 years ago in reply to noglitch

    Hi,

    Is the image that you are using with the successful generic_buffer execution available somewhere in binary format?

     

     

     

    (there's a small typo in the command line , for the devtree and non-devtree explanations: ./generic-buffer -> ./generic_buffer)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • noglitch
    0 noglitch over 11 years ago in reply to Jan Cumps

    Oh thanks for the typo correction.

     

    I use the Linux4SAM 4.7 kernel + rootfs image.

    I took the  generic_buffer.c file in the linux-3.18-at91 kernel and compiled it with a Code Sourcery toolchain (Sourcery CodeBench Lite 2014.05-29).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 11 years ago in reply to noglitch

    Success !!

     

    image

     

    I've uploaded this image:

    ftp://www.at91.com/pub/demo/linux4sam_4.7/linux4sam-poky-sama5d4_xplained-4.7.zip

     

    I did use a different generic_code.c, just downloaded the one from https://github.com/linux4sam/linux-at91/blob/master/drivers/staging/iio/Documentation/generic_buffer.c

    (raw version:https://raw.githubusercontent.com/linux4sam/linux-at91/master/drivers/staging/iio/Documentation/generic_buffer.c)

     

     

    I'm using the GNU toolchain that comes with DS-5 Community Edition

     

    image

     

     

    Invoking: GCC C Linker 4 [arm-linux-gnueabihf]'

    arm-linux-gnueabihf-gcc -static -marm -march=armv7-a -o "generic_buffer"  ./generic_buffer.o  

     

     

     

    Loaded to the board, and this is the result:

     

    root@sama5d4-xplained:~# ./generic_buffer -n fc034000.adc -t fc034000.adc-dev0-continuous -l 2

     

    iio device number being used is 0
    iio trigger number being used is 0
    /sys/bus/iio/devices/iio:device0 fc034000.adc-dev0-continuous
    1017.000000 437.000000 0.000000
    1017.000000 437.000000 119.000000
    1017.000000 437.000000 119.000000
    1017.000000 400.000000 119.000000

    Thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 11 years ago in reply to noglitch

    Success !!

     

    image

     

    I've uploaded this image:

    ftp://www.at91.com/pub/demo/linux4sam_4.7/linux4sam-poky-sama5d4_xplained-4.7.zip

     

    I did use a different generic_code.c, just downloaded the one from https://github.com/linux4sam/linux-at91/blob/master/drivers/staging/iio/Documentation/generic_buffer.c

    (raw version:https://raw.githubusercontent.com/linux4sam/linux-at91/master/drivers/staging/iio/Documentation/generic_buffer.c)

     

     

    I'm using the GNU toolchain that comes with DS-5 Community Edition

     

    image

     

     

    Invoking: GCC C Linker 4 [arm-linux-gnueabihf]'

    arm-linux-gnueabihf-gcc -static -marm -march=armv7-a -o "generic_buffer"  ./generic_buffer.o  

     

     

     

    Loaded to the board, and this is the result:

     

    root@sama5d4-xplained:~# ./generic_buffer -n fc034000.adc -t fc034000.adc-dev0-continuous -l 2

     

    iio device number being used is 0
    iio trigger number being used is 0
    /sys/bus/iio/devices/iio:device0 fc034000.adc-dev0-continuous
    1017.000000 437.000000 0.000000
    1017.000000 437.000000 119.000000
    1017.000000 437.000000 119.000000
    1017.000000 400.000000 119.000000

    Thank you!