Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Single Board Computer and RS232
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 60 subscribers
  • Views 2327 views
  • Users 0 members are here
Related

Single Board Computer and RS232

thecaptain0220
thecaptain0220 over 7 years ago

I am working on a project where I need to receive data from a device using RS232. Right now I am using a Raspberry Pi and an FTDI RS232 to USB cable.

 

https://www.adafruit.com/product/70

 

I would like to find a cheaper alternative and ideally supports RS232 natively. I would like to eliminate the need for the USB adapter. Are there any single board computers with pins that can handle RS232?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 7 years ago +2
    HI Kirk, thecaptain0220 wrote: Right now I am using a Raspberry Pi and an FTDI RS232 to USB cable. The FTDI item you've linked to does not provide RS232, it provides 3.3V or 5V-compilant levels (sometimes…
  • gdstew
    gdstew over 7 years ago +1
    I don't know of any SBCs that directly support RS232 signal levels however there are many small inexpensive RS232 level conversion boards that use a single chip to convert the serial I/O from the SBC pins…
  • thecaptain0220
    thecaptain0220 over 7 years ago in reply to shabaz +1
    I have done some research, but I will admit that I am not an expert on the subject. I am using the cable in the link to receive serial data from the device. I connect the RX, TX, and Ground. The cable…
Parents
  • gdstew
    gdstew over 7 years ago

    I don't know of any SBCs that directly support RS232 signal levels however there are many small inexpensive RS232 level conversion boards

    that use a single chip to convert the serial I/O from the SBC pins to and from RS232 signals on a DB9 connector. They usually require a +3.3V supply

    from the SBC. I have bought several of these boards on Ebay and have used them on Raspberry Pis, Odroid1 and 2, and BeagleBoard Black SBCs

    with no problems. Use a RS232 to TTL search on Ebay to find them and make sure that they support 3.3V I/O levels (most of them do).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gdstew
    gdstew over 7 years ago

    I don't know of any SBCs that directly support RS232 signal levels however there are many small inexpensive RS232 level conversion boards

    that use a single chip to convert the serial I/O from the SBC pins to and from RS232 signals on a DB9 connector. They usually require a +3.3V supply

    from the SBC. I have bought several of these boards on Ebay and have used them on Raspberry Pis, Odroid1 and 2, and BeagleBoard Black SBCs

    with no problems. Use a RS232 to TTL search on Ebay to find them and make sure that they support 3.3V I/O levels (most of them do).