Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Olimex A10S/A20-OLinuXino boards quite BBB-like
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 113 replies
  • Subscribers 64 subscribers
  • Views 16314 views
  • Users 0 members are here
  • olinuxino
  • allwinner
  • bbb
  • olimex
  • a20
  • a10
Related

Olimex A10S/A20-OLinuXino boards quite BBB-like

morgaine
morgaine over 13 years ago

I've gathered together some pieces of information on Olimex's latest Cortex-A* board range, which I think is an interesting one.

 

Allwinner's new A20 device has almost the same pinout as their old A10, so Olimex developed an A20 board very quickly by upgrading an earlier A10-based prototype with the new SoC.  They already had a different OLinuXino board based on the lower-cost A10S in early production, so the future A20 board is being positioned as a more capable version of this product.

 

This pair of boards have the product names A10S-OLinuXino-MICRO and A20-OLinuXino-MICRO, and Olimex's price list shows that each of these will also be available with 4GB of NAND flash on board, respectively named as A10S-OLinuXino-MICRO-4GB and A20-OLinuXino-MICRO-4GB.    Summary of the range:

 

 

SoCCoresARM Core
RAMProduct ModelPriceFeatures
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO45 euro
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO-4GB55 euroFlash
A202Cortex-A71GBA20-OLinuXino-MICRO55 euroSATA
A202Cortex-A71GBA20-OLinuXino-MICRO-4GB65 euroFlash, SATA

 

 

Note that there is more symmetry in the  product naming  than in the actual board layouts, as A10S and A20 boards are quite different to reflect the differences in their SoCs.

 

The NAND-less A10S-OLinuXino-MICRO [summary pdf] is already listed at Farnell UK, delivery projected for end of July, and development work on the A20-OLinuXino-MICRO seems to be progressing well.

 

The A10S-OLinuXino-MICRO-4GB is pretty similar to the BeagleBone Black (BBB) in several ways.  The A10S has a Cortex-A8 CPU just like the BBB's TI AM3359, and both are clocked at the same speed of 1GHz.  Both provide native Ethernet, not over USB.  Both boards offer 512MB of RAM.  Likewise both feature on-board embedded flash as well as sockets for external cards, although the OLinuXino has double the flash and two different card sockets.  Both provide HDMI for video output (the A10S's GPU is a MALI-400), although the OLinuXino also provides analogue audio input and output sockets.  Both provide roughly the same kind of expansion connector concept, ie. a connector on each of the opposing long edges of the board.  As usual on Olimex boards, the OLinuXino also provides a UEXT connector which allows Olimex's large range of expansion modules to be attached.

 

The above isn't intended to portray the A10S-OLinuXino-MICRO-4GB as "better" despite it having several extra features.  The BBB is quite a lot cheaper and provides stackable capes and the AM335x's exceptional PRUs, so it'll always be "horses for courses" between the two.  I do think that the two boards are close enough in features to be considered ballpark-similar.

 

The A20-OLinuXino-MICRO and -4GB version will be quite a significant step up from their A10S-based siblings.  The CPU is a dual-core Cortex-A7 (see the A20 and Allwinner family brief pdf and short A20 datasheet for more details), RAM is doubled to 1GB of DDR3, video output is through both HDMI and VGA, and SATA data and power connectors are provided.  For 55 to 65 Euro, I expect that Olimex are going to have a serious hit on their hands.

 

And the entire OLinuXino range is both open hardware and open software, give or take Allwinner's somewhat lacklustre understanding of the concept of documentation.  TI is way ahead on quality of open documentation for the BBB, except for its GPU which remains closed.  Apparently the open source Lima driver for the OLinuXino's MALI-400 is better than the Allwinner binary blob anyway, so at least for graphics support it might not matter much. image

 

Interesting times ahead.  I'm certainly keeping an eye open on Olimex, they're a very competent and extremely productive outfit.  Progress on their OLinuXino boards and other newsworthy developments are typically announced on their blog.

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 13 years ago in reply to morgaine +2
    That's a good question about the A9. I wonder if there will be or is a Sitara SoC part with that for which a similar low-cost board could be made (BeagleBone Graphene - early 2014? ). I'll see Jason in…
  • morgaine
    morgaine over 13 years ago +1
    The A10S-OLinuXino-MICRO isn't in the exceptionally low Raspberry Pi and BBB price niche, but it may be worth pointing out that this board has Raspberry Pi-like graphics and media capability (unlike the…
  • morgaine
    morgaine over 13 years ago +1
    Olimex has blogged instructions on building Linux for A10S from scratch . Since the A10S has a Cortex-A8 CPU like the BBB, these instructions and the linux-sunxi Github repositories to which they refer…
Parents
  • morgaine
    morgaine over 13 years ago

    It's Allwinner chips with everything at Olimex! image

     

    • Announcement from their blog.
    • Allwinner chips in Olimex shop.

     

    That's a very good idea from Olimex to sell the Allwinner devices directly.

     

    Not only does it support their official position on open hardware by making it easier for people to acquire the necessary components for their own PCBs, but by selling more of the devices, Olimex gains access to more volume from Allwinner and so brings down their own product BOM costs too.  Good plan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    That's a very good idea from Olimex to sell the Allwinner devices directly.

    Interesting, but I wonder how many sales of the BGA devices they'll make. Unlike the RPF, I don't presume that it's impossible for hobbiests to handle BGA's at home, but I do think that the number who will have invested the time and effort will be fairly low. Divide that by the number who will want these particular devices and what's left ?

    The other avenue is if they can supply commercial volume, but it wouldn't be unreasonable to think that anyone buying in commercial volumes will either be able to go direct to Allwinner, or will get their outsourced Chinese subcontract manufacturer to just source them locally.

    So good plan, yes. But I must be missing something for this to be much more than interesting PR.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    Are there places that will just fit a supplied BGA package to a PCB, possibly as part of printing the board?

     

    If so, I can understand enthusiasts in the West being happy to pay Olimex a bit more to avoid liaising with China themselves.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Are there places that will just fit a supplied BGA package to a PCB, possibly as part of printing the board?

    I dare say there are. Most of the places I've looked at in the past fall into two broad categories:

    1. PCB Only
    2. Give us the gerbers & BOM we'll source everything and assemble it for you

     

    So I'm sure there's some middle ground if you can find somewhere willing to deal with very low volume prototype stuff.  I've seen places that will supply a laser cut solderpaste stencil almost for free even when ordering relatively small quantities of PCB's.  It starts to become a question of whether the setup of the paste machine, pick&place machine & reflow oven is worth it for one-off or even 10 off type quantities though.

     

    I do seem to remember reading about some newer solderpaste machines that are more like an inkjet printer, so you can selectively do only what's required.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    From memory, pcbtrain (excellent manufacturer) will put on a one-off single SMD part (e.g. BGA) for £50, so not cheap, but not completely unaffordable either. I've been working on a reflow machine for over a year now! I might finish it one day. Pcbtrain can supply a metal mask, they sent a sample a while back, it looked very nice (it was steel).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    shabaz wrote:

     

    From memory, pcbtrain (excellent manufacturer) will put on a one-off single SMD part (e.g. BGA) for £50, so not cheap, but not completely unaffordable either.

    Yeah, but whatever you're doing would need to be pretty special to bother. Added to the cost of a PCB and an A20 + PMIC from Olimex and you're likely already at least double the cost of a BBB or RPi.  As a way to prove a prototype for a much bigger production run then sure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    Sounds like there's a niche for a self-soldering BGA breakout board, containing an on-board heater and clamp.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Or a socket: http://www.selwyn.co.uk/index.php?option=com_k2&view=itemlist&task=category&id=13:bga-sockets-adapters

     

    I can imagine those sockets are probably bga's themselves and I'd be surprised if they're not insanely expensive, so 50 quid to get a one-off done may not be so bad after all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    A BGA socket that has to provide low-impedance connections purely through precision contact pressure on so many balls is a tall order both mechanically and electrically, so yeah, the price would probably reflect that.

     

    In contrast, a breakout board or header with a built-in heater and solder pads wouldn't need to apply any significant pressure nor electrical contact during the soldering operation, and it would  need to be built only strong enough for alignment during heating.  It's just a gut feeling, but I think that would be a lot cheaper, way below 50 quid.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    It's a good idea. In the past I've imagined a micro reflow oven, which would essentially just be some resistance wire in a very small (maybe 1 inch square) open-box enclosure (with ideally a viewing window too), that you could just temporarily place on top of an area of the PCB (i.e. open side facing down of course), just to solder QFN/BGA packages. But then I suppose it is similar to the handheld hot-air devices (which maybe are less gentle - I've never tried them for soldering).

    A breakout board with built-in copper heating element sounds very cool though! Or, just brainstorming, maybe a sandwich board which has the element or resistance wire, that you clamp against the PCB (maybe screw holes to do the clamping) temporarily.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    shabaz wrote:

     

    But then I suppose it is similar to the handheld hot-air devices (which maybe are less gentle - I've never tried them for soldering).

    I have hot air tools and it's certainly possible to use them for BGA & QFN. Hot air has it's challenges though, especially on a populated board. You have to mask off other components with kapton tape to prevent damage. Or in the case of small resistors and capacitors to prevent them getting blown away as they'll typically heat up much quicker than the bigger bga.

     

    Other than initial reflow soldering, hot air is the way bga's, qfn's and even qfp's will be removed and replaced by the manufacturers. Although they probably will use a jig to hold the board level and hold the hot air tool above the board. Likely the board is heated from below too in order to reduce the thermal stress.

     

    PoP could be rather challenging though and whatever the process there comes a point where it's uneconomical to do it by hand at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    shabaz wrote:

     

    But then I suppose it is similar to the handheld hot-air devices (which maybe are less gentle - I've never tried them for soldering).

    I have hot air tools and it's certainly possible to use them for BGA & QFN. Hot air has it's challenges though, especially on a populated board. You have to mask off other components with kapton tape to prevent damage. Or in the case of small resistors and capacitors to prevent them getting blown away as they'll typically heat up much quicker than the bigger bga.

     

    Other than initial reflow soldering, hot air is the way bga's, qfn's and even qfp's will be removed and replaced by the manufacturers. Although they probably will use a jig to hold the board level and hold the hot air tool above the board. Likely the board is heated from below too in order to reduce the thermal stress.

     

    PoP could be rather challenging though and whatever the process there comes a point where it's uneconomical to do it by hand at all.