Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Olimex A10S/A20-OLinuXino boards quite BBB-like
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 113 replies
  • Subscribers 64 subscribers
  • Views 16225 views
  • Users 0 members are here
  • olinuxino
  • allwinner
  • bbb
  • olimex
  • a20
  • a10
Related

Olimex A10S/A20-OLinuXino boards quite BBB-like

morgaine
morgaine over 13 years ago

I've gathered together some pieces of information on Olimex's latest Cortex-A* board range, which I think is an interesting one.

 

Allwinner's new A20 device has almost the same pinout as their old A10, so Olimex developed an A20 board very quickly by upgrading an earlier A10-based prototype with the new SoC.  They already had a different OLinuXino board based on the lower-cost A10S in early production, so the future A20 board is being positioned as a more capable version of this product.

 

This pair of boards have the product names A10S-OLinuXino-MICRO and A20-OLinuXino-MICRO, and Olimex's price list shows that each of these will also be available with 4GB of NAND flash on board, respectively named as A10S-OLinuXino-MICRO-4GB and A20-OLinuXino-MICRO-4GB.    Summary of the range:

 

 

SoCCoresARM Core
RAMProduct ModelPriceFeatures
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO45 euro
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO-4GB55 euroFlash
A202Cortex-A71GBA20-OLinuXino-MICRO55 euroSATA
A202Cortex-A71GBA20-OLinuXino-MICRO-4GB65 euroFlash, SATA

 

 

Note that there is more symmetry in the  product naming  than in the actual board layouts, as A10S and A20 boards are quite different to reflect the differences in their SoCs.

 

The NAND-less A10S-OLinuXino-MICRO [summary pdf] is already listed at Farnell UK, delivery projected for end of July, and development work on the A20-OLinuXino-MICRO seems to be progressing well.

 

The A10S-OLinuXino-MICRO-4GB is pretty similar to the BeagleBone Black (BBB) in several ways.  The A10S has a Cortex-A8 CPU just like the BBB's TI AM3359, and both are clocked at the same speed of 1GHz.  Both provide native Ethernet, not over USB.  Both boards offer 512MB of RAM.  Likewise both feature on-board embedded flash as well as sockets for external cards, although the OLinuXino has double the flash and two different card sockets.  Both provide HDMI for video output (the A10S's GPU is a MALI-400), although the OLinuXino also provides analogue audio input and output sockets.  Both provide roughly the same kind of expansion connector concept, ie. a connector on each of the opposing long edges of the board.  As usual on Olimex boards, the OLinuXino also provides a UEXT connector which allows Olimex's large range of expansion modules to be attached.

 

The above isn't intended to portray the A10S-OLinuXino-MICRO-4GB as "better" despite it having several extra features.  The BBB is quite a lot cheaper and provides stackable capes and the AM335x's exceptional PRUs, so it'll always be "horses for courses" between the two.  I do think that the two boards are close enough in features to be considered ballpark-similar.

 

The A20-OLinuXino-MICRO and -4GB version will be quite a significant step up from their A10S-based siblings.  The CPU is a dual-core Cortex-A7 (see the A20 and Allwinner family brief pdf and short A20 datasheet for more details), RAM is doubled to 1GB of DDR3, video output is through both HDMI and VGA, and SATA data and power connectors are provided.  For 55 to 65 Euro, I expect that Olimex are going to have a serious hit on their hands.

 

And the entire OLinuXino range is both open hardware and open software, give or take Allwinner's somewhat lacklustre understanding of the concept of documentation.  TI is way ahead on quality of open documentation for the BBB, except for its GPU which remains closed.  Apparently the open source Lima driver for the OLinuXino's MALI-400 is better than the Allwinner binary blob anyway, so at least for graphics support it might not matter much. image

 

Interesting times ahead.  I'm certainly keeping an eye open on Olimex, they're a very competent and extremely productive outfit.  Progress on their OLinuXino boards and other newsworthy developments are typically announced on their blog.

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 13 years ago in reply to morgaine +2
    That's a good question about the A9. I wonder if there will be or is a Sitara SoC part with that for which a similar low-cost board could be made (BeagleBone Graphene - early 2014? ). I'll see Jason in…
  • morgaine
    morgaine over 13 years ago +1
    The A10S-OLinuXino-MICRO isn't in the exceptionally low Raspberry Pi and BBB price niche, but it may be worth pointing out that this board has Raspberry Pi-like graphics and media capability (unlike the…
  • morgaine
    morgaine over 13 years ago +1
    Olimex has blogged instructions on building Linux for A10S from scratch . Since the A10S has a Cortex-A8 CPU like the BBB, these instructions and the linux-sunxi Github repositories to which they refer…
Parents
  • morgaine
    morgaine over 13 years ago

    One thing that has long puzzled me is why no ARM licensee has seen fit to release a board providing two NICs, AFAIK.

     

    Such boards are common in the x86 world, especially ATX server boards and those using the Mini-ITX form factor, but because they are generic motherboards and thus contain (as usual) everything, their prices are typically high.  So high in fact that networking enthusiasts have to resort to hacking commodity routers like the Linksys WRT54GL to obtain a dual NIC comms device at a reasonable price.

     

    The first open hardware dual-NIC ARM board that appears at a "Pi era" price is going to have the market almost to itself, and I think it is reasonable to expect that legions of WRT users would snap it up.  Also, the A20 SoC provides 1000Mbps Ethernet capability, and it would be low-hanging fruit to harness this.

     

    To that end, here is a little suggestion for Olimex's hypothetical OLinuXino comms and servers product line: image

     

     

    Single-NIC comms:

     

    SoCCoresARM Core
    RAMProduct ModelPriceFeatures
    A202Cortex-A71GBA20-OLinuXino-NANO-GIGA35 euroNo video, No SATA, gigabit
    A202Cortex-A71GBA20-OLinuXino-NANO-GIGA-4GB45 euroNo video, No SATA, gigabit, Flash
    A202Cortex-A71GBA20-OLinuXino-MICRO-GIGA55 euroNo video, SATA, gigabit
    A202Cortex-A71GBA20-OLinuXino-MICRO-GIGA-4GB65 euroNo video, SATA, gigabit, Flash

     

     

    Dual-NIC comms:

     

    SoCCoresARM Core
    RAMProduct ModelPriceFeatures
    XXX *2Cortex-A7/A91GBXXX-OLinuXino-2NIC40 euroNo video, No SATA, 2xNIC
    XXX *2Cortex-A7/A91GBXXX-OLinuXino-2NIC-4GB50 euroNo video, No SATA, 2xNIC, Flash
    XXX *2Cortex-A7/A9
    1GBXXX-OLinuXino-2NIC-GIGA60 euroNo video, SATA, 2xNIC, gigabit
    XXX *2Cortex-A7/A9
    1GBXXX-OLinuXino-2NIC-GIGA-4GB70 euroNo video, SATA, 2xNIC, gigabit, Flash

    (*) A20 seems not to have dual MAC capability, so replaced here by i.MX6.**

    (**) It turns out that i.MX6 doesn't have dual MAC either and can't handle full gigabit anyway, so replaced i.M6 by "XXX".

     

     

    The proposed pricing is just guesstimate figures intended to reflect the BOM cost savings made by omitting the HDMI and VGA support devices and sockets, since the intended application area is headless communication devices and servers.  Devices like routers and firewalls typically wouldn't need SATA either, so even more savings are possible.  As a result, some of these boards in the hypothetical comms and servers product range could in principle be cheaper than Olimex's currently listed A20 OLinuXinos.

     

    Of course, this assumes that a dual-MAC SoC offering full gigabit performance exists at A20 prices ... a tall order!  That said, today's wishful thinking is tomorrow's reality, and these suggestions are for tomorrow.

     

    It's a nice sunny Sunday afternoon for dreaming up products. image

     

    Morgaine.

     

    PS. The second table has been evolving as a result of our discussions, from its original A20 to i.MX6 and now to just an XXX placeholder.  These changes may confuse any references in the thread below a bit, but if in doubt, just blame me. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    One thing that has long puzzled me is why no ARM licensee has seen fit to release a board providing two NICs, AFAIK.

    The AM3359 does include two NICs, and there is a board using it with two ethernet ports 21030432103043 however when you read the doc for that board, it appears that both ethernet ports are connected to the PRUs and hence you get access to EtherCat, but it's not clear if or how you would use them for normal ethernet.

     

    It's not immediately clear to me that the iMX6 has dual mac capability either. The reference manual is huge though, so I may have missed it. Got a pointer to that bit of useful information ?

    That said, as the i.MX6 has PCIe capability it's certainly possible to simply add multiple extra nics that way.

     

    While dual, or triple, nic configurations (perhaps similar to the PCEngines ALIX boards http://www.element14.com/community/community/knode/single-board_computers/blog/2013/06/06/alix-boards-the-open-source-alternative-to-proprietary-routers ) would be nice, if you have a vlan capable switch then it's possible to get to the same place with a single nic. Although that does bring us back to the point you made in another thread - 10/100 network is no longer good enough and it appears as if the A20 is similar to the A10 in only having 10/100, although you'd be forgiven for thinking neither of them have any network capability since it doesn't seem to get a mention in any of the datasheets.

     

    So while we're dreaming up products for Olimex, there's already an A20 MarsBoard http://www.hotmcu.com/marsboard-a20-dev-board-p-60.html

    which has 1GB, SATA, Video, Flash at $58 or approx 45 euro, downside of course is the 10/100 nic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    The AM3359 does include two NICs, and there is a board using it with two ethernet ports Re: Olimex A10S/A20-OLinuXino boards quite BBB-likeRe: Olimex A10S/A20-OLinuXino boards quite BBB-like2103043 however when you read the doc for that board, it appears that both ethernet ports are connected to the PRUs and hence you get access to EtherCat, but it's not clear if or how you would use them for normal ethernet.

     

    Wow, awesome!  How did we miss that board among ARM discussions?  It even has quite a reasonable price!

     

    however when you read the doc for that board, it appears that both ethernet ports are connected to the PRUs and hence you get access to EtherCat, but it's not clear if or how you would use them for normal ethernet.

     

    EtherCAT and Ethernet are transparent to each other.  You can run both simultaneously through the same hardware, differentiated only by frame IDs.  I assume that the same driver handles both, and if the EtherCAT mode is set on an incoming frame then the driver makes it persist in the outgoing frame.

     

    The big problem with the above board's design though is that by using the PRUs for realtime performance in EtherCAT, they've necessarily restricted their Ethernet speed to 10/100Mbps, which is a big shame when the AM3359's MACs have gigabit capability.  The board is already "interesting" just because of the extreme rarity of dual-NIC boards, but gigabit would have made it awesome.  (But unfortunately, also more expensive.)

     

    It's not immediately clear to me that the iMX6 has dual mac capability either. The reference manual is huge though, so I may have missed it. Got a pointer to that bit of useful information ?

     

    Good point, I wonder where I got that from.  If I find the corresponding info in the datasheet, I'll add it here later.  But if i.MX6 doesn't support dual NICs then simply replace i.MX6 by TI's equivalent SoC which most probably does.  Olimex likes TI anyway.

     

    it appears as if the A20 is similar to the A10 in only having 10/100, although you'd be forgiven for thinking neither of them have any network capability since it doesn't seem to get a mention in any of the datasheets.

     

    The A20's short datasheet mentions 1000Mbps in a bullet list about GMAC features on page 8:

    - Support 10/100/1000Mbps data transfer rates RGMII interface to communicate with an external Gigabit PHY

     

    It also mentions that it can handle Jumbo Ethernet Frames up to 16KB in size, which is very cool not only for fast networking but also for use in a comms device that needs to encapsulate full 1500-octet Ethernet frames in ATM for PPPoA without limiting MTUs to the dreaded limit of 1492 that causes many people problems.

     

    With so many nice features, it's a pity that the A20 isn't aimed at communications, otherwise it would offer more than just a single MAC.  On the other hand, if it did then it would probably cost more unless it sacrificed something.

     

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Wow, awesome!  How did we miss that board among ARM discussions?  It even has quite a reasonable price!

    I found it by luck many months ago. I may have mentioned it here.. somewhere.. but not sure.

     

    EtherCAT and Ethernet are transparent to each other.  You can run both simultaneously through the same hardware, differentiated only by frame IDs.  I assume that the same driver handles both, and if the EtherCAT mode is set on an incoming frame then the driver makes it persist in the outgoing frame.

    So the question is...... The BBB people say it's ok to use the 3358 (?) since the only additional feature of the 3359 is EtherCat and it's, somehow, not being used on the BBB.  So given we have EtherCat capability in the current 3359 why can't we use it ?  Is there something different about the hardware on the BBB ?  Something not wired up ?  Picked the wrong phy ?

     

    There's something in the docs saying that the EtherCat side is handled by the PRU and not the more normal linux driver. I don't pretend to know enough about EtherCat or the implementation on the am3359, but it would appear that it's not quite as simple.

     

    The A20's short datasheet mentions 1000Mbps in a bullet list about GMAC features on page 8:

    Good catch, I missed that. So it has an internal 10/100 MAC and needs some external GMAC to do 1000Mbps ?   I wonder how many boards will bother implementing gigabit if that's the case.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    So given we have EtherCat capability in the current 3359 why can't we use it ?

     

    My understanding was that we can use EtherCAT on the current AM3359 version of BBB, but nobody has so far simply because it's of such esoteric interest.  When CircuitCo shifts to using the AM3358BZCZ100 SoC instead of the AM3359, then we won't be able to use EtherCAT at all, even if we wished to.

     

    I wanted to know what aspect of the AM3358BZCZ100 would prevent use of EtherCAT and so I asked the question here in the early days of BBB, but nobody answered with that information.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    So given we have EtherCat capability in the current 3359 why can't we use it ?

     

    My understanding was that we can use EtherCAT on the current AM3359 version of BBB, but nobody has so far simply because it's of such esoteric interest.  When CircuitCo shifts to using the AM3358BZCZ100 SoC instead of the AM3359, then we won't be able to use EtherCAT at all, even if we wished to.

     

    I wanted to know what aspect of the AM3358BZCZ100 would prevent use of EtherCAT and so I asked the question here in the early days of BBB, but nobody answered with that information.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    My understanding was that we can use EtherCAT on the current AM3359 version of BBB,

    Fair enough, I don't know enough about it to argue.  I just wonder if there's something more to it, was John right in that other thread suggesting you need two ports ?

     

    Also, in the ICE user manual it very specifically says "10/100 Ethernet PRU Controlled Ports". What's the significance of that statement, if any ?  The ICE board also uses a different PHY from BBB, simple cost savings or something not supported ?

     

    For practical purposes there's no difference between all the necessary hardware being present (and connected) but no driver being available and the hardware requirements not being fully met on the BBB somehow. They are very different though, in the first case you just need to be able to write the driver or pay someone to do it..

     

    I expect it's all academic though, fairly clear that we simply don't know enough to implement it ourselves right now - at least not without a lot of help from someone who does.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I just wonder if there's something more to it, was John right in that other thread suggesting you need two ports ?

     

    Well the only requirement is a physical path to get frames from one EtherCAT device to another --- any physical topology that links masters to slaves will do.  Having two NICs allows you to cascade boards without additional glue hardware so there's a clear cost benefit, but you still have a couple of options available if your boards have only a single NIC.  One is to use them only in pairs, since the start and end of a chain of EtherCAT devices need only one NIC, although that does limit your range of application.  And the other is to use switches configured to replicate traffic on multiple ports to do all the routing between single-NIC EtherCAT boards.  Port replication is available quite widely even on low-end managed switches.

     

    The ICE board also uses a different PHY from BBB, simple cost savings or something not supported ?

     

    I don't know, but my understanding is that there is nothing special about PHYs used for EtherCAT.  As a physical layer device, you would expect it to just encode/decode the standard 802.3 frame without looking at the ethertype.  The choice of PHY is mainly determined by the interface provided by the host MAC, which is typically RMII on application SoCs to keep the pincount low.  The BBB's SMSC LAN8710 PHY supports both MII and RMII, and is supposedly compliant with the various 802.3 specs.

     

    I expect it's all academic though, fairly clear that we simply don't know enough to implement it ourselves right now - at least not without a lot of help from someone who does.

     

    It would indeed be nice to attract some expert on the subject here.  Seeing as Farnell sells so many BBBs for CircuitCo, how about someone asking Gerald Coley to pay us a short visit?  This is actually relevant to current product, because CircuitCo switched over to AM3358 on the original BeagleBone (white) with board revision A6A, so EtherCAT is now gone there, and undoubtedly will disappear soon on BBB as well.  I would like to know the physical reason that prevents the new SoC from supporting it.  It shouldn't be left as a mystery.

     

    Morgaine.

     

     

    PS.  And while we're at it, it would be good to know whether there is anything physically preventing single-NIC EtherCAT operation on AM3359-based BBBs, to avoid disappointment in case someone embarks on an EtherCAT project with expectations of fun.  There are a lot of AM3359-based BBBs out there, as well as A5A BBs.