Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Olimex A10S/A20-OLinuXino boards quite BBB-like
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 113 replies
  • Subscribers 64 subscribers
  • Views 16802 views
  • Users 0 members are here
  • olinuxino
  • allwinner
  • bbb
  • olimex
  • a20
  • a10
Related

Olimex A10S/A20-OLinuXino boards quite BBB-like

morgaine
morgaine over 13 years ago

I've gathered together some pieces of information on Olimex's latest Cortex-A* board range, which I think is an interesting one.

 

Allwinner's new A20 device has almost the same pinout as their old A10, so Olimex developed an A20 board very quickly by upgrading an earlier A10-based prototype with the new SoC.  They already had a different OLinuXino board based on the lower-cost A10S in early production, so the future A20 board is being positioned as a more capable version of this product.

 

This pair of boards have the product names A10S-OLinuXino-MICRO and A20-OLinuXino-MICRO, and Olimex's price list shows that each of these will also be available with 4GB of NAND flash on board, respectively named as A10S-OLinuXino-MICRO-4GB and A20-OLinuXino-MICRO-4GB.    Summary of the range:

 

 

SoCCoresARM Core
RAMProduct ModelPriceFeatures
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO45 euro
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO-4GB55 euroFlash
A202Cortex-A71GBA20-OLinuXino-MICRO55 euroSATA
A202Cortex-A71GBA20-OLinuXino-MICRO-4GB65 euroFlash, SATA

 

 

Note that there is more symmetry in the  product naming  than in the actual board layouts, as A10S and A20 boards are quite different to reflect the differences in their SoCs.

 

The NAND-less A10S-OLinuXino-MICRO [summary pdf] is already listed at Farnell UK, delivery projected for end of July, and development work on the A20-OLinuXino-MICRO seems to be progressing well.

 

The A10S-OLinuXino-MICRO-4GB is pretty similar to the BeagleBone Black (BBB) in several ways.  The A10S has a Cortex-A8 CPU just like the BBB's TI AM3359, and both are clocked at the same speed of 1GHz.  Both provide native Ethernet, not over USB.  Both boards offer 512MB of RAM.  Likewise both feature on-board embedded flash as well as sockets for external cards, although the OLinuXino has double the flash and two different card sockets.  Both provide HDMI for video output (the A10S's GPU is a MALI-400), although the OLinuXino also provides analogue audio input and output sockets.  Both provide roughly the same kind of expansion connector concept, ie. a connector on each of the opposing long edges of the board.  As usual on Olimex boards, the OLinuXino also provides a UEXT connector which allows Olimex's large range of expansion modules to be attached.

 

The above isn't intended to portray the A10S-OLinuXino-MICRO-4GB as "better" despite it having several extra features.  The BBB is quite a lot cheaper and provides stackable capes and the AM335x's exceptional PRUs, so it'll always be "horses for courses" between the two.  I do think that the two boards are close enough in features to be considered ballpark-similar.

 

The A20-OLinuXino-MICRO and -4GB version will be quite a significant step up from their A10S-based siblings.  The CPU is a dual-core Cortex-A7 (see the A20 and Allwinner family brief pdf and short A20 datasheet for more details), RAM is doubled to 1GB of DDR3, video output is through both HDMI and VGA, and SATA data and power connectors are provided.  For 55 to 65 Euro, I expect that Olimex are going to have a serious hit on their hands.

 

And the entire OLinuXino range is both open hardware and open software, give or take Allwinner's somewhat lacklustre understanding of the concept of documentation.  TI is way ahead on quality of open documentation for the BBB, except for its GPU which remains closed.  Apparently the open source Lima driver for the OLinuXino's MALI-400 is better than the Allwinner binary blob anyway, so at least for graphics support it might not matter much. image

 

Interesting times ahead.  I'm certainly keeping an eye open on Olimex, they're a very competent and extremely productive outfit.  Progress on their OLinuXino boards and other newsworthy developments are typically announced on their blog.

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 13 years ago in reply to morgaine +2
    That's a good question about the A9. I wonder if there will be or is a Sitara SoC part with that for which a similar low-cost board could be made (BeagleBone Graphene - early 2014? ). I'll see Jason in…
  • morgaine
    morgaine over 13 years ago +1
    The A10S-OLinuXino-MICRO isn't in the exceptionally low Raspberry Pi and BBB price niche, but it may be worth pointing out that this board has Raspberry Pi-like graphics and media capability (unlike the…
  • morgaine
    morgaine over 13 years ago +1
    Olimex has blogged instructions on building Linux for A10S from scratch . Since the A10S has a Cortex-A8 CPU like the BBB, these instructions and the linux-sunxi Github repositories to which they refer…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Morgaine Dinova wrote:

     

    The A10S-OLinuXino-MICRO-4GB is pretty similar to the BeagleBone Black (BBB) in several ways. 

    I'm conflicted here...  I very much want to like the Olimex stuff, especially the A10 boards.  However, video isn't even on my list of things to have.  So I'm left wondering what the advantages of the A10S-Olinuxino is for the extra cost. As you say, they are very similar in a lot of other ways.

     

    If Olimex could get their boards out of the door a bit quicker and a bit cheaper I think I'd have several by now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I very much want to like the Olimex stuff, especially the A10 boards.  However, video isn't even on my list of things to have.  So I'm left wondering what the advantages of the A10S-Olinuxino is for the extra cost. As you say, they are very similar in a lot of other ways.

     

    As always, it's a matter of matching features to problem requirements.  Like yourself, I have no significant interest in media, so while I might dedicate a board to such functions one day, it's not even on my TODO list at present.

     

    In contrast, low-consumption Internet servers are an active area of interest for me, which makes the SATA interface a very attractive feature in the A20-based OLinuXinos, strongly helped by the dual cores since Internet service can make good use of hardware parallism.  I'm sure to get some of those A20 boards if Farnell or some other local UK company stocks them.

     

    The A10S-OLinuXino[-4GB] lacks SATA and costs more than BBB, so its niche appears to be "An open hardware version of Raspberry Pi with expanded hardware interfacing and faster."  If that spec is what someone needs and the extra cost is still viable, then it has a niche.  We'll see.  Personally I don't have that set of requirements, since BBB covers my interfacing needs nicely.  The A20-OLinuXino will fulfill a completely different requirement for me, Internet servers.

     

    Morgaine.

     

    Addendum.  Of course, the Wandboard would make an even better Internet server with its gigabit Ethernet, SATA, and 1-2-4 cores.  Unfortunately it's not sold in the UK and so they didn't get my money.  I hope that Olimex takes note of this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    If that spec is what someone needs and the extra cost is still viable,

    I can't see it, not unless you've had your head in the sand for a couple of years and don't know the RPi or BBB exist. Sure, there are philosophical reasons for wanting a more open platform than an RPi, but I always wonder how those sorts of reasons stack up against the financial cost. Sure, there are those of us who might believe it's worth it, but the masses won't.

     

      Unfortunately it's not sold in the UK and so they didn't get my money.  I hope that Olimex takes note of this.

    I do too.  I'm still considering getting a couple of wandboards from future-electronics who seem to offer the best gbp price while still shipping from the US. Olimex are in the same boat though, while there's some limited availability here, I'm unlikely to invest a lot of time/effort building something around a board that I can't easily replace if something ever does go wrong.

     

    While we don't seem to have had much luck with Farnell getting a better range of these boards, I wonder if someone at CPC might be listening.. Could be an opportunity for them image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

     

    While we don't seem to have had much luck with Farnell getting a better range of these boards, I wonder if someone at CPC might be listening.. Could be an opportunity for them image

     

    I Hope so image  It does look like Farnell is pitching CPC  more for the "Maker" market they have produced a MakerTech catalogue.

    I have driven past CPC twice this week without calling in, suffering withdrawal symptoms.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bwelsby
    bwelsby over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

     

    While we don't seem to have had much luck with Farnell getting a better range of these boards, I wonder if someone at CPC might be listening.. Could be an opportunity for them image

     

    I Hope so image  It does look like Farnell is pitching CPC  more for the "Maker" market they have produced a MakerTech catalogue.

    I have driven past CPC twice this week without calling in, suffering withdrawal symptoms.image