Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Olimex A10S/A20-OLinuXino boards quite BBB-like
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 113 replies
  • Subscribers 64 subscribers
  • Views 16374 views
  • Users 0 members are here
  • olinuxino
  • allwinner
  • bbb
  • olimex
  • a20
  • a10
Related

Olimex A10S/A20-OLinuXino boards quite BBB-like

morgaine
morgaine over 13 years ago

I've gathered together some pieces of information on Olimex's latest Cortex-A* board range, which I think is an interesting one.

 

Allwinner's new A20 device has almost the same pinout as their old A10, so Olimex developed an A20 board very quickly by upgrading an earlier A10-based prototype with the new SoC.  They already had a different OLinuXino board based on the lower-cost A10S in early production, so the future A20 board is being positioned as a more capable version of this product.

 

This pair of boards have the product names A10S-OLinuXino-MICRO and A20-OLinuXino-MICRO, and Olimex's price list shows that each of these will also be available with 4GB of NAND flash on board, respectively named as A10S-OLinuXino-MICRO-4GB and A20-OLinuXino-MICRO-4GB.    Summary of the range:

 

 

SoCCoresARM Core
RAMProduct ModelPriceFeatures
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO45 euro
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO-4GB55 euroFlash
A202Cortex-A71GBA20-OLinuXino-MICRO55 euroSATA
A202Cortex-A71GBA20-OLinuXino-MICRO-4GB65 euroFlash, SATA

 

 

Note that there is more symmetry in the  product naming  than in the actual board layouts, as A10S and A20 boards are quite different to reflect the differences in their SoCs.

 

The NAND-less A10S-OLinuXino-MICRO [summary pdf] is already listed at Farnell UK, delivery projected for end of July, and development work on the A20-OLinuXino-MICRO seems to be progressing well.

 

The A10S-OLinuXino-MICRO-4GB is pretty similar to the BeagleBone Black (BBB) in several ways.  The A10S has a Cortex-A8 CPU just like the BBB's TI AM3359, and both are clocked at the same speed of 1GHz.  Both provide native Ethernet, not over USB.  Both boards offer 512MB of RAM.  Likewise both feature on-board embedded flash as well as sockets for external cards, although the OLinuXino has double the flash and two different card sockets.  Both provide HDMI for video output (the A10S's GPU is a MALI-400), although the OLinuXino also provides analogue audio input and output sockets.  Both provide roughly the same kind of expansion connector concept, ie. a connector on each of the opposing long edges of the board.  As usual on Olimex boards, the OLinuXino also provides a UEXT connector which allows Olimex's large range of expansion modules to be attached.

 

The above isn't intended to portray the A10S-OLinuXino-MICRO-4GB as "better" despite it having several extra features.  The BBB is quite a lot cheaper and provides stackable capes and the AM335x's exceptional PRUs, so it'll always be "horses for courses" between the two.  I do think that the two boards are close enough in features to be considered ballpark-similar.

 

The A20-OLinuXino-MICRO and -4GB version will be quite a significant step up from their A10S-based siblings.  The CPU is a dual-core Cortex-A7 (see the A20 and Allwinner family brief pdf and short A20 datasheet for more details), RAM is doubled to 1GB of DDR3, video output is through both HDMI and VGA, and SATA data and power connectors are provided.  For 55 to 65 Euro, I expect that Olimex are going to have a serious hit on their hands.

 

And the entire OLinuXino range is both open hardware and open software, give or take Allwinner's somewhat lacklustre understanding of the concept of documentation.  TI is way ahead on quality of open documentation for the BBB, except for its GPU which remains closed.  Apparently the open source Lima driver for the OLinuXino's MALI-400 is better than the Allwinner binary blob anyway, so at least for graphics support it might not matter much. image

 

Interesting times ahead.  I'm certainly keeping an eye open on Olimex, they're a very competent and extremely productive outfit.  Progress on their OLinuXino boards and other newsworthy developments are typically announced on their blog.

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 13 years ago in reply to morgaine +2
    That's a good question about the A9. I wonder if there will be or is a Sitara SoC part with that for which a similar low-cost board could be made (BeagleBone Graphene - early 2014? ). I'll see Jason in…
  • morgaine
    morgaine over 13 years ago +1
    The A10S-OLinuXino-MICRO isn't in the exceptionally low Raspberry Pi and BBB price niche, but it may be worth pointing out that this board has Raspberry Pi-like graphics and media capability (unlike the…
  • morgaine
    morgaine over 13 years ago +1
    Olimex has blogged instructions on building Linux for A10S from scratch . Since the A10S has a Cortex-A8 CPU like the BBB, these instructions and the linux-sunxi Github repositories to which they refer…
Parents
  • morgaine
    morgaine over 12 years ago

    Interesting news on Olimex's A20-based products in their latest  blog post on "A20-SOM Update" :

     

    OLIMEX Ltd wrote:

     

    On A20-SOM-EVB we put two new peripherials: Gigabit Ethernet and 2Mpix @30fps camera.

     

    The Gigabit Ethernet gave us a little bit of troubles at the beginning as the Gmac pinmux was quite different than Emac, but now it works.

     

    What is a bit dissapointing is that Gigabit Ethernet can't achieve more than 330Mbit/s transfer with the current state of the drivers, there were few comments that this may improve a bit later, but ARMs seems not quite capable with Gigabit Interfaces if you read for other popular ARMs like imx6 also can't have full throughput of Gigabit Ethernet.

     

    What Oliver Schinagl point out in #linux-sunxi IRC channel is that A20 emac and gmac share different multiplexing on different ports and use different registers, so it may be possible A20 to have two Ethernet ports one 100Mbit and one 1Gbit as same time, but this nobody try yet as no hardware to check.

     

    Sure with A20-SOM it would be easy to modify the current EVB and to add second 100Mbit Ethernet interface and to try if it works.

     

    Last thing we fight now is the camera, it is GT2005 and supported in Android but the support in Linux is not complete, nevermind we are going to run A20-SOM now in production and deal with the camera later as at hardware level everything seems ok.

     

    So we are going to rework some mistakes we found on the prototypes and will run production, so in November A20-SOM should be ready in stock.

     

    Note that the combined A20-SOM plus A20-SOM-EVB baseboard is not a cheap solution.  According to this blog post from September:

     

    A20-SOM-EVB (including A20-SOM) will cost EUR 80 and A20-SOM-4GB-EVB (including A20-SOM-4GB) will cost EUR 85.

     

    So,  interesting developments on the A20 front.  Not sure about progress on the A20-OLinuXino though.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to morgaine

    STOP PRESS!!!  The A20-OLinuXino boards were already released!  Olimex corrected my mistake:

     

    Olimex Ltd wrote:

     

    A20-OLinuXino-MICRO is in production and thousands are already in use, it has most complete Android and Linux support from all our board

     

    Super!  So now it's just a matter of Farnell UK getting their act together and listing it for me.

     

    Olimex product page links for easy access:

     

    • A20-OLinuXino-MICRO
    • A20-OLinuXino-MICRO-4GB

     

    It's a good day! image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    STOP PRESS!!!  The A20-OLinuXino boards were already released!  Olimex corrected my mistake:

    They've been listed in the olimex shop for a while now.  I'm never quite clear if they actually have stock or if it's a placeholder listing though.

    Super!  So now it's just a matter of Farnell UK getting their act together and listing it for me.

    That's my usual complaint for olimex boards, no availability through normal channels image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    They've been listed in the olimex shop for a while now.

     

    Yes, but unfortunately that has no bearing on commercial availability.  They were listed in the shop back when I started this thread, and at that time they were still discussing their development in the blog.

     

    I'm never quite clear if they actually have stock or if it's a placeholder listing though.

     

    Aye, that's quite a problem with Olimex's shop.  A simple "In development / In production / In stock / Restocking" legend would help enormously.

     

    That's my usual complaint for olimex boards, no availability through normal channels image

     

    Since 233-OLinuXino, A13-OLinuXino and A10S-OLinuXino are all listed and in stock at Farnell UK, I'm going to cross my fingers and hope that the Farnell UK buyer will come out of the perpetual business meetings soon and add the two A20-OLinuXino-MICRO boards to their catalogue.

     

    As they say, "Take my money!!!". image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    They've been listed in the olimex shop for a while now.

     

    Yes, but unfortunately that has no bearing on commercial availability.  They were listed in the shop back when I started this thread, and at that time they were still discussing their development in the blog.

     

    I'm never quite clear if they actually have stock or if it's a placeholder listing though.

     

    Aye, that's quite a problem with Olimex's shop.  A simple "In development / In production / In stock / Restocking" legend would help enormously.

     

    That's my usual complaint for olimex boards, no availability through normal channels image

     

    Since 233-OLinuXino, A13-OLinuXino and A10S-OLinuXino are all listed and in stock at Farnell UK, I'm going to cross my fingers and hope that the Farnell UK buyer will come out of the perpetual business meetings soon and add the two A20-OLinuXino-MICRO boards to their catalogue.

     

    As they say, "Take my money!!!". image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    As they say, "Take my money!!!". image

    Your money (and mine) appears to be safe where it is image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 12 years ago in reply to e14 Contributor

    I like more and more what the Olimex folks are doing. I've on the bench under test right now the OlinuXino Nano with the Freescale iMX233 running Debian Linux and works like a charm !!

     

    No problems at all to get it up running and connected to a wireless network.

     

    U$S26

     

    -J