Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Olimex A10S/A20-OLinuXino boards quite BBB-like
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 113 replies
  • Subscribers 64 subscribers
  • Views 16344 views
  • Users 0 members are here
  • olinuxino
  • allwinner
  • bbb
  • olimex
  • a20
  • a10
Related

Olimex A10S/A20-OLinuXino boards quite BBB-like

morgaine
morgaine over 13 years ago

I've gathered together some pieces of information on Olimex's latest Cortex-A* board range, which I think is an interesting one.

 

Allwinner's new A20 device has almost the same pinout as their old A10, so Olimex developed an A20 board very quickly by upgrading an earlier A10-based prototype with the new SoC.  They already had a different OLinuXino board based on the lower-cost A10S in early production, so the future A20 board is being positioned as a more capable version of this product.

 

This pair of boards have the product names A10S-OLinuXino-MICRO and A20-OLinuXino-MICRO, and Olimex's price list shows that each of these will also be available with 4GB of NAND flash on board, respectively named as A10S-OLinuXino-MICRO-4GB and A20-OLinuXino-MICRO-4GB.    Summary of the range:

 

 

SoCCoresARM Core
RAMProduct ModelPriceFeatures
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO45 euro
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO-4GB55 euroFlash
A202Cortex-A71GBA20-OLinuXino-MICRO55 euroSATA
A202Cortex-A71GBA20-OLinuXino-MICRO-4GB65 euroFlash, SATA

 

 

Note that there is more symmetry in the  product naming  than in the actual board layouts, as A10S and A20 boards are quite different to reflect the differences in their SoCs.

 

The NAND-less A10S-OLinuXino-MICRO [summary pdf] is already listed at Farnell UK, delivery projected for end of July, and development work on the A20-OLinuXino-MICRO seems to be progressing well.

 

The A10S-OLinuXino-MICRO-4GB is pretty similar to the BeagleBone Black (BBB) in several ways.  The A10S has a Cortex-A8 CPU just like the BBB's TI AM3359, and both are clocked at the same speed of 1GHz.  Both provide native Ethernet, not over USB.  Both boards offer 512MB of RAM.  Likewise both feature on-board embedded flash as well as sockets for external cards, although the OLinuXino has double the flash and two different card sockets.  Both provide HDMI for video output (the A10S's GPU is a MALI-400), although the OLinuXino also provides analogue audio input and output sockets.  Both provide roughly the same kind of expansion connector concept, ie. a connector on each of the opposing long edges of the board.  As usual on Olimex boards, the OLinuXino also provides a UEXT connector which allows Olimex's large range of expansion modules to be attached.

 

The above isn't intended to portray the A10S-OLinuXino-MICRO-4GB as "better" despite it having several extra features.  The BBB is quite a lot cheaper and provides stackable capes and the AM335x's exceptional PRUs, so it'll always be "horses for courses" between the two.  I do think that the two boards are close enough in features to be considered ballpark-similar.

 

The A20-OLinuXino-MICRO and -4GB version will be quite a significant step up from their A10S-based siblings.  The CPU is a dual-core Cortex-A7 (see the A20 and Allwinner family brief pdf and short A20 datasheet for more details), RAM is doubled to 1GB of DDR3, video output is through both HDMI and VGA, and SATA data and power connectors are provided.  For 55 to 65 Euro, I expect that Olimex are going to have a serious hit on their hands.

 

And the entire OLinuXino range is both open hardware and open software, give or take Allwinner's somewhat lacklustre understanding of the concept of documentation.  TI is way ahead on quality of open documentation for the BBB, except for its GPU which remains closed.  Apparently the open source Lima driver for the OLinuXino's MALI-400 is better than the Allwinner binary blob anyway, so at least for graphics support it might not matter much. image

 

Interesting times ahead.  I'm certainly keeping an eye open on Olimex, they're a very competent and extremely productive outfit.  Progress on their OLinuXino boards and other newsworthy developments are typically announced on their blog.

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 13 years ago in reply to morgaine +2
    That's a good question about the A9. I wonder if there will be or is a Sitara SoC part with that for which a similar low-cost board could be made (BeagleBone Graphene - early 2014? ). I'll see Jason in…
  • morgaine
    morgaine over 13 years ago +1
    The A10S-OLinuXino-MICRO isn't in the exceptionally low Raspberry Pi and BBB price niche, but it may be worth pointing out that this board has Raspberry Pi-like graphics and media capability (unlike the…
  • morgaine
    morgaine over 13 years ago +1
    Olimex has blogged instructions on building Linux for A10S from scratch . Since the A10S has a Cortex-A8 CPU like the BBB, these instructions and the linux-sunxi Github repositories to which they refer…
  • morgaine
    morgaine over 13 years ago

    The A10S-OLinuXino-MICRO isn't in the exceptionally low Raspberry Pi and BBB price niche, but it may be worth pointing out that this board has Raspberry Pi-like graphics and media capability (unlike the BBB), and so will the A20 version.  This suggests that the A10S/A20 range of OLinuXino boards may provide the best of Pi graphics/media handling and BBB hardware interfacing capability for some users, when price is not the commanding factor.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago

    Olimex has blogged instructions on building Linux for A10S from scratch.  Since the A10S has a Cortex-A8 CPU like the BBB, these instructions and the linux-sunxi Github repositories to which they refer could be of interest to the BBB community as well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 13 years ago

    Very nice, I really like what Olimex is doing.  Hoping we'll get some of the more exciting OLinuXino's stocked soon in North America (I think Newark element14 only has iMX.233 last I checked; the Allwinner models are available via Farnell direct ship to US).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to fustini

    Indeed Drew.  In particular, the SATA capability on the two A20 models is going to open up a whole new set of applications in the conventional "computing" sphere, as storage performance is so lacklustre with SD cards.  I expect them to be popular as lightweight Internet servers positioned slightly above BBB, aided also by their dual cores.

     

    These two A20 models are going to be competing at the low end with Sabre-Lite, Wandboard and Minnowboard, and low-end/low-price is a good niche to be in.  I expect that Olimex are going to be selling a lot of them, while those competitors hold the high ground with their gigabit Ethernet and Cortex-A9 or Atom processors but sell far fewer.

     

    PS. Summary table added to first post.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to fustini

    Drew Fustini wrote:

     

    only has iMX.233 last I checked;

    I got one of the iMX.233 olinuxino boards and while I don't want to put anyone off, you'll be amazed at just how poor the comparative performance is to a cheaper R-Pi never mind a BBB.  While it does have much better IO than the RPi, I kind of wonder which niche, if any, it actually fits into.

    Hoping we'll get some of the more exciting OLinuXino's stocked soon

    Hoping we'll get any stocked soon... They've been on backorder for ages now. The BBB snuck in there and stole the show while Olimex weren't paying attention.

    I really want to like the Olimex stuff, but it's hard when you can't easily get hold of them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    the SATA capability on the two A20 models is going to open up a whole new set of applications

    The way I see things is that there's three distinct features that people want:

    1. GPU
    2. GPIO
    3. SATA

     

    While some uses are completely different, there's a fair amount of overlap - if you're doing XBMC then it'd be nice to have better storage than SD cards to keep your films on.

    So I tend to see the addition of SATA as being a plus point for all the other uses as well as a distinct feature. It makes all manner of other stuff so much easier.

     

    As such, I'll give any board with a SATA port a +1 on my list. With the A20 being a dual core it's even better.

     

    Do we know what speed the A20 boards will run at ?  I don't see anything obvious on that front on the Olimex page.

     

    I still think that 2Gb Wandboard Quad is going to be a hard one to beat though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Morgaine Dinova wrote:

     

    The A10S-OLinuXino-MICRO-4GB is pretty similar to the BeagleBone Black (BBB) in several ways. 

    I'm conflicted here...  I very much want to like the Olimex stuff, especially the A10 boards.  However, video isn't even on my list of things to have.  So I'm left wondering what the advantages of the A10S-Olinuxino is for the extra cost. As you say, they are very similar in a lot of other ways.

     

    If Olimex could get their boards out of the door a bit quicker and a bit cheaper I think I'd have several by now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago

    Speaking of Allwinner A10/A20, Rhombus-Tech is back in the news with their EOMA-68 card.  Latest news is that they've got Debian 7.0 Wheezy running on the A10, and are planning to make an A20 version thanks to the compatible pinout.  I've always liked the EOMA-68 form factor, which uses the same 50 mil 68-pin connector as PCMCIA [*] cards.  There's a GNU/Linux laptop in the works called Vivaldi "Flying Squirrel" which used an EOMA-68 as its brains so that it's easy to upgrade to a new CPU instead of tossing the old laptop into Morgaine's collection image

     

    No idea when anybody is going to be able to buy any of this stuff.

     

    EOMA-68 A20 and mini-docking card: http://liliputing.com/2013/06/eoma-68-pc-on-a-card-goes-dual-core-supports-debian-linux-has-new-accessories-in-the-works.html

     

    Rhombus-Tech news including Debian 7.0 Wheezy and first samples of A10 EOMA-68: http://rhombus-tech.net/allwinner_a10/news/

     

    [*] PCMCIA = People Cannot Memorize Computer Industry Acronyms.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I very much want to like the Olimex stuff, especially the A10 boards.  However, video isn't even on my list of things to have.  So I'm left wondering what the advantages of the A10S-Olinuxino is for the extra cost. As you say, they are very similar in a lot of other ways.

     

    As always, it's a matter of matching features to problem requirements.  Like yourself, I have no significant interest in media, so while I might dedicate a board to such functions one day, it's not even on my TODO list at present.

     

    In contrast, low-consumption Internet servers are an active area of interest for me, which makes the SATA interface a very attractive feature in the A20-based OLinuXinos, strongly helped by the dual cores since Internet service can make good use of hardware parallism.  I'm sure to get some of those A20 boards if Farnell or some other local UK company stocks them.

     

    The A10S-OLinuXino[-4GB] lacks SATA and costs more than BBB, so its niche appears to be "An open hardware version of Raspberry Pi with expanded hardware interfacing and faster."  If that spec is what someone needs and the extra cost is still viable, then it has a niche.  We'll see.  Personally I don't have that set of requirements, since BBB covers my interfacing needs nicely.  The A20-OLinuXino will fulfill a completely different requirement for me, Internet servers.

     

    Morgaine.

     

    Addendum.  Of course, the Wandboard would make an even better Internet server with its gigabit Ethernet, SATA, and 1-2-4 cores.  Unfortunately it's not sold in the UK and so they didn't get my money.  I hope that Olimex takes note of this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Rhombus-Tech is back in the news with their EOMA-68 card. 

    Unfortunately they're taking way too long to actually produce a working product. Until they can it's all just vapourware. Don't get me wrong, the RPi and many of the others could easily have gone the same way, but most of them seem to have jumped that last hurdle and actually got their product to market.

     

    As for EOMA-68, I think it's interesting that a lot of other devices are opting for the EDM format like the wandboard. Searching for EOMA-68 pretty much gets you Rhombus-Tech and nothing else and maybe some other un-realised ideas several pages down..

     

    How good, or bad, the technology is doesn't seem to matter. The competition have built the boards and sold them to people already, so the question becomes whether anyone will care about Rhombus & EOMA when they're a year late to every party and the tech has moved on to something better.

     

    I think we had a similar discussion about Rhombus way back last year, and sadly I can see us doing it again next year image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>