Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum BBB - Building the Linux Kernel
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 59 subscribers
  • Views 5549 views
  • Users 0 members are here
  • beaglebone_black
  • bbb
  • bb_black
  • beagle_bone_black
Related

BBB - Building the Linux Kernel

shabaz
shabaz over 13 years ago

Hi, I've added a step-by-step guide to building the Linux kernel for the BBB at the elinux wiki, so we can all edit it to improve the process. Particular thanks to Vlad Ungureanu for helping with debugging.

 

It took a while to get the steps ironed out. I still need to figure out how how to build the rest of the file system (there is a file system supplied

with TI's SDK) and getting it NFS-mounted.

 

These are the current steps documented (hopefully these links work):

 

  • 1 Beaglebone Black – Building Images
    • 1.1 Introduction
      • 1.1.1 Is it difficult?
      • 1.1.2 What is required?
      • 1.1.3 What steps are involved?
    • 1.2 Getting started - Folders
    • 1.3 Installing the build tools (toolchain)
      • 1.3.1 3. 1 Compile tools
      • 1.3.2 3.2 Some miscellaneous items
      • 1.3.3 3.3 U-boot
    • 1.4 Downloading and building the Linux Kernel
    • 1.5 Transferring the image to the BBB via TFTP
    • 1.6 Appendix: Installing and configuring the TFTP server
    • 1.7 Appendix: Installing and using Minicom
  • Sign in to reply
  • Cancel

Top Replies

  • bwelsby
    bwelsby over 13 years ago in reply to shabaz +1
    If you want a RHL/Centos style distro then you could try installing this root file system to go with your kernel from http://www.redsleeve.org/ no idea if it will work (in theory it should) but I will…
  • bwelsby
    bwelsby over 13 years ago in reply to shabaz +1
    Me too, when I was in gainfull employment I used nothing but Centos and RHEL. I only got into Debian and Ubuntu because of the R-Pi. It looks like a package repository is being built mainly for R-Pi but…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz +1
    shabaz wrote: ~/kernel/kernel$ make ARCH=arm CROSS_COMPILE=arm-angstrom-linux-gnueabi- INSTALL_MOD_PATH=$HOME/kernel/kernel/rootfs modules_install I'm not sure what it does, I'll try it. Does it create…
Parents
  • morgaine
    morgaine over 13 years ago

    That's excellent, shabaz!  I'll follow along on one of my Gentoo boxes and add any Gentoo-specific lines to the document.  I don't expect many differences.

     

    First of all I need to know the provinence of RHEL's ARM gcc variant.  Is it CodeSourcery, or is RedHat validating their own ARM compiler releases?  Gentoo has the following 3 ARM compiler  packages available in Portage, so if yours isn't one of these, Gentoo users will have to install a ggc-arm manually from some repo outside of Portage, not with the package manager:

     

    * dev-embedded/sgpp-lite-arm-eabi-bin
         Available versions:  (2010.09.51) ~2010.09.51
         Homepage:            http://www.codesourcery.com/sgpp/lite/arm
         Description:         regular, validated releases of the GNU Toolchain for arm processors by CodeSourcery

    * dev-embedded/sgpp-lite-arm-linux-bin
         Available versions:  (2010.09.50) ~2010.09.50
         Homepage:            http://www.codesourcery.com/sgpp/lite/arm
         Description:         regular, validated releases of the GNU Toolchain for arm processors by CodeSourcery

    * dev-embedded/sgpp-lite-arm-uclinux-bin
         Available versions:  (2010.09.58) ~2010.09.58
         Homepage:            http://www.codesourcery.com/sgpp/lite/arm
         Description:         regular, validated releases of the GNU Toolchain for arm processors by CodeSourcery

     

    PS. I sure hope the "2010" isn't a year, otherwise these ARM releases in Portage are clearly prehistoric. image  Gentoo's own ARM  installation procedure doesn't use the above, which hints that those 3 packages are a historical relic.

     

    Instead, Gentoo provides these instructions, specifically for BeagleBone, with cross tools installed using crossdev.

     

    Regarding the kernel, the above link advises to get the kernel using:

     

    git clone git://arago-project.org/git/projects/linux-am33x.git

     

    Is that kernel similar to yours in respect of version and patches?  Reading about the Arago Project, I'm a bit worried about kernel biodiversity creeping in here. image

     

    If your ARM compiler is maintained and validated by RedHat themselves, I suspect that for full compatibility with your steps, Gentoo users will have to grab your source RPM and unpack it directly.  If so, it would help if you could identify the actual package filepath that your commands install.

     

     

    [Fixed the almighty cocktail of compiler and kernel topics which made this post barely comprehensible.]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    Hi Morgaine,

     

    Morgaine Dinova wrote:

    I'll follow along on one of my Gentoo boxes and add any Gentoo-specific lines to the document.  I don't expect many differences.

    That's great! I hope the steps make sense, and it will be great to have them refined. I used RHEL for my Linux server, mainly because I'm not familiar with other variants, and the toolchain I used was one that was available pre-compiled via yum. But I did try CodeSourcery originally, and although it compiled the kernel, after TFTP'ing, it didn't work for me, but later I realized I was issuing the wrong u-boot parameters, so it's quite likely CodeSourcery is fine.  The CodeSourcery site (i.e. the Mentor Graphics site) did have much more recent toolchain dates, I had downloaded from there. In fact I've still got those steps because I was writing it as I went, I've pasted below. When it didn't work for me, I moved to the one via yum, and didn't get round to re-checking with CodeSourcery after I'd discovered the u-boot mistake I was making.

    From that arago-project, I had only downloaded some blob. The kernel was downloaded using git clone git://github.com/beagleboard/kernel.git

    That instruction was based on some websites that had instructions for Debian, but it seemed to work fine on my RHEL VM. I wish I knew how to get the exact tag for the releases though, because if I'm building the head of 3.8, then I'll never be sure what others may have checked-in I guess :-(

     

    ----------------------

    The compiler is Sourcery CodeBench Lite Edition for ARM GNU/Linux (2013.05-24 version) from Mentor Graphics’ website

    http://www.mentor.com/embedded-software/sourcery-tools/sourcery-codebench/lite/?cmpid=7108&lite=arm&target_os=GNU%2FLinux&target_arch=ARM&returnURL=https%253A%252F%252Fsourcery.mentor.com%252FGNUToolchain%252Fsubscription3057%253Flite%253Darm%2526cmpid%253D7108

    Note: the current toolchains from the Angstrom site and from TI’s SDK both had issues building the kernel.

    From that Mentor Graphics link, use the IA32 GNU/Linux TAR file rather than the installer

    The downloaded file was put in the toolchain folder and extracted (it created an arm-2013.05 folder). The folder /home/username/develop/toolchain/arm-2013.05/bin is important, it contains the compile tools. The PATH environment variable needs to be updated to prepend this: (assuming bash shell)

    PATH=/home/username/develop/toolchain/arm-2013.05/bin:$PATH

    Prepends the toolchain folder

    export PATH

    Sets the path for scripts to use

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to shabaz

    I was working with Arch linux earlier and had the exact same errors, it turned out I was running kernel 3.8.13-3-ARCH and when I looked in /usr/lib/modules I saw a subdirectory 3.8.13-1-ARCH  I forced an update of kernel and modules and the subdirectory was replaced to match the kernel...  and all the errors went away. image

     

    You need a step in your instructions for installing the modules.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to bwelsby

    Hi Brian,

     

    I see on this site this instruction, which I seem to be missing:

    ~/kernel/kernel$ make ARCH=arm CROSS_COMPILE=arm-angstrom-linux-gnueabi- INSTALL_MOD_PATH=$HOME/kernel/kernel/rootfs modules_install

    I'm not sure what it does, I'll try it. Does it create a file system containing the modules that I will need to tftp do you think?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to shabaz

    If you want a RHL/Centos style distro then you could try installing this root file system to go with your kernel from  http://www.redsleeve.org/ no idea if it will work (in theory it should) but I will give it a try when I get chance.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to bwelsby

    That's great!! I'm looking forward to trying it.

    I would be extremely happy with this on the BBB!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bwelsby

    Brian Welsby wrote:

     

    I take it these systemd[1]  boot errors are because the correct kernel modules have not been installed in /usr/lib/modules/

    Hmm..  effectively they're due to systemd trying to do all sorts of unnecessary "I'm-a-resource-hungry-desktop-app" nonesense. A huge chunk of what systemd does could easily be considered a simple waste of precious resources on a small embedded system.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to shabaz

    Me too, when I was in gainfull employment I used nothing but Centos and RHEL. I only got into Debian and Ubuntu because of the R-Pi.

    It looks like a package repository is being built mainly for R-Pi but at least with RH/Centos the package source RPMs are easily available.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    shabaz wrote:

     

    ~/kernel/kernel$ make ARCH=arm CROSS_COMPILE=arm-angstrom-linux-gnueabi- INSTALL_MOD_PATH=$HOME/kernel/kernel/rootfs modules_install

    I'm not sure what it does, I'll try it. Does it create a file system containing the modules that I will need to tftp do you think?

    building and installing (or packaging) a kernel needs you to do a set of things:

     

    1. make menuconfig (or make oldconfig if you have an appropriate .config already)
    2. make  (compile everything)
    3. make install (install just the kernel, but be careful with this as it may not do what you expect)
    4. make modules_install (install the modules)
    5. make headers_install (install the development headers into /usr/include/linux)

     

    and possibly clone git://git.kernel.org/pub/scm/linux/kernel/git/firmware/linux-firmware.git or parts of it into /lib/firmware

     

    The obvious problems start when you find out that by default, modules get installed into /lib/modules/<KERNELVER> on the build system. Largely this isn't what you want, especially if you're cross compiling (or packaging the result for a system that's not the build system).

     

    There are other complications if you use the available features to seperate the source directory from the build directory so that you can use the same source for many different targets.

     

    INSTALL_MOD_PATH lets you specify a prefix for the install location which means you can set it to something like /tmp/kernel-3.8.13 and your files end up under that directory instead of trampling all over the build system.

    You can also do:

    make headers_install INSTALL_HDR_PATH=/tmp/kernel-3.8.13/usr

    in order to get the headers without trashing your build system.

     

    What I do is to install all of the eventual kernel files into a temp directory, then create a tarball of that. This lets me compile once, and deploy that tarball to many different systems.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Brian Welsby wrote:

     

    I take it these systemd[1]  boot errors are because the correct kernel modules have not been installed in /usr/lib/modules/

    Hmm..  effectively they're due to systemd trying to do all sorts of unnecessary "I'm-a-resource-hungry-desktop-app" nonesense. A huge chunk of what systemd does could easily be considered a simple waste of precious resources on a small embedded system.

    Yes one of the first things I did with Angstrom was use systemctl to disable/remove unnecessary stuff,  just like MS Windoze really .. (sorry for swearing).

    I too hate systemd.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to e14 Contributor

    selsinork wrote:

    directory instead of trampling all over the build system.

    You can also do:

    make headers_install INSTALL_HDR_PATH=/tmp/kernel-3.8.13/usr
    in order to get the headers without trashing your build system.

     

     

    I always make sure I am not logged in as root or with root privs when cross compiling kernels, I made that mistake once.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bwelsby

    Brian Welsby wrote:

     

    I always make sure I am not logged in as root or with root privs when cross compiling kernels, I made that mistake once.

    building kernels isn't really that hard, unfortunately there's many traps and assumptions in the process that can catch out the unwary..

     

    like you'll always be building for the running system, and that /lib/modules/'uname -r'/build is a sensible place to be looking for anything.

     

    I almost always do build as root, partially for historic reasons, partially because that's how my build machines are setup. I do have a set of build scripts that have been carefully crafted to deal with the pitfalls though and I currently build about 15 target variations from a single source tree using the O= feature to create seperate build directories. So it's important to get it right or else I'd end up in all sorts of trouble very quickly.

     

    The Kbuild system has lots of useful options to make your life easier, sadly they're not well understood as evidenced by the uname -r hackery that seems all to common.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bwelsby

    Brian Welsby wrote:

     

    I always make sure I am not logged in as root or with root privs when cross compiling kernels, I made that mistake once.

    building kernels isn't really that hard, unfortunately there's many traps and assumptions in the process that can catch out the unwary..

     

    like you'll always be building for the running system, and that /lib/modules/'uname -r'/build is a sensible place to be looking for anything.

     

    I almost always do build as root, partially for historic reasons, partially because that's how my build machines are setup. I do have a set of build scripts that have been carefully crafted to deal with the pitfalls though and I currently build about 15 target variations from a single source tree using the O= feature to create seperate build directories. So it's important to get it right or else I'd end up in all sorts of trouble very quickly.

     

    The Kbuild system has lots of useful options to make your life easier, sadly they're not well understood as evidenced by the uname -r hackery that seems all to common.