Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum BBB - Building the Linux Kernel
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 59 subscribers
  • Views 5571 views
  • Users 0 members are here
  • beaglebone_black
  • bbb
  • bb_black
  • beagle_bone_black
Related

BBB - Building the Linux Kernel

shabaz
shabaz over 13 years ago

Hi, I've added a step-by-step guide to building the Linux kernel for the BBB at the elinux wiki, so we can all edit it to improve the process. Particular thanks to Vlad Ungureanu for helping with debugging.

 

It took a while to get the steps ironed out. I still need to figure out how how to build the rest of the file system (there is a file system supplied

with TI's SDK) and getting it NFS-mounted.

 

These are the current steps documented (hopefully these links work):

 

  • 1 Beaglebone Black – Building Images
    • 1.1 Introduction
      • 1.1.1 Is it difficult?
      • 1.1.2 What is required?
      • 1.1.3 What steps are involved?
    • 1.2 Getting started - Folders
    • 1.3 Installing the build tools (toolchain)
      • 1.3.1 3. 1 Compile tools
      • 1.3.2 3.2 Some miscellaneous items
      • 1.3.3 3.3 U-boot
    • 1.4 Downloading and building the Linux Kernel
    • 1.5 Transferring the image to the BBB via TFTP
    • 1.6 Appendix: Installing and configuring the TFTP server
    • 1.7 Appendix: Installing and using Minicom
  • Sign in to reply
  • Cancel

Top Replies

  • bwelsby
    bwelsby over 13 years ago in reply to shabaz +1
    If you want a RHL/Centos style distro then you could try installing this root file system to go with your kernel from http://www.redsleeve.org/ no idea if it will work (in theory it should) but I will…
  • bwelsby
    bwelsby over 13 years ago in reply to shabaz +1
    Me too, when I was in gainfull employment I used nothing but Centos and RHEL. I only got into Debian and Ubuntu because of the R-Pi. It looks like a package repository is being built mainly for R-Pi but…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz +1
    shabaz wrote: ~/kernel/kernel$ make ARCH=arm CROSS_COMPILE=arm-angstrom-linux-gnueabi- INSTALL_MOD_PATH=$HOME/kernel/kernel/rootfs modules_install I'm not sure what it does, I'll try it. Does it create…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi Shabaz,

    Thank you for your set-by-set post. I like it much, but I faild on step

    Transferring the image to the BBB via TFTP

     

    When I enter

    tftp 0x80200000 uImage-BBB

    I have follwoing info

     

    U-Boot# tftp 0x80200000 uImage-BBB

    link up on port 0, speed 100, full duplex

    Using cpsw device

    TFTP from server 192.168.111.189; our IP address is 192.168.111.131

    Filename 'uImage-BBB'.

    Load address: 0x80200000

    Loading: T T T T T T T T T T T T T T T T T T T T

    Retry count exceeded; starting again

    using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in

    MAC c8:a0:30:b8:ac:84

    HOST MAC de:ad:be:af:00:00

    RNDIS ready

    ERROR: The remote end did not respond in time.

    at ether.c:2395/usb_eth_init()

    link up on port 0, speed 100, full duplex

     

    than repeat and repeat again utill I kill it.

    I have check tftp server and seems work. My host is ubunut 12.04 on a virtualBox.

    Do you have any idea how I should fix this issue? Thank you

     

    Joe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi Joe,

     

    I did once see that output, I think that might mean that either a firewall is blocking TFTP, or maybe the TFTP server folder (from where it will serve the file) is different to the folder where the image is placed. I'm not familiar with Ubuntu (it may come with a different TFTP server) so it may be worth double-checking what the default TFTP folder is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi Joe,

     

    I did once see that output, I think that might mean that either a firewall is blocking TFTP, or maybe the TFTP server folder (from where it will serve the file) is different to the folder where the image is placed. I'm not familiar with Ubuntu (it may come with a different TFTP server) so it may be worth double-checking what the default TFTP folder is.