Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum BBB - Building the Linux Kernel
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 59 subscribers
  • Views 5538 views
  • Users 0 members are here
  • beaglebone_black
  • bbb
  • bb_black
  • beagle_bone_black
Related

BBB - Building the Linux Kernel

shabaz
shabaz over 13 years ago

Hi, I've added a step-by-step guide to building the Linux kernel for the BBB at the elinux wiki, so we can all edit it to improve the process. Particular thanks to Vlad Ungureanu for helping with debugging.

 

It took a while to get the steps ironed out. I still need to figure out how how to build the rest of the file system (there is a file system supplied

with TI's SDK) and getting it NFS-mounted.

 

These are the current steps documented (hopefully these links work):

 

  • 1 Beaglebone Black – Building Images
    • 1.1 Introduction
      • 1.1.1 Is it difficult?
      • 1.1.2 What is required?
      • 1.1.3 What steps are involved?
    • 1.2 Getting started - Folders
    • 1.3 Installing the build tools (toolchain)
      • 1.3.1 3. 1 Compile tools
      • 1.3.2 3.2 Some miscellaneous items
      • 1.3.3 3.3 U-boot
    • 1.4 Downloading and building the Linux Kernel
    • 1.5 Transferring the image to the BBB via TFTP
    • 1.6 Appendix: Installing and configuring the TFTP server
    • 1.7 Appendix: Installing and using Minicom
  • Sign in to reply
  • Cancel

Top Replies

  • bwelsby
    bwelsby over 13 years ago in reply to shabaz +1
    If you want a RHL/Centos style distro then you could try installing this root file system to go with your kernel from http://www.redsleeve.org/ no idea if it will work (in theory it should) but I will…
  • bwelsby
    bwelsby over 13 years ago in reply to shabaz +1
    Me too, when I was in gainfull employment I used nothing but Centos and RHEL. I only got into Debian and Ubuntu because of the R-Pi. It looks like a package repository is being built mainly for R-Pi but…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz +1
    shabaz wrote: ~/kernel/kernel$ make ARCH=arm CROSS_COMPILE=arm-angstrom-linux-gnueabi- INSTALL_MOD_PATH=$HOME/kernel/kernel/rootfs modules_install I'm not sure what it does, I'll try it. Does it create…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi,

     

    Really sorry, I am quite new and I spent several days traying a lot of things. First of all, my goal is update new kernel in my beaglebone black.

     

    I followed this procedure, Building BBB Kernel - eLinux.org , without any problem until "Start up minicom, and power up the BBB; quickly press space repeatedly to stop it at the u-boot prompt."

    I don't know how to get u-boot prompt. I bougth a uSD card and followed plenty of procedures (i.e. BeagleBone Black - Linux on ARM - eewiki) but i can not get it.

     

    I followed the procedures to run an angstron image from sd, but always got angstom prompt instead of u-boot propt.

    I tryyes as well to copy MLO, u-boot.img into boot partition of uSD, but when I connect the usb 3 leds (USR0:2) turn on and keep this status always. I wonder if maybe i need a serial cable (http://es.farnell.com/ftdi/ttl-232r-3v3/cable-usb-to-ttl-level-serial-conv/dp/1329311) to do this or i can get u-boot prompt directly from usb

     

    I am using a ubuntu virtual machine to do everything.

     

    Could u help me a little bit with this

     

    really sorry ffor thinconeniences

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi Ignacio,

     

    I'm sorry I didn't mention it in the text, but yes that bit used a serial cable. I don't believe it is possible in any other way, because the USB won't be running at that stage. The cable you refer to will work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    best to ignore the usb otg port altogether IMHO.  anything presented through that will only be visible after angstrom is fully booted up and has chance to load and configure the driver from an init-script. Proper serial cable connected to J1 is the only way to get to u-boot prompt.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    best to ignore the usb otg port altogether IMHO.  anything presented through that will only be visible after angstrom is fully booted up and has chance to load and configure the driver from an init-script. Proper serial cable connected to J1 is the only way to get to u-boot prompt.