Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Google Go on ARM
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 59 subscribers
  • Views 3957 views
  • Users 0 members are here
  • debian
  • bbb
  • go
  • rasperry_pi
  • golang
  • arm
Related

Google Go on ARM

morgaine
morgaine over 13 years ago

Ealier today, selsinork wrote in another thread (new one here owing to my change of topic):

selsinork wrote:

 

Interestingly,  it's not so long ago that x86 systems were far less capable in terms of  memory, storage and likely CPU than today's ARM systems, yet were  perfectly capable of compiling everything required natively. How quickly  we forget, and how quickly we bloat the software with unnecessary junk  to the point this is no longer true.

That is so very true!!!

 

Software technology needs occasional revolutions too, just like society, to remove layers of accreted crud.  This happens so rarely in computing alas that we're up to our eyeballs in it and barely keeping our heads clear.  It is so rare that I'd like to highlight one relatively recent instance of it, although it is admittedly a revolution with a small 'r'  as it hasn't captured much mindshare in the computing industry.  It's the programming language Google Go.

 

It's not the Go language syntax nor semantics that are revolutionary,  although it is nice enough in both respects and has lots of very effective features especially for concurrent programming.  What is revolutionary about it is its implementation meme, which renouces the idea that building software is divorced from language definition and is performed by third party tools ("make" and its many equivalents in the commandline and IDE worlds) with limited knowledge of the language beyond syntax.  That almost universally prevalent idea has slowed down system building to a crawl right across the world of computing, and it's almost single-handedly reponsible for the problem you described.  (I'm referring to build time only here.)

 

Instead, Go provides integrated build tools and a software construction meme in which to compile a module requires looking only at its immediate dependencies, no further.  In other words, if module A is dependent on B, and B is dependent on C, then to compile A does not require looking at C.  (No explosion of header file lookups.)  Extrapolate this to complex systems with many layers of dependency in breadth and in which each dependency is itself dependent on multiple layers of dependency in depth, and as you can imagine, Go application building can be literally orders of magnitude faster than in most of the languages in common use today.  Many compiles are pretty much instantaneous despite having lots of dependencies.

 

That's "revolutionary" of the kind that removes decades of accumulated crud which has slowed down our systems to a crawl.  It's worth spreading the word about it.  Oh, and it works on ARM, not as efficiently as on x86 yet but it's improving all the time.  I think we should be using Go very widely for as much as possible outside the kernel.

 

Just today on one of my BBB's with Debian installed:

debian@bbb:#  apt-get install golang

...

Need to get 21.9 MB of archives.
After this operation, 81.4 MB of additional disk space will be used.

...

debian@bbb:$  go version

go version go1.0.2

debian@bbb:$  vi hello.go

debian@bbb:$  cat hello.go

package main

 

import "fmt"

 

func main() {
        fmt.Println("Hello, World!")
}

debian@bbb:$  go build hello.go

debian@bbb:$  ./hello

Hello, World!

debian@bbb:$

Viva la revolucion!  image

 

More seriously, it still has a long way to go in a few areas (integration/interoperation is one), but I see very good things ahead for Go.  I recommend that engineers add it to their toolbox and gradually expand their use over time.  Expect huge reductions in crud / time gains on large projects.

 

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine +1
    Morgaine Dinova wrote: The result isn't in dispute. Anyone can experience it for themselves The result is rarely in dispute. At least not by anyone willing to do some simple comparisons. History, however…
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor +1
    selsinork wrote: History, however, is littered with cases of the inferior choice 'winning'. VHS vs Betamax ? RPi vs * ? Yeah, but fortunately we can leave the discussions about "winning" to the respective…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    That almost universally prevalent idea has slowed down system building to a crawl right across the world of computing, and it's almost single-handedly reponsible for the problem you described.  (I'm referring to build time only here.)

    Actually, C has the nice feature that compilations can be done in parallel,

    using -j or --jobs, so having a multi-core machine can speed up compilation nicely.

    I think in order to have Go's transitive compilation independence, your data structures

    need to (implicitly) use a lot more indirection, so you pay a run-time performance penalty,

    although I have not looked at Go closely.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    That's not a C feature, it's a feature of make:

    make  -j [jobs]  --jobs[=jobs]

    Make knows almost nothing at all about C, so if you've added the -j option to its compilation flags it'll merrily kick off concurrent builds for anything that the Makefile hasn't specifically ordered through sequential dependencies.  The most common candidate is to build concurrently all the .o files listed on the RHS of a target, but it does so without understanding why, ie. merely because its Makefile has been configured that way.

     

    And what's worse, those many instances of the C compiler that have been kicked off by make will all process the same C header files repeatedly and independently, only slightly held back from total insanity by the magic #ifdef-#include-#endif incantations in the .h headers which are added manually by programmers, not a feature of the language system.

     

    It's very different in Go.  The "go" build utility doesn't obey a configuration file at all, and instead it digs out the dependency information directly from the module being compiled.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    No, when compiling A then Go doesn't need to consider C.  C is a dependency for B, and therefore any change in C means that B is no longer up to date, so the "go" build tool will rebuild B first before it starts on A.  Then when compiling A it will examine only B, not C.

     

    You are describing how languages like Ada have managed dependencies for 30+ years.

    Is that what you mean by revolutionary?

     

    btw, Kuhn teaches that in order to have a scientific revolution you first need to have

    a scientific paradigm, and I think he would consider computer science to be pre paradigm.

    You don't see anyone suggesting to do scientific experiments in computer science where

    for example you might implement a large project in two different programming languages to

    see which works better, or teach two sections of an introductory programming class, using

    two different languages, to see which section does better.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    coder27 wrote:

    To avoid that transitive dependency, you have to access structs indirectly.

    and you need a pile of metadata to do that - I guess that's what you meant when you talked about a run time performance penalty ?

     

    exactly.  Although I think I initially misunderstood what Morgaine was saying about Go not having transitive dependencies.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    coder27 wrote:

     

    ... You don't see anyone suggesting to ... teach two sections of an introductory programming class, using

    two different languages, to see which section does better.

    I suspect the result will be that whichever has the better teacher who is more enthusiastic about the language being taught will do better.  For example, I'd do better teaching ASM than C++ because I love the simplicity and hands-on character of ASM versus the complexities of C++.  JMO/YMMV.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    If you're hung up on the word "revolution" I'll withdraw it, since it's not essential to my point.

     

    My point was to answer selsinork's correct observation that our computing systems have become bloated with so much unnecessary cruft that they behave like machines of yesteryear despite being far more capable on spec.  I offered Go as a very practical example of the removal of accumulated cruft, since it compiles extremely fast by combining an effective module system that eliminates deep traversals of dependencies and a language-aware build tool that uses knowledge of that module structure to reduce compilations to a minimum, without manual configuration.

     

    The result isn't in dispute.  Anyone can experience it for themselves by compiling the entire Go compiler suite in a few seconds and the entire modules library in a small number of minutes.  The gcc equivalents (if an analogous set were to be constructed as fairly as possible) would take many hours to build.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem
    I suspect the result will be that whichever has the better teacher who is more enthusiastic about the language being taught will do better.  For example, I'd do better teaching ASM than C++ because I love the simplicity and hands-on character of ASM versus the complexities of C++.  JMO/YMMV.

     

    Agreed.  That's why it isn't done, because everyone would dismiss the results as being biased

    by uncontrolled factors.   Similarly nobody suggests teaching programming with a class full of

    Windows PC compared to a class full of RPi's to test the theory that RPi's make for better learning,

    before proposing to buy millions of RPi's.

     

    But that's what sets apart pseudo science from real experimental science, where you routinely do

    experiments that control for extraneous factors to some degree of statistical significance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    The result isn't in dispute.  Anyone can experience it for themselves by compiling the entire Go compiler suite in a few seconds and the entire modules library in a small number of minutes.  The gcc equivalents (if an analogous set were to be constructed as fairly as possible) would take many hours to build.

    When comparing the numbers, I'd want to know how much this is due to the amount of source code.  Since Go is fairly new, it probably hasn't accumulated anywhere near the number of libraries that GCC has.  Also, what's the state of optimization in both cases?  I would think that a lot of GCC code is optimization and code generation for myriad platforms -- how does Go compare?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    The result isn't in dispute.  Anyone can experience it for themselves

    The result is rarely in dispute. At least not by anyone willing to do some simple comparisons. 

     

    History, however, is littered with cases of the inferior choice 'winning'.

    VHS vs Betamax ?   RPi vs * ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    When comparing the numbers, I'd want to know how much this is due to the amount of source code.  Since Go is fairly new, it probably hasn't accumulated anywhere near the number of libraries that GCC has.

    I tried to normalize for that difference, by saying "if an analogous set were to be constructed as fairly as possible".  Admittedly it doesn't really address the matter.  I suspect it's not really feasible to set up an accurate comparison.  Even if we tried to achieve feature parity by extra work on the Go libraries, someone would probably complain "Look, you used a more optimum algorithm there", and they might even be right.  The only thing that's certain is that compilation is fast.  The rest can probably be debated until the cows come home, and not wrongly.

     

    Also, what's the state of optimization in both cases?  I would think that a lot of GCC code is optimization and code generation for myriad platforms -- how does Go compare?

    It's a very good point, but from Go's lack of header files one instantly knows that the type of conditional compilation one finds in C systems to adapt code to different platforms just doesn't exist in Go.  I've read at least one article about how Go addresses this issue, and it seems to be through using different code trees for different platforms (Go has a concept of workspaces which are similar to include paths in C), so on each different platform you only build the modules written for that platform.  This isn't a problem, although it does require the engineer to split modules into platform-dependent and platform-independent parts.  That's good practice anyway though.

     

    That said, Go supports only a tiny number of platforms compared to the awesome tour de force that is gcc, so I'm certain that it has not encountered many of the problems that gcc has not only encountered but solved.  It's still early days for Go.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    History, however, is littered with cases of the inferior choice 'winning'. VHS vs Betamax ?   RPi vs * ?

     

    Yeah, but fortunately we can leave the discussions about "winning" to the respective teams of fanbois, and as engineers we'll just add our shiny new tool to our toolbox regardless.  From where I'm sitting right now I see a stack of Betamax tapes on the shelf, and there's a VHS box in the A/V rack.  I have Pi and BBB and Olimex and Arduino boards and many others, and they all have their niche.

     

    Hmmmm, this screwdriver really wins the contest against this hammer.  Oh wait, no, this chainsaw is absolutely FTW, I'm sure to assemble my IKEA furniture fastest with it ! image

     

    Perhaps IKEA furniture really is best assembled with a chainsaw, but that wasn't the point. image

     

    (Yes I know I'm preaching to the converted, heh)

     

    Not saying we should ignore Go either. but that's part of the problem, which ones to pick ?

     

    Because there are only 48 hours in the day, my approach is to gain just a small amount of practical acquaintance with each new tool that comes along so that the memory stays and the unexpressed fear of the unknown is defused, and then spend much longer reading up thoroughly on its background and features and people's experiences of its application.

     

    Engineers are not experts at everything, but they're damn good at knowing what tool might be worth trying if they've been exposed to it before --- the more breadth of exposure the better.  And only at that point do you allocate priceless time to dive in deep.

     

    (Conversely, without that prior exposure they will never know that they would have made a different choice if they had been suitably informed, and that's deeply unfortunate.)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Perhaps IKEA furniture really is best assembled with a chainsaw, but that wasn't the point. image

    Give them some credit, they give you enough extra bits of metal and spare allen keys to build your own chainsaw.  My only ikea furniture is two desks and I swear I'll never need to buy allan keys again until the end of time image

     

    Way to go on thread drift BTW image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Perhaps IKEA furniture really is best assembled with a chainsaw, but that wasn't the point. image

    Give them some credit, they give you enough extra bits of metal and spare allen keys to build your own chainsaw.  My only ikea furniture is two desks and I swear I'll never need to buy allan keys again until the end of time image

     

    Way to go on thread drift BTW image