Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Intel to give away 50,000 Arduino-friendly computers based on 400MHz Quark SoC
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 63 subscribers
  • Views 4755 views
  • Users 0 members are here
Related

Intel to give away 50,000 Arduino-friendly computers based on 400MHz Quark SoC

e14 Contributor
e14 Contributor over 13 years ago

http://www.theregister.co.uk/2013/10/03/intel_seeks_slice_of_pi_with_arduinofriendly_galileo_board_computer/

http://www.intel.com/content/www/us/en/do-it-yourself/galileo-maker-quark-board.html

http://download.intel.com/support/galileo/Galileo_Datasheet_329681.pdf

https://communities.intel.com/docs/DOC-21828

http://www.anandtech.com/show/7387/intel-announces-galileo-quark-based-arduino-compatible-developer-board

 

ISA: 32-bit x86

RAM:  256MB  (SoC can support up to 2GB)

DImensions:  4.2 inches long by 2.8 inches wide.

fab: 32nm

SoC package: Flip-Chip Ball Grid Array (FCBGA) package with 393 solder

                       balls with 0.593 mm ball pitch. The package dimensions are 15mm x 15mm.

L1 cache: 16Kbyte shared I/D

 

Power supply:  3A at 5V

Price:  Under $60

Availability: December, 2013

 

Development OS Support (see Note below):

  • Linux Ubuntu 12.04* (32-bit & 64-bit)
  • Mac OS X version 10.8.5* (also tested on Mac OS X 10.6.8, 10.7.5, and 10.9* developer preview)
  • Windows 7* (32-bit & 64-bit) and Windows 8*

 

I/O:

  • A full sized mini-PCI Express slot,
  • 100Mb Ethernet port,
  • Micro-SD slot,
  • RS-232 serial port,
  • USB Host port,
  • USB Client port,
  • 8MByte NOR flash.

 

NOTE:  don't understand how 32-bit ISA claims to support 64-bit OSs.

added:  Maybe these OS's aren't actually running on the board itself, but are

intended to run on a connected host computer. 

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 13 years ago in reply to morgaine +1
    I have some special research tools that I build that are still at work on my MS DOS computers. Yes I still have some up and running for data collection purposes. If the new board supports the 8086 instruction…
  • morgaine
    morgaine over 13 years ago in reply to DAB +1
    DAB wrote: Plus I was never into this throw away society. My German roots run deep and we try to keep everything running as long as they can still do the job. +1. I like the philosophy you express above…
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor +1
    Although true, most upgrades aren't made because the user will benefit from improved efficiency, but because the old gear is no longer compatible with new product or else is portrayed by marketing as no…
Parents
  • johnbeetem
    johnbeetem over 13 years ago

    All right, why is it called a Galileo board if it has a Quark SoC?  They should call it a James Joyce or a Finnegan board image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 13 years ago

    All right, why is it called a Galileo board if it has a Quark SoC?  They should call it a James Joyce or a Finnegan board image