Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Intel to give away 50,000 Arduino-friendly computers based on 400MHz Quark SoC
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 63 subscribers
  • Views 4741 views
  • Users 0 members are here
Related

Intel to give away 50,000 Arduino-friendly computers based on 400MHz Quark SoC

e14 Contributor
e14 Contributor over 13 years ago

http://www.theregister.co.uk/2013/10/03/intel_seeks_slice_of_pi_with_arduinofriendly_galileo_board_computer/

http://www.intel.com/content/www/us/en/do-it-yourself/galileo-maker-quark-board.html

http://download.intel.com/support/galileo/Galileo_Datasheet_329681.pdf

https://communities.intel.com/docs/DOC-21828

http://www.anandtech.com/show/7387/intel-announces-galileo-quark-based-arduino-compatible-developer-board

 

ISA: 32-bit x86

RAM:  256MB  (SoC can support up to 2GB)

DImensions:  4.2 inches long by 2.8 inches wide.

fab: 32nm

SoC package: Flip-Chip Ball Grid Array (FCBGA) package with 393 solder

                       balls with 0.593 mm ball pitch. The package dimensions are 15mm x 15mm.

L1 cache: 16Kbyte shared I/D

 

Power supply:  3A at 5V

Price:  Under $60

Availability: December, 2013

 

Development OS Support (see Note below):

  • Linux Ubuntu 12.04* (32-bit & 64-bit)
  • Mac OS X version 10.8.5* (also tested on Mac OS X 10.6.8, 10.7.5, and 10.9* developer preview)
  • Windows 7* (32-bit & 64-bit) and Windows 8*

 

I/O:

  • A full sized mini-PCI Express slot,
  • 100Mb Ethernet port,
  • Micro-SD slot,
  • RS-232 serial port,
  • USB Host port,
  • USB Client port,
  • 8MByte NOR flash.

 

NOTE:  don't understand how 32-bit ISA claims to support 64-bit OSs.

added:  Maybe these OS's aren't actually running on the board itself, but are

intended to run on a connected host computer. 

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 13 years ago in reply to morgaine +1
    I have some special research tools that I build that are still at work on my MS DOS computers. Yes I still have some up and running for data collection purposes. If the new board supports the 8086 instruction…
  • morgaine
    morgaine over 13 years ago in reply to DAB +1
    DAB wrote: Plus I was never into this throw away society. My German roots run deep and we try to keep everything running as long as they can still do the job. +1. I like the philosophy you express above…
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor +1
    Although true, most upgrades aren't made because the user will benefit from improved efficiency, but because the old gear is no longer compatible with new product or else is portrayed by marketing as no…
Parents
  • DAB
    DAB over 13 years ago

    Very interesting.

     

    I wonder if Element 14 could snag a few for us to test. image

     

    If it is truely 86 compatible, I can see a lot of interesting uses for this new system.

     

    I would definately pay 60 USD for one just to see what I could do with it and to see what legacy software I could run.  I have a few old MS DOS tools that would just scream if I could run them on this fast of a processor set.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to DAB

    DAB wrote:

     

    I have a few old MS DOS tools that would just scream if I could run them on this fast of a processor set.

    It would certainly be interesting to see if DOS could be made to run on some of these new x86 boards, but I suspect it's simply not going to be possible.  The Minnowboard for example has UEFI firmware, not a traditional BIOS. So a lot of the stuff that DOS relies on simply isn't there.  I'm not even sure the hardware would still be capable of supporting it, probably too much has changed in the last 10 years or so.

    Lack of bios support might be solved by something like http://en.wikipedia.org/wiki/SeaBIOS but that could be complex enough on it's own.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to DAB

    DAB wrote:

     

    I have a few old MS DOS tools that would just scream if I could run them on this fast of a processor set.

    It would certainly be interesting to see if DOS could be made to run on some of these new x86 boards, but I suspect it's simply not going to be possible.  The Minnowboard for example has UEFI firmware, not a traditional BIOS. So a lot of the stuff that DOS relies on simply isn't there.  I'm not even sure the hardware would still be capable of supporting it, probably too much has changed in the last 10 years or so.

    Lack of bios support might be solved by something like http://en.wikipedia.org/wiki/SeaBIOS but that could be complex enough on it's own.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • DAB
    DAB over 13 years ago in reply to e14 Contributor

    You are probably correct, but it is something to think about.  Especially as we get more data on the board and the chip.

     

    Time will tell.  Plus if others think running MS DOS type programs on an SBC, they might build up a BIOS for the chip.

     

    I have found that there are a lot of people out there with a lot of time on their hands who like a good challenge.

     

    DAB