Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Intel to give away 50,000 Arduino-friendly computers based on 400MHz Quark SoC
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 63 subscribers
  • Views 4665 views
  • Users 0 members are here
Related

Intel to give away 50,000 Arduino-friendly computers based on 400MHz Quark SoC

e14 Contributor
e14 Contributor over 12 years ago

http://www.theregister.co.uk/2013/10/03/intel_seeks_slice_of_pi_with_arduinofriendly_galileo_board_computer/

http://www.intel.com/content/www/us/en/do-it-yourself/galileo-maker-quark-board.html

http://download.intel.com/support/galileo/Galileo_Datasheet_329681.pdf

https://communities.intel.com/docs/DOC-21828

http://www.anandtech.com/show/7387/intel-announces-galileo-quark-based-arduino-compatible-developer-board

 

ISA: 32-bit x86

RAM:  256MB  (SoC can support up to 2GB)

DImensions:  4.2 inches long by 2.8 inches wide.

fab: 32nm

SoC package: Flip-Chip Ball Grid Array (FCBGA) package with 393 solder

                       balls with 0.593 mm ball pitch. The package dimensions are 15mm x 15mm.

L1 cache: 16Kbyte shared I/D

 

Power supply:  3A at 5V

Price:  Under $60

Availability: December, 2013

 

Development OS Support (see Note below):

  • Linux Ubuntu 12.04* (32-bit & 64-bit)
  • Mac OS X version 10.8.5* (also tested on Mac OS X 10.6.8, 10.7.5, and 10.9* developer preview)
  • Windows 7* (32-bit & 64-bit) and Windows 8*

 

I/O:

  • A full sized mini-PCI Express slot,
  • 100Mb Ethernet port,
  • Micro-SD slot,
  • RS-232 serial port,
  • USB Host port,
  • USB Client port,
  • 8MByte NOR flash.

 

NOTE:  don't understand how 32-bit ISA claims to support 64-bit OSs.

added:  Maybe these OS's aren't actually running on the board itself, but are

intended to run on a connected host computer. 

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 12 years ago in reply to morgaine +1
    I have some special research tools that I build that are still at work on my MS DOS computers. Yes I still have some up and running for data collection purposes. If the new board supports the 8086 instruction…
  • morgaine
    morgaine over 12 years ago in reply to DAB +1
    DAB wrote: Plus I was never into this throw away society. My German roots run deep and we try to keep everything running as long as they can still do the job. +1. I like the philosophy you express above…
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor +1
    Although true, most upgrades aren't made because the user will benefit from improved efficiency, but because the old gear is no longer compatible with new product or else is portrayed by marketing as no…
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    I just found this at LinuxGizmos: Intel tempts IoT hackers with free Galileo SBCs, prizes.

     

    Galileo is now US$80 instead of the earlier quoted "under $60".  I can't tell if Intel has distributed any of the free 50K units to universities.  They have announced plans for a 20-city "road show" at which they'll distribute 5K units, as well as a developer contest.

     

    My impression is that Intel is talking a lot about Galileo and making tentative moves while other development boards are taking over the embedded SBC space.  However, this is JMO -- YMMV.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 12 years ago

    I just found this at LinuxGizmos: Intel tempts IoT hackers with free Galileo SBCs, prizes.

     

    Galileo is now US$80 instead of the earlier quoted "under $60".  I can't tell if Intel has distributed any of the free 50K units to universities.  They have announced plans for a 20-city "road show" at which they'll distribute 5K units, as well as a developer contest.

     

    My impression is that Intel is talking a lot about Galileo and making tentative moves while other development boards are taking over the embedded SBC space.  However, this is JMO -- YMMV.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem

    John Beetem wrote:

    My impression is that Intel is talking a lot about Galileo and making tentative moves while other development boards are taking over the embedded SBC space.  However, this is JMO -- YMMV.

    Agreed. There's still that mini PCIe connector to add some interest, but I don't see any other selling points. Not at $80.  The price simply isn't worth it when there's a $45 BBB available.  Things Like the 30 Euro Olimex Lime make that even more interesting, and I'm not sure x86 is a selling point for something targetting Arduino style gadgets.  Uphill struggle for Intel I think.

    The thing is, I expect Intel could produce something interesting if they could find the will to ditch x86 for things like Galileo