Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Who wants to review a free pcDuino v2?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 66 subscribers
  • Views 2483 views
  • Users 0 members are here
  • sbc
  • single_board_computers
  • pcduino
Related

Who wants to review a free pcDuino v2?

fustini
fustini over 12 years ago

I received a pcDuino v2 with integrated Wi-Fi at Maker Faire New York 2013.  I thought it would be fun to have someone from element14 Community take it for a spin.  Here's my gallery of the board: https://plus.google.com/photos/117542001281850354871/albums/5940327956141042529?banner=pwa

 

I'm going to give this pcDuino v2 for free to a lucky Community member with the request that the winner please write a review (either in the blog here or somewhere else on the web).  It doesn't have to be anything fancy so don't be intimidated.  Sorry, no minors, you must be 18 years of age or older! 

 

To enter, do the following:

 

  • Reply to this post with a short description of why you are interested (1 to 2 sentences is fine)
  • I'll will pick a winner at random on Wednesday, November 6th, at 5pm US CDT.

 

Note: I'm located in Chicago and will ship it for free to the winner using the lowest cost option available.  If the winner is located outside the US, then the winner will be responsible for paying any customs fees or duty that may apply.  I will list the value as $55 USD.

 

 

Cheers,

Drew

http://twitter.com/pdp7

  • Sign in to reply
  • Cancel
Parents
  • bad_boy_y
    bad_boy_y over 12 years ago

    Do you knot if the arduino pin are 3.3v or 5v?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bad_boy_y
    bad_boy_y over 12 years ago

    Do you knot if the arduino pin are 3.3v or 5v?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fustini
    fustini over 12 years ago in reply to bad_boy_y

    I believe it's 3.3V

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 12 years ago in reply to bad_boy_y

    @bad_boy_y do you wish to be entered in the list of names I'll randomly draw from for the  pcDuino?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bad_boy_y
    bad_boy_y over 12 years ago in reply to fustini

    yes I wish I want to try the arduino ready computer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to bad_boy_y

    It's interesting that they say

    Moreover, it has a hardware header interface compatible with Arduino.

    However the pictures suggest the form factor is different. They are pins, rather than female headers, and along one side.

     

     

    Drew's pictures show that V2 version is compatible, so it appears mcmelectronics only have version 1 (which you've linked to)

     

    V2 on the pcDuino website http://www.pcduino.com/?page_id=1618

     

    I struggled to find if the GPIO is 5v or 3v3, but it is only 4mA, rather than the 20mA an Arduino is capable of.

    from here

    1. Here is the list of I/O interfaces on pcDuino board.
    2. 14 digital pins for GPIO: GPIO max out current is 4mA.
    3. One UART RX, one UART TX
    4. Two PWM pins, support up to 24MHz.
    5. Six ADC pins, ADC 0 and ADC 1 are 6 bits resolution, while the rest are 10 bits resolution.
    6. Four SPI pins
    7. Two I2C pins

    This page suggests a level shifter is required Shields

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 12 years ago in reply to mcb1

    Thanks, yeah, I think one of the key difference between v1 and v2 is that v2 had the physical Arduino headers.  The v1 needed some type of adapter board I believe.