Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum OlinuXino LIME vs BBB ?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 59 subscribers
  • Views 3353 views
  • Users 0 members are here
  • olinuxino
Related

OlinuXino LIME vs BBB ?

e14 Contributor
e14 Contributor over 13 years ago

http://olimex.wordpress.com/2013/11/14/a10-olinuxino-lime-eur-30-open-source-hardware-linux-sbc-first-prototypes/

 

Plus points:

Designed to be cased from the outset.

Connectors placed with some thought.

SATA image

 

Downsides:

1.27mm gpio connectors not so easy to use

100Mb/s network

 

At 30 euros with a decent spec that includes sata there's a fair chance it could give the BBB a run for it's money, and it's an obvious RPi killer. Indeed these days the only use I have for the RPi is the camera, so largely don't see it as competitive any more - it's had it's day and did a good job of kick starting competition..

 

There's more than a few of us who would buy the LIME if e14 were to stock them...

 

element14Dave any chance of passing along to your procurement people that we'd really love it it e14 were to offer more of the OlinuXino range ?

  • Sign in to reply
  • Cancel

Top Replies

  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor +2
    selsinork wrote: and here was me thinking you'd been having a quiet word in someones ear Quiet word? He was smacking them over the head with a baseball bat until they submitted! Morgaine.
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine +1
    Morgaine Dinova wrote: I just need the Sabre-Lite to be cheaper! Agreed. However it's a bit of a compromise for me... The cost of one (quad core) SL is equivalent to four-and-a-bit BBB's. So does…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor +1
    I just checked the supplied android image and that sets the DDR3 to 432MHz instead of the 480MHz that the debian image they supply uses. So seems you were right, my particular board isn't happy at 480MHz…
Parents
  • morgaine
    morgaine over 13 years ago

    Excellent board and excellent price!

     

    By the way, I don't think you should list "100Mb/s network" as a Downside, because you titled your thread "LIME vs BBB", and it's not a downside vs BBB since BBB also has the same nominal link speed.

     

    I agree with your intended sentiment of course, that all networking should be gigabit or faster. image

     

    selsinork wrote:

     

     

    element14Dave any chance of passing along to your procurement people that we'd really love it it e14 were to offer more of the OlinuXino range ?

     

    Seconded -- I want to buy several of these, as I did BBBs.  I don't think that there's much hope of it though.  Farnell UK isn't even listing the now-established A20-OLinuXino boards yet (let alone stocking), so LIME probably won't appear until Q2 2014, if then.  Farnell procurement seems to be moving at snails' pace for some reason.  It's so bad that Farnell is beginning to look silly, and I'll have to start looking elsewhere.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Yes, 100Mb/s network is just a general thing.  I've been compiling a lot of software on some of these boards recently and the bits that stand out are that none of them have the memory for me to be able to setup an 8GB ram based tmpfs on /tmp and use that to speed up compiles the way I would on x86, so I'm looking for either decent SATA performance, or gigabit network so that I can nfs mount /tmp to a large ram backed store on another system.

    With the 3.12 kernel, the SL has just become my new favourite build machine, even though it's taken a full year to get there. I'm aiming for a common kernel & userspace across BBB, SL & Cubie2.  It's taken a while, but BBB & SL seem to be getting their acts together and are reasonably close to mainline, the A10/A20 stuff is still way behind with 3.4 kernels even though there's a good community around sunxi.org, hopefully they'll catch up soon.

    Like Ubuntu/Fedora etc, I'm rapidly reaching the conclusion that the critical mass around Cortex A8 class onwards is a good thing and that dropping the RPi and it's ARM11 is the right decision. Final nail in that coffin springs to mind...

     

    If you're still interested in more BBB's, CPC have a modest offer on them from last weeks mailer. Only a couple of quid off, but still... valid to the end of January IIRC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

     

    If you're still interested in more BBB's, CPC have a modest offer on them from last weeks mailer. Only a couple of quid off, but still... valid to the end of January IIRC.

     

    Thanks, I might well do that.  Even when LIME and others start undercutting the BBB, its twin PRUs still make it untouchable for a few special types of realtime applications.  I think it's a big pity that TI and Beagleboard haven't capitalized on that feature a lot more, since it's a high profile product differentiator which competitors cannot easily match.

     

    With the 3.12 kernel, the SL has just become my new favourite build machine, even though it's taken a full year to get there.

    I just need the Sabre-Lite to be cheaper! image

     

    I'm rapidly reaching the conclusion that the critical mass around Cortex A8 class onwards is a good thing and that dropping the RPi and it's ARM11 is the right decision.

     

    Agreed, Cortex-A8 was a game changer.  Even my original Galaxy Tab used a Cortex-A8, and its performance easily handled the requirements of an Android tablet ---it's still working fine today.  A really great ARM core, and a great AM3359 SoC from TI too.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Hi,

     

    just want to make small update: today we assembled LIME with A20 and the result is: A20 Dual Core Cortex-A7 @1Ghz need just 0.14A@5V vs. Single Core Cortex-A8 @1Ghz needs 0.18A i.e. A20 is 30% less power hungry and runs about x1.7 times faster than A10

     

    A20-OLinuXino-LIME update | olimex

     

    when comparing to BBB also note that A10/A20 HDMI is native and supports any resolution up to 2160p while BBB uses converter IC and have limited resolutions, LIME have LiPo charger and can run 30 hours on our 6.6Ah LiPo battery

    and of course the native SATA

     

    Tsvetan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I just need the Sabre-Lite to be cheaper!

    Agreed. However it's a bit of a compromise for me... The cost of one (quad core) SL is equivalent to four-and-a-bit BBB's.  So does the Cortex A9 + now decently performing SATA outweigh setting up distcc + getting everything on nfs?  It's a hard decision..  Now if the cost of one SL got me 5x BBB it'd be different.

     

    The LIME changes things again, that 30 euro price tag suggests I'll get five-and-a-bit of them for the cost of one SL, plus the LIME has SATA while the BBB doesn't.  So for compilation duties the LIME could end up being better than both.

     

    Don't get me wrong, for all sorts of other things the BBB with onboard eMMC can be a better choice. We need to see what the LIME with onboard 4Gb NAND comes in at to pick a winner.  Like you say, the PRUs will decide for certain applications..  For things like my RPi GPS NTP boxes, all I need is one GPIO for PPS, the ability to run ntpd and for it to run reliably forever.  The recent nonesense with an RPi kernel update making a few of mine unbootable due to no longer liking the previously working SD cards is the sort of thing that makes you think that onboard eMMC or NAND in the case of LIME are good solutions for reliability - they're bound to get tested!

     

    Been a while since I posted any pics of this, but the collection is growing, I'll be needing to build the expansion soon image

    image

    Each carrier looks something like this:

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Tsvetan,

     

    Your A20 LIME looks really interesting. I have an A20 based Cubieboard2 and have some issues with the kernel locking up randomly after multiple days. I suspect it's simply a case of the sunxi guys needing to get a bit more of the A20 kernel sorted out, but once that happens I'm certainly looking forward to more A20 based boards.

     

    Since you're working for Olimex, I don't suppose you can tell us if e14 will become distributors for your A20 boards as they have for some of the other OlinuXino boards ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    Tsvetan Usunov wrote:

     

    Hi,

     

    just want to make small update: today we assembled LIME with A20 and the result is: A20 Dual Core Cortex-A7 @1Ghz need just 0.14A@5V vs. Single Core Cortex-A8 @1Ghz needs 0.18A i.e. A20 is 30% less power hungry and runs about x1.7 times faster than A10

     

    A20-OLinuXino-LIME update | olimex

     

    when comparing to BBB also note that A10/A20 HDMI is native and supports any resolution up to 2160p while BBB uses converter IC and have limited resolutions, LIME have LiPo charger and can run 30 hours on our 6.6Ah LiPo battery

    and of course the native SATA

    That's excellent news, Tsvetan! image

     

    You're going to have a big seller on your hands with LIME, and I'll definitely be helping to exhaust your stocks. image

     

    The lower power consumed by A20 attracts me a lot, because I'll be using the LiPo facility as a 2nd stage UPS and so operating time under backup power will improve too.  It probably runs cooler as well, which is always a good thing.  And dual cores can't hurt even if the application doesn't need them.

     

    But I'll be getting a few A10 LIME anyway, since that's coming out first.  Can't wait! imageimageimage

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    Tsvetan Usunov wrote:

     

    Hi,

     

    just want to make small update: today we assembled LIME with A20 and the result is: A20 Dual Core Cortex-A7 @1Ghz need just 0.14A@5V vs. Single Core Cortex-A8 @1Ghz needs 0.18A i.e. A20 is 30% less power hungry and runs about x1.7 times faster than A10

     

    A20-OLinuXino-LIME update | olimex

     

    when comparing to BBB also note that A10/A20 HDMI is native and supports any resolution up to 2160p while BBB uses converter IC and have limited resolutions, LIME have LiPo charger and can run 30 hours on our 6.6Ah LiPo battery

    and of course the native SATA

    That's excellent news, Tsvetan! image

     

    You're going to have a big seller on your hands with LIME, and I'll definitely be helping to exhaust your stocks. image

     

    The lower power consumed by A20 attracts me a lot, because I'll be using the LiPo facility as a 2nd stage UPS and so operating time under backup power will improve too.  It probably runs cooler as well, which is always a good thing.  And dual cores can't hurt even if the application doesn't need them.

     

    But I'll be getting a few A10 LIME anyway, since that's coming out first.  Can't wait! imageimageimage

     

    Morgaine.