Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum The future of PRU in TI's SoC evolution
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 59 subscribers
  • Views 4397 views
  • Users 0 members are here
  • cortex-a8
  • pru
  • bbb
  • cortex-a9
  • cortex-a15
  • ti
  • cortex-a7
Related

The future of PRU in TI's SoC evolution

morgaine
morgaine over 12 years ago

The video in Drew's recent blog post about "Maker Mom to demo BeagleBone Black on Chicago's WGN TV morning news" showed the BBB doing what it does so well, fast realtime I/O without CPU intervention, courtesy of its remarkable twin PRUs (Programmable Real-time Units).

 

We've had a lot of discussions about the PRUs on this forum, but that blog got me thinking about their future, how they could be developed further.  There is always room for hardware improvements, more local memory per PRU being clearly desirable and a speed increment always being welcome.  On the software front there are many improvements that could be done in terms of flexible drivers and language support to bring the PRUs into the solution space for more people.

 

Unfortunately, speculating on the bright future possibilities for PRUs then brought to mind a very grim possibility:  that PRUs are seen by TI marketing and product designers not as the exceptional hardware feature and product differentiators that they are, but as irrelevant to future product lines "because nobody is asking for them" or because "nobody else is doing that".  If PRUs were discontinued from TI's future application processor lineup, it wouldn't be the first time that awesome engineering has been scuppered by blinkered business decisions.

 

So, I'll end with some questions and a suggestion:

 

  • If anyone here knows TI's SoC offerings beyond Cortex-A8, did you see PRUs featured in the hardware?  If so, are the PRUs the same as in the BBB's AM3359, or have they evolved further?  Has TI released any relevant information on this issue?
  • Since Drew is in regular contact with Jason Kridner, and perhaps other Element14 staff have knowledge of TI future offerings on a business level as well, could you perhaps inquire for us whether TI's plan is to continue to offer PRUs in future SoCs, or to discontinue the concept, or "no comment" for business reasons, or are they genuinely undecided?

 

From a customer perspective, PRUs can be a very good reason for buying AM335x, but forward-looking engineering decisions involve the existence of a future migration path as well.  If PRUs are end-of-life beyond TI's Cortex-A8-based family, then they're no longer a very appealing feature because not many people are willing to invest much time and effort in a powerful solution that has no future.  I think this is an important question to ask of TI.

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine +2
    Ah, but two things would actually be interesting about the K1: 1. no more porting things to OpenGL ES, you have the full OpenGL at your disposal too. 2. Even though firmly in the binary blob category,…
  • morgaine
    morgaine over 12 years ago in reply to morgaine +1
    morgaine wrote: two Cortex-M4 cores in OMAP5 interface to the dual Cortex-A15 A new competitor in the OMAP5 space has just been released by nVidia, the Tegra K1 featuring quad+1 Cortex-A15 CPU cores…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine +1
    Luc Verhaegen is quite active in the sunxi mailing lists and seemingly uses Olimex boards for development work on Limadriver. Yes, slightly worrying that there appears to be no public progress recently…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Info on the PRU's seems scarce, they seem to have been used in some of the earlier stuff around OMAP 1 and the AM335x 'Sitara'. I'm still not quite clear on where exactly the Sitara sits, it seems to be vaguely equivalent to some level of OMAP, but I'm unsure if it's OMAP 3 or what. Then there's the DaVinci in there somewhere as well and it seems clear that OMAP/Sitara/DaVinci all use somewhat common building blocks.

     

    Looking at OMAP 4/5 they seem to come with Cortex-M* rather than PRU, looking at TI's Sitara processor list Sitara ARM Processor Products | ARM Processors |Texas Instruments it's not obvious what ones contain PRUs so I don't expect it to be easy to work out what other devices might.

     

    I don't pretend to know what the advantages/disadvantages are for PRU vs Cortex-M* but you could in some ways understand going for a common Cortex-A* with Cortex-M* setup if for no other reason than keeping developers in more familiar territory.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I don't pretend to know what the advantages/disadvantages are for PRU vs Cortex-M* but you could in some ways understand going for a common Cortex-A* with Cortex-M* setup if for no other reason than keeping developers in more familiar territory.

     

    That's a good point.  Even though the PRU instruction set is pretty trivial, it might put some ARM-focused people off having to learn another one.  It doesn't seem a solid objection though, not for something that simple.

     

    A related possibility is that the need to provide dedicated tools to support a different instruction set was weighing on TI's mind, since software support is costly.  The PRU assembler is trivial enough, but the maintenance issues change sharply once C and other compilers enter the picture.  Using internal ARM microcontroller cores eliminates that as an issue.

     

    I haven't yet checked how the two Cortex-M4 cores in OMAP5 interface to the dual Cortex-A15, but hopefully it's a high bandwidth interface.  Here for all bed-time readers' delight is a link to TI's 6105-page OMAP543x Technical Reference Manual.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    A related possibility is that the need to provide dedicated tools to support a different instruction set was weighing on TI's mind, since software support is costly.  The PRU assembler is trivial enough, but the maintenance issues change sharply once C and other compilers enter the picture.  Using internal ARM microcontroller cores eliminates that as an issue.

    I wasn't consciously thinking about that, but yes that could make a huge difference. The likelyhood that you can tap into a ready made toolset with no significant investment or support costs needed will no doubt see the beancounters eyes light up image  Even if it's not the correct decision from an engineering standpoint, it could make a lot of sense economically.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

    Here for all bed-time readers' delight is a link to TI's 6105-page OMAP543x Technical Reference Manual.

    bed time reading ?  The bedside table will collapse under the weight image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I haven't yet checked how the two Cortex-M4 cores in OMAP5 interface to the dual Cortex-A15, but hopefully it's a high bandwidth interface.  Here for all bed-time readers' delight is a link to TI's 6105-page OMAP543x Technical Reference Manual.

    Cool!  I had no idea TI had released an OMAP TRM for anything since the BeagleBoard's OMAP 3.  Dual Cortex-A15 -- very nice!  I wonder when (if) there's going to be a BeagleBigDog?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    In the hope that Jason is working on a big OMAP5 BeagleBone for us, here's a suitably big 1920x1200 block diagram extracted from the TRM:

     

    image

     

    The two Cortex-M4 embedded microcontroller cores are shown at 1 o'clock as the "IPU subsystem", and the pathway to them is shown as 64-bit.  So far, so good! image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to morgaine

    morgaine wrote:

     

    two Cortex-M4 cores in OMAP5 interface to the dual Cortex-A15

     

    A new competitor in the OMAP5 space has just been released by nVidia, the Tegra K1 featuring quad+1 Cortex-A15 CPU cores (the "big.LITTLE" approach) plus 192 GPU cores.  The fact that it's marketed as a mobile device (essentially, meaning tablets) constrains both its power consumption and its price, so it may well appear embedded on an SBC or in non-tablet cased products.

     

    Historically though, nVidia doesn't seem to be getting much market share for its Tegra line.  Perhaps it just pitches them at too high a price to attract OEM interest away from the likes of Allwinner.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Ah, but two things would actually be interesting about the K1:

    1. no more porting things to OpenGL ES, you have the full OpenGL at your disposal too.

    2. Even though firmly in the binary blob category, nVidia are fairly good at keeping their GPU driver up to date with mainline kernels, no reason to expect different here.

     

    The combination is a SoC that's not stuck on some ancient vendor kernel and can do most anything a x86 desktop can with nothing more than a straight recompile.  Still, it remains to be seen if it'll be used by anyone. If they make the mistake of no SATA, or network-via-USB it'll be a no-hoper for SBC usage even if it does take off for tablets.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Ah, but two things would actually be interesting about the K1:

    1. no more porting things to OpenGL ES, you have the full OpenGL at your disposal too.

    2. Even though firmly in the binary blob category, nVidia are fairly good at keeping their GPU driver up to date with mainline kernels, no reason to expect different here.

     

    The combination is a SoC that's not stuck on some ancient vendor kernel and can do most anything a x86 desktop can with nothing more than a straight recompile.  Still, it remains to be seen if it'll be used by anyone. If they make the mistake of no SATA, or network-via-USB it'll be a no-hoper for SBC usage even if it does take off for tablets.