Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum [How-to] BB-View on latest Debian
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 142 replies
  • Subscribers 64 subscribers
  • Views 29623 views
  • Users 0 members are here
  • debian
  • embedded_linux
  • bb-view
  • bbb
Related

[How-to] BB-View on latest Debian

compeoree
compeoree over 12 years ago

I thought some others might like to know how to get the BB-View working under the latest Debian beta images.

 

Unfortunately, you are going to have to recompile the Kernel. The video works fine without a recompile (the red/blue swap is easy to fix), but the touchscreen control connections are not the same as the standard TI 4-wire interface. I tried to patch the ti_am335x_tsc.c file, so the changes would be limited to a dts recompile, but I haven't been able to get that working yet (I'm pretty sure it is a state machine / bit assignment issue). But anyway, here are the steps that you need to perform.....

 

Overview

1) Download the necessary files

     a) Robert Nelson's handy tools for compiling the Beaglebone kernel

     b) BB-View source for Angstrom

2) Build the default kernel

3) Patch the Kernel and perform a fast recompile

4) Copy the new kernel to the Beaglebone

5) Edit the xorg.conf file to correct the Red/Blue color swap

6) Revel in the 4 days you just saved image

 

Let's Get Started

I am using Ubuntu 12.04 LTS 64 bit running in a VirtualBox VM to compile the kernel:

Make a new folder called bb-view, this is where our build will happen.

> mkdir bb-view

> cd bb-view

 

Install git, if you haven't already:

> apt-get install git

 

Clone Robert Nelson's linux-dev project locally. Be prepared for a large download (~100 Mb for the cross-compiler and ~700 Mb for the kernel source).

> git clone https://github.com/RobertCNelson/linux-dev.git

 

Change into the new linux-dev folder and select branch/tag that matches the Debian version.

> cd linux-dev

> git checkout 3.8.13-bone37 -b tmp

 

Now we need to build the base image, so our cape drivers folder gets populated. The script will tell you if you need to do or install anything else.

> ./build_kernel.sh

 

Come back in an hour or so.....(You might want to download the Angstrom source from element14 now)

 

Patching the Kernel

Extract two files from the Angstrom source:

> unzip angstrom-source.zip

> tar -zxf bb-black-kernel-3.8.13-bb-view.tar.bz2

> cp ./kernel/kernel/drivers/input/touchscreen/ti_am335x_tsc.c  ~/bb-view/linux-dev/KERNEL/drivers/input/touchscreen/

> cp ./kernel/kernel/firmware/capes/BB-VIEW-LCD7-01-00A0.dts  ~/bb-view/linux-dev/KERNEL/firmware/capes/

 

Now we need to let the compiler know that we want to add the firmware to the build:

> nano   ~/bb-view/linux-dev/KERNEL/firmware/Makefile

 

Add the following line somewhere near line 192 (CTRL-C will display current cursor position):

BB-VIEW-LCD7-01-00A0.dtbo \

 

Don't forget the trailing backslash....it is important. Now save and exit by doing CTRL-O, Enter, CTRL-X.

Change back to the linux-dev root folder:

> cd   ~/bb-view/linux-dev

 

Now issue the kernel rebuild command, this won't take very long at all:

> ./tools/rebuild.sh

 

 

Copy Kernel to BBB

The following instructions assume that you already have the Debian beta installed and booted up on the BBB.

The easiest way is to copy the files over the network, via the 'scp' command:

> scp   ~/bb-view/linux-dev/deploy/3.8.13-bone37.zImage   debian@192.168.7.2:/home/debian

Replace debian (both instances) with the username you are running on the BBB and 192.168.7.2 with the IP address of the BBB.

 

Now log into the BBB and copy the kernel image to the boot partition:

> ssh debian@192.168.7.2

bbb>  sudo cp 3.8.13-bone37.zImage   /boot/uboot/zImage

 

We need to do one more thing before the LCD will work. Since the cape doesn't have an EEPROM, we need to black-list the HDMI drivers and force-load the BB-VIEW drivers in the boot command file:

bbb>  sudo  nano  /boot/uboot/uEnv.txt

 

Find the "optargs" line and edit it to be:

optargs=capemgr.disable_partno=BB-BONELT-HDMI,BB-BONELT-HDMIN  capemgr.enable_partno=BB-VIEW-LCD7-01

Notice that the preceding "#" has been removed. You don't want to disable BB-BONE-EMMC-2G, or you won't be able to boot from eMMC.

Now save and exit by doing CTRL-O, Enter, CTRL-X.

 

Reboot the BBB and the LCD should now work....except the blue and red are reversed.

 

Fixing Red/Blue Color Swap

This is due to errata in the TI AM335x processor when switching between 16 and 24 bit video modes. To fix this, we must first find the name of our screen:

> ssh debian@192.168.7.2

bbb> cat  /var/log/Xorg.0.log  |  grep  screen

Mine was "Builtin Default fbdev Screen 0"

 

Now we edit our X configuration file:

bbb> sudo nano  /usr/share/X11/xorg.conf.d/10-evdev.conf

 

and add a "Screen" section at the end of the file:

Section "Screen"

        Identifier "Builtin Default fbdev Screen 0"

        Monitor "Configured Monitor"

        Device "Configured Video Device"

        DefaultDepth 24

EndSection

Save and exit by doing CTRL-O, Enter, CTRL-X.

Reboot and enjoy!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    Hello selsinork, "Which kernel version are you using ?" I use the 3.8. "Did you apply the patch Louis posted ?" I rebuild the kernel with Louis' edits in the "4. Re:[How-to] BB-View on latest Debian" message…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    Ok, so with the overlay loaded then the touch screen driver should be able to work. You can check the proper device using 'evtest' like this: root@lcd:~/evtest# ./evtest No device specified, trying to…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    Interesting. I seem to remember that one of the LEDs on the cape was configured as heartbeat. Perhaps that was the TI-SDK image then as looking at the overlay files I see: gpio-leds-cape-lcd { compatible…
Parents
  • mao84
    mao84 over 12 years ago

    Hi Louis,

     

    First of all, thank you for this exhaustive manual on how to make the BB-view work with Debian! That's a great job and thanks to folks like you the youngsters can discover the whole new world of embedded Linux application.

     

    There's one issue I've got - after patching the kernel, the board is not recognized by PC via USB by its IP address anymore. I'm running Ubuntu 12.04 LTS. After re-flashing the BBB back with original Debian image, everything turns normal, i.e. PC recognizes it and one can access the board by 192.168.2.7. I suppose the problem may be in the configuration used for the kernel assembly - ethernet via USB support is not enabled or something like that. Can you please verify this point or maybe I'm doing something wrong?

     

    Thanks and Regards,

    Mao

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • compeoree
    compeoree over 12 years ago in reply to mao84

    You're welcome Mao,

     

    I can't say for sure, as I don't use the USB Ethernet, so I have not verified its operation. You may want to search for gadget or RNDIS services.

     

    Did you modify any of the Kernel configuration? I did not.

     

    Are you only replacing files in the /boot/uboot folder, or others too?

     

    You might run 'systemctl | grep usb' to see if you get something like this:

    debian@beaglebone:~$ systemctl | grep usb

    sys-devi...et-usb0.device loaded active plugged       /sys/devices/ocp.3/47400000.usb/musb-hdrc.0.auto/gadget/net/usb0

    sys-devi...-ttyGS0.device loaded active plugged       /sys/devices/ocp.3/47400000.usb/musb-hdrc.0.auto/gadget/tty/ttyGS0

    ifup@usb0.service         loaded active exited        ifup for usb0

     

    or 'dmesg | grep rndis'

    debian@beaglebone:~$ dmesg | grep rndis

    [    0.704540] usbcore: registered new interface driver rndis_host

    [   13.007932]  gadget: adding 'rndis'/de531200 to config 'Multifunction with RNDIS'/bf8127e0

    [   13.007962] rndis_register: configNr = 0

    [   13.007971] rndis_set_param_medium: 0 0

    [   13.008055]  gadget:   interface 0 = rndis/de531200

    [   13.008064]  gadget:   interface 1 = rndis/de531200

     

    Louis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • compeoree
    compeoree over 12 years ago in reply to mao84

    You're welcome Mao,

     

    I can't say for sure, as I don't use the USB Ethernet, so I have not verified its operation. You may want to search for gadget or RNDIS services.

     

    Did you modify any of the Kernel configuration? I did not.

     

    Are you only replacing files in the /boot/uboot folder, or others too?

     

    You might run 'systemctl | grep usb' to see if you get something like this:

    debian@beaglebone:~$ systemctl | grep usb

    sys-devi...et-usb0.device loaded active plugged       /sys/devices/ocp.3/47400000.usb/musb-hdrc.0.auto/gadget/net/usb0

    sys-devi...-ttyGS0.device loaded active plugged       /sys/devices/ocp.3/47400000.usb/musb-hdrc.0.auto/gadget/tty/ttyGS0

    ifup@usb0.service         loaded active exited        ifup for usb0

     

    or 'dmesg | grep rndis'

    debian@beaglebone:~$ dmesg | grep rndis

    [    0.704540] usbcore: registered new interface driver rndis_host

    [   13.007932]  gadget: adding 'rndis'/de531200 to config 'Multifunction with RNDIS'/bf8127e0

    [   13.007962] rndis_register: configNr = 0

    [   13.007971] rndis_set_param_medium: 0 0

    [   13.008055]  gadget:   interface 0 = rndis/de531200

    [   13.008064]  gadget:   interface 1 = rndis/de531200

     

    Louis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mao84
    mao84 over 12 years ago in reply to compeoree

    Hi Louis,

     

    Well, that's not such a big issue anyway, it was just a bit confusing not to see 192.168.7.2 connected via USB as usually.  I should say that ethernet via eth0 works perfectly.

     

    I didn't modify anything and performed all actions exactly as in your first post. I've only replaced the zImage and edited the documents as described as well (except that my bb-view is four inch so I've used files for 4" and put 4 instead of 7 where it should be put).

     

    systemctl | grep usb doesn't return anything. Here's the copy of my systemctl output

    One can see that the only failed task is:

    'systemd-...s-load.service loaded failed failed Load Kernel Modules'

    'dmesg | grep rndis' output is

    [ 0.742586] usbcore: registered new interface driver rndis_host

     

    Best Regards,

    Mao