Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum [How-to] BB-View on latest Debian
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 142 replies
  • Subscribers 64 subscribers
  • Views 29645 views
  • Users 0 members are here
  • debian
  • embedded_linux
  • bb-view
  • bbb
Related

[How-to] BB-View on latest Debian

compeoree
compeoree over 12 years ago

I thought some others might like to know how to get the BB-View working under the latest Debian beta images.

 

Unfortunately, you are going to have to recompile the Kernel. The video works fine without a recompile (the red/blue swap is easy to fix), but the touchscreen control connections are not the same as the standard TI 4-wire interface. I tried to patch the ti_am335x_tsc.c file, so the changes would be limited to a dts recompile, but I haven't been able to get that working yet (I'm pretty sure it is a state machine / bit assignment issue). But anyway, here are the steps that you need to perform.....

 

Overview

1) Download the necessary files

     a) Robert Nelson's handy tools for compiling the Beaglebone kernel

     b) BB-View source for Angstrom

2) Build the default kernel

3) Patch the Kernel and perform a fast recompile

4) Copy the new kernel to the Beaglebone

5) Edit the xorg.conf file to correct the Red/Blue color swap

6) Revel in the 4 days you just saved image

 

Let's Get Started

I am using Ubuntu 12.04 LTS 64 bit running in a VirtualBox VM to compile the kernel:

Make a new folder called bb-view, this is where our build will happen.

> mkdir bb-view

> cd bb-view

 

Install git, if you haven't already:

> apt-get install git

 

Clone Robert Nelson's linux-dev project locally. Be prepared for a large download (~100 Mb for the cross-compiler and ~700 Mb for the kernel source).

> git clone https://github.com/RobertCNelson/linux-dev.git

 

Change into the new linux-dev folder and select branch/tag that matches the Debian version.

> cd linux-dev

> git checkout 3.8.13-bone37 -b tmp

 

Now we need to build the base image, so our cape drivers folder gets populated. The script will tell you if you need to do or install anything else.

> ./build_kernel.sh

 

Come back in an hour or so.....(You might want to download the Angstrom source from element14 now)

 

Patching the Kernel

Extract two files from the Angstrom source:

> unzip angstrom-source.zip

> tar -zxf bb-black-kernel-3.8.13-bb-view.tar.bz2

> cp ./kernel/kernel/drivers/input/touchscreen/ti_am335x_tsc.c  ~/bb-view/linux-dev/KERNEL/drivers/input/touchscreen/

> cp ./kernel/kernel/firmware/capes/BB-VIEW-LCD7-01-00A0.dts  ~/bb-view/linux-dev/KERNEL/firmware/capes/

 

Now we need to let the compiler know that we want to add the firmware to the build:

> nano   ~/bb-view/linux-dev/KERNEL/firmware/Makefile

 

Add the following line somewhere near line 192 (CTRL-C will display current cursor position):

BB-VIEW-LCD7-01-00A0.dtbo \

 

Don't forget the trailing backslash....it is important. Now save and exit by doing CTRL-O, Enter, CTRL-X.

Change back to the linux-dev root folder:

> cd   ~/bb-view/linux-dev

 

Now issue the kernel rebuild command, this won't take very long at all:

> ./tools/rebuild.sh

 

 

Copy Kernel to BBB

The following instructions assume that you already have the Debian beta installed and booted up on the BBB.

The easiest way is to copy the files over the network, via the 'scp' command:

> scp   ~/bb-view/linux-dev/deploy/3.8.13-bone37.zImage   debian@192.168.7.2:/home/debian

Replace debian (both instances) with the username you are running on the BBB and 192.168.7.2 with the IP address of the BBB.

 

Now log into the BBB and copy the kernel image to the boot partition:

> ssh debian@192.168.7.2

bbb>  sudo cp 3.8.13-bone37.zImage   /boot/uboot/zImage

 

We need to do one more thing before the LCD will work. Since the cape doesn't have an EEPROM, we need to black-list the HDMI drivers and force-load the BB-VIEW drivers in the boot command file:

bbb>  sudo  nano  /boot/uboot/uEnv.txt

 

Find the "optargs" line and edit it to be:

optargs=capemgr.disable_partno=BB-BONELT-HDMI,BB-BONELT-HDMIN  capemgr.enable_partno=BB-VIEW-LCD7-01

Notice that the preceding "#" has been removed. You don't want to disable BB-BONE-EMMC-2G, or you won't be able to boot from eMMC.

Now save and exit by doing CTRL-O, Enter, CTRL-X.

 

Reboot the BBB and the LCD should now work....except the blue and red are reversed.

 

Fixing Red/Blue Color Swap

This is due to errata in the TI AM335x processor when switching between 16 and 24 bit video modes. To fix this, we must first find the name of our screen:

> ssh debian@192.168.7.2

bbb> cat  /var/log/Xorg.0.log  |  grep  screen

Mine was "Builtin Default fbdev Screen 0"

 

Now we edit our X configuration file:

bbb> sudo nano  /usr/share/X11/xorg.conf.d/10-evdev.conf

 

and add a "Screen" section at the end of the file:

Section "Screen"

        Identifier "Builtin Default fbdev Screen 0"

        Monitor "Configured Monitor"

        Device "Configured Video Device"

        DefaultDepth 24

EndSection

Save and exit by doing CTRL-O, Enter, CTRL-X.

Reboot and enjoy!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    Hello selsinork, "Which kernel version are you using ?" I use the 3.8. "Did you apply the patch Louis posted ?" I rebuild the kernel with Louis' edits in the "4. Re:[How-to] BB-View on latest Debian" message…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    Ok, so with the overlay loaded then the touch screen driver should be able to work. You can check the proper device using 'evtest' like this: root@lcd:~/evtest# ./evtest No device specified, trying to…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    Interesting. I seem to remember that one of the LEDs on the cape was configured as heartbeat. Perhaps that was the TI-SDK image then as looking at the overlay files I see: gpio-leds-cape-lcd { compatible…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    hello , everyone if someone interesting how to  fix colors for 3.8.13, to work without X  , here is the fix:

    replace blue and red color offset values

    compile new kernel and enjoy. (tested on 3.8.13-bone43_1)

     

     

    /linux-dev/KERNEL/drivers/gpu/drm/drm_fb_helper.c
    @@ -621,9 +621,9 @@
      var->transp.offset = 15;
      break;
      case 16:
    - var->red.offset = 11;
    + var->blue.offset = 11;
      var->green.offset = 5;
    - var->blue.offset = 0;
    + var->red.offset = 0;
      var->red.length = 5;
      var->green.length = 6;
      var->blue.length = 5;
    @@ -631,9 +631,9 @@
      var->transp.offset = 0;
      break;
      case 24:
    - var->red.offset = 16;
    + var->blue.offset = 16;
      var->green.offset = 8;
    - var->blue.offset = 0;
    + var->red.offset = 0;
      var->red.length = 8;
      var->green.length = 8;
      var->blue.length = 8;
    @@ -641,9 +641,9 @@
      var->transp.offset = 0;
      break;
      case 32:
    - var->red.offset = 16;
    + var->blue.offset = 16;
      var->green.offset = 8;
    - var->blue.offset = 0;
    + var->red.offset = 0;
      var->red.length = 8;
      var->green.length = 8;
      var->blue.length = 8;
    @@ -888,9 +888,9 @@
      info->var.transp.length = 0;
      break;
      case 15:
    - info->var.red.offset = 10;
    + info->var.blue.offset = 10;
      info->var.green.offset = 5;
    - info->var.blue.offset = 0;
    + info->var.red.offset = 0;
      info->var.red.length = 5;
      info->var.green.length = 5;
      info->var.blue.length = 5;
    @@ -898,18 +898,18 @@
      info->var.transp.length = 1;
      break;
      case 16:
    - info->var.red.offset = 11;
    + info->var.blue.offset = 11;
      info->var.green.offset = 5;
    - info->var.blue.offset = 0;
    + info->var.red.offset = 0;
      info->var.red.length = 5;
      info->var.green.length = 6;
      info->var.blue.length = 5;
      info->var.transp.offset = 0;
      break;
      case 24:
    - info->var.red.offset = 16;
    + info->var.blue.offset = 16;
      info->var.green.offset = 8;
    - info->var.blue.offset = 0;
    + info->var.red.offset = 0;
      info->var.red.length = 8;
      info->var.green.length = 8;
      info->var.blue.length = 8;@

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    hello , everyone if someone interesting how to  fix colors for 3.8.13, to work without X  , here is the fix:

    replace blue and red color offset values

    compile new kernel and enjoy. (tested on 3.8.13-bone43_1)

     

     

    /linux-dev/KERNEL/drivers/gpu/drm/drm_fb_helper.c
    @@ -621,9 +621,9 @@
      var->transp.offset = 15;
      break;
      case 16:
    - var->red.offset = 11;
    + var->blue.offset = 11;
      var->green.offset = 5;
    - var->blue.offset = 0;
    + var->red.offset = 0;
      var->red.length = 5;
      var->green.length = 6;
      var->blue.length = 5;
    @@ -631,9 +631,9 @@
      var->transp.offset = 0;
      break;
      case 24:
    - var->red.offset = 16;
    + var->blue.offset = 16;
      var->green.offset = 8;
    - var->blue.offset = 0;
    + var->red.offset = 0;
      var->red.length = 8;
      var->green.length = 8;
      var->blue.length = 8;
    @@ -641,9 +641,9 @@
      var->transp.offset = 0;
      break;
      case 32:
    - var->red.offset = 16;
    + var->blue.offset = 16;
      var->green.offset = 8;
    - var->blue.offset = 0;
    + var->red.offset = 0;
      var->red.length = 8;
      var->green.length = 8;
      var->blue.length = 8;
    @@ -888,9 +888,9 @@
      info->var.transp.length = 0;
      break;
      case 15:
    - info->var.red.offset = 10;
    + info->var.blue.offset = 10;
      info->var.green.offset = 5;
    - info->var.blue.offset = 0;
    + info->var.red.offset = 0;
      info->var.red.length = 5;
      info->var.green.length = 5;
      info->var.blue.length = 5;
    @@ -898,18 +898,18 @@
      info->var.transp.length = 1;
      break;
      case 16:
    - info->var.red.offset = 11;
    + info->var.blue.offset = 11;
      info->var.green.offset = 5;
    - info->var.blue.offset = 0;
    + info->var.red.offset = 0;
      info->var.red.length = 5;
      info->var.green.length = 6;
      info->var.blue.length = 5;
      info->var.transp.offset = 0;
      break;
      case 24:
    - info->var.red.offset = 16;
    + info->var.blue.offset = 16;
      info->var.green.offset = 8;
    - info->var.blue.offset = 0;
    + info->var.red.offset = 0;
      info->var.red.length = 8;
      info->var.green.length = 8;
      info->var.blue.length = 8;@

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • compeoree
    compeoree over 12 years ago in reply to e14 Contributor

    @Vagif Thanks for posting this, I was just about to tackle that. I will test out your patch.

     

    @ Matthew I will look at my 7 inch screen tomorrow and possibly send photos. I have it connected to a BBB, but have not tried to run it on a BBW.

     

    Louis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to compeoree

    @Louis ,  np  we should thank you for making this post.

     

    I have never made patch files, so don't judge if it is in reverse order image . And I have not tested it with Xorg, but will assume it does what is should.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Thank you very much Vagif !

     

    Tux and LXDE look better now image