Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum BBB - BeagleBone Black WiFi Settings
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 58 subscribers
  • Views 1109 views
  • Users 0 members are here
  • wifi
  • beaglebone_black
  • beagleboneblack
  • bbb
  • texas_instruments
  • ti
  • linux
Related

BBB - BeagleBone Black WiFi Settings

shabaz
shabaz over 12 years ago

I thought it may be a good idea to record working WiFi configs - stored here so we can all edit and refine in a single location, rather than have dispersed (and sometimes incorrect or incomplete) information everywhere.

I've kicked it off with UWN100/UWN200 on the current Debian image. I'm no expert with this (usually use wired connections on my Linux boxes) so they may not be currently "optimum" but worked for me. Hopefully those more knowledgeable can refine these over time.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem +1
    John Beetem wrote: I think you just proved my point. Probably It's my feeling that the distro should make it all transparent and easy, at least for the common cases. That it's fairly simple to do…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz +1
    I suppose there may be people out there still using WEP, so you should probably add a section to the supplicant config something like this network={ ssid="you have been compromised already" key_mgmt=none…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    I'm often amazed at how many people seem to have problems with WiFi on Linux on SBCs.

     

    Certainly maybe 4 or 5 years ago wifi could be a pain but these days the problems should largely be a thing of the past.  That does tend to mean that the blame mostly falls on the distros.

     

    Your config looks ok to me, the only fly in the ointment being that with a different network card it may not be ra0, but could be wlan0, ath0, or even just eth1... and that's before you get to the distro installing some odd naming rules into udev and making it even worse.

    Other than that, and presence of the appropriate firmware if required, it should just work with any wifi adapter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I'm often amazed at how many people seem to have problems with WiFi on Linux on SBCs.

    Personally, I'm amazed that normal people can get networking to work at all.  I used to write datacom software (mostly at the device/link layer rather than the network/application layer) and the are so many things that can go wrong, it seems like pure luck when people are able to get all the settings right.

    Your config looks ok to me, the only fly in the ointment being that with a different network card it may not be ra0, but could be wlan0, ath0, or even just eth1... and that's before you get to the distro installing some odd naming rules into udev and making it even worse.

    I think you just proved my point. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I think you just proved my point.

    Probably image   It's my feeling that the distro should make it all transparent and easy, at least for the common cases.  That it's fairly simple to do, but they still don't is the puzzling part.

    You're right that there's so much to go wrong, but the common case is likely to be one wired network port and one wifi on either an SBC or Laptop. Typically only one wired for a desktop. These cases are trivial to get right out of the box.

    Something acting as a router or using vlans is typically complex enough that the default networking setup in the distro can't cope anyway, so trying to do so and forcing that complexity onto the common case is highly counter productive.

     

    Still, It's probably also true that some people will still manage to break things no matter how easy it's been made image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I think you just proved my point.

    Probably image   It's my feeling that the distro should make it all transparent and easy, at least for the common cases.  That it's fairly simple to do, but they still don't is the puzzling part.

    You're right that there's so much to go wrong, but the common case is likely to be one wired network port and one wifi on either an SBC or Laptop. Typically only one wired for a desktop. These cases are trivial to get right out of the box.

    Something acting as a router or using vlans is typically complex enough that the default networking setup in the distro can't cope anyway, so trying to do so and forcing that complexity onto the common case is highly counter productive.

     

    Still, It's probably also true that some people will still manage to break things no matter how easy it's been made image