Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Cloud9
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 59 subscribers
  • Views 812 views
  • Users 0 members are here
Related

Cloud9

e14 Contributor
e14 Contributor over 12 years ago

In the new Debian release is there documentation anywhere of the changes made to the Cloud9 environment?  Or maybe an update to "Getting started with Beaglebone"?

  • Sign in to reply
  • Cancel

Top Replies

  • jkridner
    jkridner over 12 years ago +1
    Yes, it can handle running all the PWMs at once. You need to be careful that you aren't using the same PMW on two different pins. Using two different signals out of the same PWM requires you to use the…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to jkridner +1
    I did get it to work after commenting out 2 of the three in the code and bringing them one at a time. I'm using EHRPWM0. EHRPWM1 and EHRPWM2, it looks like each one can feed two output pins, but it seems…
Parents
  • fustini
    fustini over 12 years ago

    Check this blog post... it works with Javascript, Python and even Arduino sketches now!

    BeagleBoard.org - 2014-03-05-debian-beta-released

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to fustini

    One thing (of many).  In Getting Started With BegleBone in the section on bonescript  The user is told to save the source file by clicking on the disk icon.  In the Debian release it's just not there anymore, and file --> save from the menu doesn't always put the file where you think it will.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 12 years ago in reply to e14 Contributor

    jkridner: any idea about this issue with the new Cloud9?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fustini
    fustini over 12 years ago in reply to e14 Contributor

    jkridner: any idea about this issue with the new Cloud9?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to fustini

    Another question.  The technical reference manual for the CPU says it has 3 independent PWM modules.  Bonescript gives assorted errors when trying to use more than one, "file already exists", "uncaught exception" etc.  Can bonescript handle 3 PWMs?