Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Riot Board ethernet problem
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 57 subscribers
  • Views 1461 views
  • Users 0 members are here
Related

Riot Board ethernet problem

tjmerics
tjmerics over 12 years ago

trying to ping from u-boot and cannot get it to work on the riot board. I've set the ethaddr & ipaddr variables. Using the same procedure I can ping  from a sabre-lite board. Cannot get the mii command to work on u-boot. Tried mii dump [0-4] (should be @ 4) and I get an error from u-boot. I'm trying to port QNX to this board and have every thing working except the networking. I think there may be a problem with the phy.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Which version of u-Boot ?

     

    There's a version of v2014.04 available that includes patches for RIoTboard and it does work with the network happily

     

    => version

    U-Boot 2014.04-00074-g93af0a0-dirty (Apr 26 2014 - 18:40:59)

    gcc (GCC) 4.8.2

    GNU ld (GNU Binutils) 2.23.2

     

    => mii device

    MII devices: 'FEC'

    Current device: 'FEC'

    => mii info

    PHY 0x04: OUI = 0x1374, Model = 0x07, Rev = 0x02, 100baseT, FDX

    => mii dump 4

    0.     (3100)                 -- PHY control register --

      (8000:0000) 0.15    =     0    reset

      (4000:0000) 0.14    =     0    loopback

      (2040:2000) 0. 6,13 =   b01    speed selection = 100 Mbps

      (1000:1000) 0.12    =     1    A/N enable

      (0800:0000) 0.11    =     0    power-down

      (0400:0000) 0.10    =     0    isolate

      (0200:0000) 0. 9    =     0    restart A/N

      (0100:0100) 0. 8    =     1    duplex = full

      (0080:0000) 0. 7    =     0    collision test enable

      (003f:0000) 0. 5- 0 =     0    (reserved)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tjmerics
    tjmerics over 12 years ago in reply to e14 Contributor

    I have the 2009 version which comes with the board. Is the a place to download the image from or do you have to build it from scratch ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tjmerics
    tjmerics over 12 years ago in reply to e14 Contributor

    I have the 2009 version which comes with the board. Is the a place to download the image from or do you have to build it from scratch ?