Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Riot Board ethernet problem
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 57 subscribers
  • Views 1455 views
  • Users 0 members are here
Related

Riot Board ethernet problem

tjmerics
tjmerics over 12 years ago

trying to ping from u-boot and cannot get it to work on the riot board. I've set the ethaddr & ipaddr variables. Using the same procedure I can ping  from a sabre-lite board. Cannot get the mii command to work on u-boot. Tried mii dump [0-4] (should be @ 4) and I get an error from u-boot. I'm trying to port QNX to this board and have every thing working except the networking. I think there may be a problem with the phy.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Which version of u-Boot ?

     

    There's a version of v2014.04 available that includes patches for RIoTboard and it does work with the network happily

     

    => version

    U-Boot 2014.04-00074-g93af0a0-dirty (Apr 26 2014 - 18:40:59)

    gcc (GCC) 4.8.2

    GNU ld (GNU Binutils) 2.23.2

     

    => mii device

    MII devices: 'FEC'

    Current device: 'FEC'

    => mii info

    PHY 0x04: OUI = 0x1374, Model = 0x07, Rev = 0x02, 100baseT, FDX

    => mii dump 4

    0.     (3100)                 -- PHY control register --

      (8000:0000) 0.15    =     0    reset

      (4000:0000) 0.14    =     0    loopback

      (2040:2000) 0. 6,13 =   b01    speed selection = 100 Mbps

      (1000:1000) 0.12    =     1    A/N enable

      (0800:0000) 0.11    =     0    power-down

      (0400:0000) 0.10    =     0    isolate

      (0200:0000) 0. 9    =     0    restart A/N

      (0100:0100) 0. 8    =     1    duplex = full

      (0080:0000) 0. 7    =     0    collision test enable

      (003f:0000) 0. 5- 0 =     0    (reserved)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Details on building mainline u-boot here The specified item was not found.

    although I suspect you'll want some different default options from what I've used with linux in mind..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tjmerics
    tjmerics over 12 years ago in reply to e14 Contributor

    I have the 2009 version which comes with the board. Is the a place to download the image from or do you have to build it from scratch ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    MX6Solo RIOT U-Boot > version

     

    U-Boot 2009.08-00695-g055df3a (Dec 25 2013 - 09:56:12)

     

    MX6Solo RIOT U-Boot > mii dump 4

    Error reading from the PHY addr=04 reg=00

     

    So the shipped version of u-Boot is fubar as far as networking is concerned.  So the simple solution is - don't use it !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tjmerics
    tjmerics over 12 years ago in reply to e14 Contributor

    What are the chances newark / farnell will make woking software available on there web site ? I cannot down load the ubuntu image with mfgtool without the linux image running out of memory and crashing before it finishes burning the eMMC. Unfortunately I don't have a Linux box to build u-boot with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to tjmerics

    Well there's a chicken and egg problem if ever there was one... I posted instructions today for putting the ubuntu image onto an SD card

    The specified item was not found.

    The obvious problem being that you need a linux machine to do it image

     

    No chance to install a virtualbox / vmware player or workstation virtual machine with linux inside ?

     

    As far as working software being made available by e14.. there have been lots of similar requests along with reports of all sorts of things that don't work properly. So far the only responses have been along the lines of "we're working on it, please bare with us". So far no light at the end of that tunnel.

     

    I can certainly put up a binary of the u-boot version from my blog post, but I don't know how useful it'll be for you since I've configured it down to doing just one thing well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Thomas,  slightly different question...  u-Boot supporting networking or not shouldn't really affect your QNX port. u-Boot doesn't have any need for lots of the peripherals in the i.MX6 SoC so won't ever configure them, leaving that to the OS.

    Similarly, the OS should just configure the network adapter and phy itself if it is to have any hope it's been done right.

     

    So what exactly are you trying to do?  Are you simply trying to network boot the OS image, or are you relying on u-boot for something it's never going to guarantee to do for you?   In the latter case, you should really fix QNX to properly configure the hardware..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tjmerics
    tjmerics over 12 years ago in reply to e14 Contributor

    I'm using the QNX bootloader which is working fine. I'm trying to get the networking going but I'm seeing some issues with the phy. I wanted to use u-boot just to make sure the networking is working and nothing is broken. I guess I'll try to setup a Linux box over the weekend. Thanks !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to tjmerics

    try this.  write it to an SD card at 1K from the start, set the boot switches appropriately The specified item was not found.

    can't promise it'll help, but it might save you some time at least..

    Attachments:
    u-boot.imx.zip