Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Double DRAM capacity on Beaglebone Black
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 58 subscribers
  • Views 1544 views
  • Users 0 members are here
  • ddr3
  • memory
  • ddr3l
  • BeagleBone
Related

Double DRAM capacity on Beaglebone Black

e14 Contributor
e14 Contributor over 12 years ago

Is there a demand for more than 512MB DDR3 memory on the Beaglebone Black?

Intelligent Memory is in production with 8Gbit DDR3 components with a single chip-select (part# IM8G16D3FBBG)  that would make it possible to upgrade the Beaglebone to 1GB by replacing the DRAM.

 

Surely it is not easy to de-solder the DRAM and put a new one on it, but if there was some demand in a 1GB version, then Element14 might offer a 1GB version of the BBB as an ordering-option maybe?

Regards,

Thorsten

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    Is the RAM pin compatible with the currently installed ram chip, if not then it wont work without a PCB re design, assuming the CPU can use it also

     

    I have not looked into this yet so I an just speculating and prompting you do check if you have not already into a couple of possible issues with this

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    Hi Peter,

     

    yes, it is generally pin-compatible.

    Address line A15 is used to reach the memory capacity. I just looked up the latest design file from March 21st 2014 and A15 is connected from CPU to DRAM.

     

    To access the 8Gbit memory device completely, the memory-initialization routine needs to be changed to use A0-A15 (total 16 lines) for the row address, instead of the current setting to use A0-A14 for 4Gbit DRAMs

     

    Regards,

    Thorsten

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    Hi Peter,

     

    yes, it is generally pin-compatible.

    Address line A15 is used to reach the memory capacity. I just looked up the latest design file from March 21st 2014 and A15 is connected from CPU to DRAM.

     

    To access the 8Gbit memory device completely, the memory-initialization routine needs to be changed to use A0-A15 (total 16 lines) for the row address, instead of the current setting to use A0-A14 for 4Gbit DRAMs

     

    Regards,

    Thorsten