Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum BB: getting python Tkinter GUI, display error
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 58 subscribers
  • Views 2114 views
  • Users 0 members are here
Related

BB: getting python Tkinter GUI, display error

e14 Contributor
e14 Contributor over 10 years ago

I am trying to get the python GUI package Tkinter running on the BeagleBone Black (debian Jessie) to connect to the display. I get this error when running a simple test script over ssh, but not when running the script locally:

 

root@beaglebone:/boot# python /home/debian/oqy/tktest.py

No protocol specified

No protocol specified

Traceback (most recent call last):

  File "/home/debian/oqy/tktest.py", line 3, in <module>

    root = Tk()

  File "/usr/lib/python2.7/lib-tk/Tkinter.py", line 1813, in __init__

    self.tk = _tkinter.create(screenName, baseName, className, interactive, wantobjects, useTk, sync, use)

_tkinter.TclError: couldn't connect to display ":0.0"

 

How can I configure the X11 server to find the right display via ssh?

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 10 years ago

    It isn't entirely straightforward actually.

    Local Pi Display

    (search for the comment from me on that page, it contains the URL you need).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Did you set up X11 forwarding?  If not, I suggest that you do a search on ssh x11 forwarding debian, filtered to a time-frame within the last year.  There are several tutorials.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    Ah, I may have misunderstood the question.

    Jill, Richard's method will allow you to use the display on the machine you're SSH'ing from.

    My response assumed the opposite, that you wished to use the display connected to the BBB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    Your question is not clear... Do you have a display on the BBB that you want to use or do you want X11 on SSH?

    1> Requires a X11 process to find the display attached on BBB.

    2>Is as said, use X11 forwarding when SSH into BBB.

    Sponsored Welcome Screen- http://www.unix.com

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Assuming the following:

    • A = SSH client machine that wishes to connect to Debian-ish (Debian, Ubuntu, Mint, etc.) machine B, running an SSH daemon.
    • X11 is installed on both A and B (common in the POSIX world with some exceptions such as some data centre servers).
    • B is the X11 client and A is the X11 server (where the keyboard, mouse, and display hardware are).

     

    On B, make sure that /etc/ssh/sshd_config has the following 2 parameter settings:

         X11Forwarding        yes

         X11DisplayOffset     10

    If not, set up those 2 parameters and restart the SSH daemon on B (or reboot).

     

    Now, on A, execute:

     

         ssh -Y username-on-B@B-host-address

     

    That should do it.  Don't forget the -Y flag.  The -Y flag enables "trusted" X11 forwarding to the SSH client (X11 server).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Yes, thank you. These worked. I can now get the Tkinter GUI on either display!