Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum BB: getting python Tkinter GUI, display error
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 58 subscribers
  • Views 2116 views
  • Users 0 members are here
Related

BB: getting python Tkinter GUI, display error

e14 Contributor
e14 Contributor over 10 years ago

I am trying to get the python GUI package Tkinter running on the BeagleBone Black (debian Jessie) to connect to the display. I get this error when running a simple test script over ssh, but not when running the script locally:

 

root@beaglebone:/boot# python /home/debian/oqy/tktest.py

No protocol specified

No protocol specified

Traceback (most recent call last):

  File "/home/debian/oqy/tktest.py", line 3, in <module>

    root = Tk()

  File "/usr/lib/python2.7/lib-tk/Tkinter.py", line 1813, in __init__

    self.tk = _tkinter.create(screenName, baseName, className, interactive, wantobjects, useTk, sync, use)

_tkinter.TclError: couldn't connect to display ":0.0"

 

How can I configure the X11 server to find the right display via ssh?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Assuming the following:

    • A = SSH client machine that wishes to connect to Debian-ish (Debian, Ubuntu, Mint, etc.) machine B, running an SSH daemon.
    • X11 is installed on both A and B (common in the POSIX world with some exceptions such as some data centre servers).
    • B is the X11 client and A is the X11 server (where the keyboard, mouse, and display hardware are).

     

    On B, make sure that /etc/ssh/sshd_config has the following 2 parameter settings:

         X11Forwarding        yes

         X11DisplayOffset     10

    If not, set up those 2 parameters and restart the SSH daemon on B (or reboot).

     

    Now, on A, execute:

     

         ssh -Y username-on-B@B-host-address

     

    That should do it.  Don't forget the -Y flag.  The -Y flag enables "trusted" X11 forwarding to the SSH client (X11 server).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Assuming the following:

    • A = SSH client machine that wishes to connect to Debian-ish (Debian, Ubuntu, Mint, etc.) machine B, running an SSH daemon.
    • X11 is installed on both A and B (common in the POSIX world with some exceptions such as some data centre servers).
    • B is the X11 client and A is the X11 server (where the keyboard, mouse, and display hardware are).

     

    On B, make sure that /etc/ssh/sshd_config has the following 2 parameter settings:

         X11Forwarding        yes

         X11DisplayOffset     10

    If not, set up those 2 parameters and restart the SSH daemon on B (or reboot).

     

    Now, on A, execute:

     

         ssh -Y username-on-B@B-host-address

     

    That should do it.  Don't forget the -Y flag.  The -Y flag enables "trusted" X11 forwarding to the SSH client (X11 server).