Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Power Requirements for the BeagleBone Blue
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 60 subscribers
  • Views 3407 views
  • Users 0 members are here
  • beaglebone blue
  • BeagleBone
  • beaglebone_black_accessory
Related

Power Requirements for the BeagleBone Blue

locknutbushing
locknutbushing over 8 years ago

Hi, I am using the BeagleBone Blue for a robotics project, but I have no intention of using the recommended 2-cell Lipos recommended in the documentation, as they don't have enough voltage or power output for the application. I would much rather use a step-down converter to power the board from the 3-cell Lipo that I am using for the robot. However, this begs the question: what are the power requirements? The documentation is surprisingly vague about this. The recommended battery has 7.4V and 20 amps burst, but there's also a 9-18V power jack...

 

What are the voltage and current inputs that are enough for the BeagleBone Blue to run all four motor drivers and some other pins, but not enough to damage or brick it?

  • Sign in to reply
  • Cancel

Top Replies

  • locknutbushing
    locknutbushing over 8 years ago +1
    So I finally realized that this power adapter is recommended for the Blue: https://www.jameco.com/z/TR9CE4100LCP-A-Globtek-50W-12V-4-16A-AC-to-DC-Regulated-Switching-Wall-Adapter_2229247.html?CID… It outputs…
  • jomoenginer
    jomoenginer over 7 years ago +1 suggested
    locknutbushing wrote: What are the voltage and current inputs that are enough for the BeagleBone Blue to run all four motor drivers and some other pins, but not enough to damage or brick it? I was using…
Parents
  • locknutbushing
    0 locknutbushing over 8 years ago

    So I finally realized that this power adapter is recommended for the Blue:

     

    https://www.jameco.com/z/TR9CE4100LCP-A-Globtek-50W-12V-4-16A-AC-to-DC-Regulated-Switching-Wall-Adapter_2229247.html?CID…

     

    It outputs 12V 4A. So I suppose I can just roll with that...?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • locknutbushing
    0 locknutbushing over 8 years ago

    So I finally realized that this power adapter is recommended for the Blue:

     

    https://www.jameco.com/z/TR9CE4100LCP-A-Globtek-50W-12V-4-16A-AC-to-DC-Regulated-Switching-Wall-Adapter_2229247.html?CID…

     

    It outputs 12V 4A. So I suppose I can just roll with that...?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • odadaj
    0 odadaj over 7 years ago in reply to locknutbushing

    Getting info on the bbblue is quite a challenge.

    Was wondering if it can be powered from an ESC