Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum How can I build an image for the MaaxBoard myself?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 30 replies
  • Answers 12 answers
  • Subscribers 63 subscribers
  • Views 5634 views
  • Users 0 members are here
  • maaxboard
Related

How can I build an image for the MaaxBoard myself?

bryantfhayes
bryantfhayes over 6 years ago

I would like to compile my own image using Yocto, is there a guide for this?

  • Sign in to reply
  • Cancel

Top Replies

  • gonewtinwind
    gonewtinwind over 6 years ago +2
    done! because the maaxboard modified the soc.mk file at u-boot/tools/imx-boot/iMX8M/soc.mk(yocto at imx-mkimage/imx-boot ) it can not support optee before because of no yocto project. I change back, so…
  • bryantfhayes
    bryantfhayes over 6 years ago in reply to joshb86 +1
    Joshua, Great to hear someone is in the same boat. I appreciate you letting me know that EVK conf didn’t work, as that was something I wanted to try. Please do let me know if you have any success with…
  • joshb86
    joshb86 over 6 years ago in reply to bryantfhayes +1 suggested
    First build utilizing imx8_all failed with errors relating to optee. It initially looked like there was a typo somewhere down the layer conf. It reports " Unsupported PLATFORM_FLAVOR "mx8_all " - Notice…
Parents
  • clem57
    0 clem57 over 6 years ago

    MaaXBoard supports OS include:

    1. Android 9.0

    2. Yocto:

    - U-Boot version: 2018.03

    - Kernel version: 4.14.78

    - image: Yocto sumo 2.5

    - Qt 5.10.1 Library or later

    - Customized UI

     

    Well I looked and I can tell you the way it was built

    https://www.yoctoproject.org/docs/2.5.1/brief-yoctoprojectqs/brief-yoctoprojectqs.html .

    The bad news is the hardware specifics are not freely available. Maybe someone here can help locate the Yocto hardware details?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bryantfhayes
    0 bryantfhayes over 6 years ago in reply to clem57

    Thanks for the response!

     

    I am familiar with building via Yocto, I guess my question is more about getting access to the Yocto Board Support Layers used to build specifically for the MaaxBoard Hardware. Are there not build instructions on how to produce an image similar to the pre-built one? Typically, I try to find a BSP layer to make sure the image is compatible with the hardware, but I haven't seen anything like that so far for this board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 6 years ago in reply to bryantfhayes

    Hey Bryant,

     

    The BSP for the MaaXBoard can be found here MaaXBoard

     

    image

     

    Is that what your looking for?

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bryantfhayes
    0 bryantfhayes over 6 years ago in reply to jafoste4

    I've seen the kernel BSP stuff, I guess I am referring to the Layers responsible for Yocto building a root file system. In my past experience with the iMX8MQ, NXP has provided layers to build a demo image. It seems like Embest provides the kernel and uboot source, but no Yocto layers that actually use this source code. I would expect to find a linux-4.14.98.bbappend recipe file or something that builds the kernel for the target hardware.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bryantfhayes
    0 bryantfhayes over 6 years ago in reply to jafoste4

    I've seen the kernel BSP stuff, I guess I am referring to the Layers responsible for Yocto building a root file system. In my past experience with the iMX8MQ, NXP has provided layers to build a demo image. It seems like Embest provides the kernel and uboot source, but no Yocto layers that actually use this source code. I would expect to find a linux-4.14.98.bbappend recipe file or something that builds the kernel for the target hardware.