Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum MaaxBoard does not boot when power is supplied.  It is dead on arrival.  This is the second one.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • +1 person also asked this people also asked this
  • Replies 2 replies
  • Answers 2 answers
  • Subscribers 59 subscribers
  • Views 1877 views
  • Users 0 members are here
  • maaxboard
Related

MaaxBoard does not boot when power is supplied.  It is dead on arrival.  This is the second one.

bspikol
bspikol over 5 years ago

Also, there was a loose screw in the anti-static bag with the board.  It is from the heat sink.  This is the second board purchased that is dead on arrival.  Is there a severe quality control problem? 

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 5 years ago +1 suggested
    Hi Robert, I have not heard of this issue thus far. All boards are checks for functionality at the manufacturer. In regards to your first board, did you contact someone at Avnet for help or are you in…
  • yoctoeco
    yoctoeco over 5 years ago in reply to jafoste4 +1 suggested
    I had issues myself with MaaxBoard - the one with HDMI port. If I have HDMI port connected when powering up, it will not boot. So disconnect HDMI cord and wait few minutes, then connect power again. This…
  • jafoste4
    0 jafoste4 over 5 years ago

    Hi Robert,

     

    I have not heard of this issue thus far. All boards are checks for functionality at the manufacturer. In regards to your first board, did you contact someone at Avnet for help or are you in communication with your local Avnet FAE?

     

    Please allow me to try and help trouble shoot.

     

    1. What SD Card are you using?

         - We reccomend use of a MLC UHS-1 class 10 MicroSD Card.

         - Such as - https://www.newark.com/delkin-devices/s416apg49-u3000-3/memory-card-microsdhc-mlc-16gb/dp/37AC8604 

     

    2. Are you using the MaaXBoard or MaaXBoard Mini?

         - My assumption based on your post is the MaaXBoard, however I'd just like to confirm to avoid any confusion

     

    3. Do you see any LEDs light up when you power the board?

     

    4. What are you using to power the board? A dedicated power supply? Or plugging it into your PC?

         - We reccomend a 5V/3A supply such as https://www.avnet.com/shop/us/products/avnet-engineering-services/aes-acc-maax-pwrul-3074457345642357173/

         -This is especially important if you are plugging in a display or camera into the board.

     

    5. Are you pluggin anything else into the board? (such as a camera or display)?

     

    6. What program are you using to flash your SD Card? I personally use balenaEtcher https://www.balena.io/etcher/

     

    4. What image did you program onto your SD Card? Please respond with the name of the image you programmed into the board. Please note, the MaaXBoard and MaaXBoard Mini have their out of box examples located on the same page. Please confirm you choose the correct image for your board.

    image

     

    Thanks,
    Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • yoctoeco
    0 yoctoeco over 5 years ago in reply to jafoste4

    I had issues myself with MaaxBoard - the one with HDMI port.

    If I have HDMI port connected when powering up, it will not boot.

     

    So disconnect HDMI cord and wait few minutes, then connect power again.

     

    This is a real issue... of couple boards I have... should be addressed by Avnet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer