Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Maaxboard sn65dsi83 mipi dsi to lvds Converter Issue
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 58 subscribers
  • Views 3088 views
  • Users 0 members are here
  • mipi
  • sn65dsi83
  • dsi
  • nwl
  • dsitolvds
  • imx8mq
  • dcss
  • screen
  • maaxboard
Related

Maaxboard sn65dsi83 mipi dsi to lvds Converter Issue

akoc
akoc over 5 years ago

Hello all,

     I have a 10.25 "1280 * 480 resolution screen. I want to run this screen with maaxboard, but I was not successful.

I connect the screen with sn65dsi83 which is a mipi dsi to lvds converter, I tried the kernel configurations with dcss and lcdif, I could only print the test pattern in the test mode on  screen when i use sn65dsi83 with maaxboard via i2c communication. I could not get any image in the normal mode .

 

I'm trying to stand up with maaxboard-dcss-mipi.dtb;

     When I use this dtb file, the system gets up properly, I see that the sn65dsi83 installation has been done properly, but I can't get any image. You can see the output of dmesg in the "maaxboard-dcss-mipi-dmesg.txt" file.

 

I'm trying to stand up with maaxboard-lcdif-mipi.dts;

     When I use this dtb file, the system loading is interrupted and the root file cannot jump to the system.

You can see the output of dmesg in the "maaxboard-lcdif-mipi-dmesg.txt" file.

 

Device                : Maaxboard imx8mq / https://www.avnet.com/wps/portal/us/products/new-product-introductions/npi/avnet-maaxboard/

Yocto version      : https://github.com/Avnet/meta-maaxboard/tree/zeus

sn65dsi83 driver : https://github.com/digi-embedded/linux/tree/v5.4/dey-3.0%2Fmaint/drivers/gpu/drm/bridge/sn65dsi83

Screen                : 10.25 '' 1280x480

 

I have a hard time understanding where I am having problems. I would be glad if you could help. Thanks

 

Files

1) maaxboard-dcss-mipi-dmesg.txt

2) maaxboard-lcdif-mipi-dmesg.txt

3) maaxboard-dcss-mipi.dts

4) maaxboard-lcdif-mipi.dts

5) maaxboard-dsi-common.dtsi

6) TestPatern.jpeg

 

Message was edited by: ahmet koc

Attachments:
maaxboard-dcss-mipi-dmesg.txt.zip
maaxboard-lcdif-mipi-dmesg.txt.zip
image
maaxboard-lcdif-mipi.txt.zip
maaxboard-dcss-mipi.txt.zip
maaxboard-dsi-common.txt.zip
  • Sign in to reply
  • Cancel
Parents
  • akoc
    0 akoc over 5 years ago

    Thanks for your response Josh,

      Yes, there are different outputs, I was aware of this, but I could not solve the problem. Instead I used hdmi to lvds converter as a workaround.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • akoc
    0 akoc over 5 years ago

    Thanks for your response Josh,

      Yes, there are different outputs, I was aware of this, but I could not solve the problem. Instead I used hdmi to lvds converter as a workaround.