Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum What boards should element14 carry besides the Raspberry Pi?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 59 subscribers
  • Views 2574 views
  • Users 0 members are here
  • industrial
  • sbc
  • sabre
  • sabrelite
  • saber
  • embedded
  • raspberry_pi
  • cabeatwell
  • development
  • prototyping
  • innovation
  • sabre_lite
  • communication
Related

What boards should element14 carry besides the Raspberry Pi?

Catwell
Catwell over 13 years ago

Take a look at the blogs... and report back here.

 

I would like to see the ODROID and UDOO board here.

 

C

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    I like the Odroid-U2 for it's faster cpu and 2Gb ram, but not for the interesting looking heatsink 'case' and usb ethernet. The UDOO with it's iMX6 SoC is interesting, but I'd like more gpio via the iMX6…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine +1
    Morgaine Dinova wrote: It's worth noting that in the time this thread was inactive, the Wandboard Quad was added to the family and features not only a populated SATA connector but also 2 gigs of RAM. And…
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor +1
    selsinork wrote: With 2GB ram, a couple of these just got added to my list.. just a pity we can't get them from e14 ! I certainly agree with that, and I'll add a couple here! E14, you have at least 4 guaranteed…
Parents
  • morgaine
    0 morgaine over 13 years ago

    This thread enjoyed pretty much unanimous agreement on which features are pluses and which are minuses.  The problem with such a list when turned into a board spec though is that a highly featured product would be quite likely to cost too much to enjoy high commercial success.  The lack of sales would ensure that the price never drops through volume BOM discounts, and the small community wouldn't generate enough buzz to make all this change.  What Raspberry Pi demonstrated superbly was that the #1 requirement for success is low price.

     

    Although it's tangential to Cabe's question of which boards E14 should stock, what I'd like to propose is that E14 should encourage development of modular and/or extensible board families, so that the family offers the full feature set while individual boards offer only a subset of features but at very low cost.  Modern SoCs make this possible because the SoCs always come in families and their individual devices typically have highly compatible pinouts.

     

    Raspberry Pi Models A and B provide an example of using the same SoC but with varying board features, and BeagleBone and BeagleBone Black are another example despite the board changing significantly between models.  Clearly this approach works well, and there is plenty of room for more family members --- for example, the BeagleBone family could in principle offer variants with two NICs instead of one, and gigabit NIC(s) instead of 100Mbps, because the necessary support is already available in the SoC.  Such variants could become highly popular as very low cost and very frugal Internet servers or firewall/routers, and removing everything on the board that isn't required in an Internet server would keep costs in the BBB ballpark.  It might feel painful to see a BBx released that omits your favourite feature like HDMI, but that just indicates that you need a different variant.

     

    Selecting a different SoC from within a SoC family can be even more powerful than the above.  I like Freescale i.MX6 boards because of the single/dual/quad CPU options, but Freescale doesn't seem to be encouraging "Pi niche" pricing for some reason, or at least no such product has appeared yet.  I hope that a Pi/BBB-priced i.MX6 board will eventually materialize, but currently that isn't possible because designers of i.MX6 boards have piled on the board features, and that is suicide because your costs shoot up.  Price is king.

     

    I suspect that E14/Farnell has a fair bit of influence among semiconductor and board manufacturers, and could encourage this kind of very low cost approach to company and product promotion, while at the same time supporting engineering enthusiasm in the community, for which low cost is almost mandatory.  I'd like to see that, more than seeing them add high-cost full-featured boards to their catalogue.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • morgaine
    0 morgaine over 13 years ago

    This thread enjoyed pretty much unanimous agreement on which features are pluses and which are minuses.  The problem with such a list when turned into a board spec though is that a highly featured product would be quite likely to cost too much to enjoy high commercial success.  The lack of sales would ensure that the price never drops through volume BOM discounts, and the small community wouldn't generate enough buzz to make all this change.  What Raspberry Pi demonstrated superbly was that the #1 requirement for success is low price.

     

    Although it's tangential to Cabe's question of which boards E14 should stock, what I'd like to propose is that E14 should encourage development of modular and/or extensible board families, so that the family offers the full feature set while individual boards offer only a subset of features but at very low cost.  Modern SoCs make this possible because the SoCs always come in families and their individual devices typically have highly compatible pinouts.

     

    Raspberry Pi Models A and B provide an example of using the same SoC but with varying board features, and BeagleBone and BeagleBone Black are another example despite the board changing significantly between models.  Clearly this approach works well, and there is plenty of room for more family members --- for example, the BeagleBone family could in principle offer variants with two NICs instead of one, and gigabit NIC(s) instead of 100Mbps, because the necessary support is already available in the SoC.  Such variants could become highly popular as very low cost and very frugal Internet servers or firewall/routers, and removing everything on the board that isn't required in an Internet server would keep costs in the BBB ballpark.  It might feel painful to see a BBx released that omits your favourite feature like HDMI, but that just indicates that you need a different variant.

     

    Selecting a different SoC from within a SoC family can be even more powerful than the above.  I like Freescale i.MX6 boards because of the single/dual/quad CPU options, but Freescale doesn't seem to be encouraging "Pi niche" pricing for some reason, or at least no such product has appeared yet.  I hope that a Pi/BBB-priced i.MX6 board will eventually materialize, but currently that isn't possible because designers of i.MX6 boards have piled on the board features, and that is suicide because your costs shoot up.  Price is king.

     

    I suspect that E14/Farnell has a fair bit of influence among semiconductor and board manufacturers, and could encourage this kind of very low cost approach to company and product promotion, while at the same time supporting engineering enthusiasm in the community, for which low cost is almost mandatory.  I'd like to see that, more than seeing them add high-cost full-featured boards to their catalogue.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • morgaine
    0 morgaine over 13 years ago in reply to morgaine

    It's worth noting that in the time this thread was inactive, the Wandboard Quad was added to the family and features not only a populated SATA connector but also 2 gigs of RAM.  And of course a much higher price tag than the base model, which means that its sales will never rise above mildly buoyant.

     

    Board manufacturers just don't seem to be learning effectively from the Pi and now BBB precedent.  I doubt that they want low sales, but they're just not learning.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    It's worth noting that in the time this thread was inactive, the Wandboard Quad was added to the family and features not only a populated SATA connector but also 2 gigs of RAM.  And of course a much higher price tag than the base model, which means that its sales will never rise above mildly buoyant.

    Even so, $129 is still very good for a 2Gb quad core.  Looking at their distributors, future electronics equate that to 79.58 GBP (97.48 from mouser?), not exactly BBB/R-Pi territory, but very much better than Sabre-Lite.

    With 2GB ram, a couple of these just got added to my list.. just a pity we can't get them from e14 !

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • morgaine
    0 morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    With 2GB ram, a couple of these just got added to my list.. just a pity we can't get them from e14 !

     

    I certainly agree with that, and I'll add a couple here!  E14, you have at least 4 guaranteed boards sales if you stock this. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I certainly agree with that, and I'll add a couple here!  E14, you have at least 4 guaranteed boards sales if you stock this.

    I gave up waiting and ordered two WB Quads from Future in the US.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • morgaine
    0 morgaine over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I gave up waiting and ordered two WB Quads from Future in the US.

     

    I think you're right.  Farnell still doesn't have A20-OLinuXino listed, not even mentioned as a product in advance of stocking.

     

    I guess there's a moral in this.  Large companies eventually end up sitting on their laurels, and "We are listening" becomes pure PR with not a shred of reality behind it.  9-5'ers probably don't care that they're bringing a company that was "Best of British" into disrepute anyway.  (This might be related to the people who hear us not being British and so feeling no stake in a group reputation built over decades.  The "upgrade" disaster suggests that possibility.)

     

    I might take your lead and order some Wandboards from Europe too as a self-Xmas present.  There's nothing much to challenge the Quad on specs at this time.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I might take your lead and order some Wandboards from Europe too

    I took a look at the two european distys, Denx & Texim and thought that their shipping & handling charges were somewhat eye watering..  Might skip the export paperwork delay, but I'm wondering it that's worth an extra 50 quid image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Niether of them seem to have stock of the Quad right now anyway image