Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum BBView 7" LCD does not work on BeagleBone Black (Rev A6)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 56 subscribers
  • Views 546 views
  • Users 0 members are here
  • cape
  • lcd
  • bbview
  • BeagleBone
Related

BBView 7" LCD does not work on BeagleBone Black (Rev A6)

anhalim
anhalim over 12 years ago

Hi there

 

I just bought a 7" LCD expansion cape for my BBB. However, I could not get the LCD to display anything.

I could perfectly test the keypads and LEDs without the LCD connected to the cape. When the LCD is connected, however, there is a background light came out from the LCD for a while and then the whole system turned off.

 

I tried to plug the whole system (BBB + 7" LCD) to 5V/2A USB adapter, but the problem still persists.

In addition, the LCD datasheet mentioned two parameters regarding Current Consumption, i.e. Icc typically at 250mA and Iled (LED driving current) typically at 500mA, which already exceed USB2.0 specification (but still in the range of my USB adapter capability). On the other hand, there is no current consumption specified in the 4.3" LCD datasheet.

 

Has anyone face the same problem as mine?

 

To the forum moderator: Has the 7" LCD been tested with BBB before, as claimed in the user manual (i.e. the LCD can be powered directly from BBB), or is it only valid for 4.3" LCD?

Is there any schematic for the LCD?

 

Please let me know. I am looking forward to hearing from you soon. Thanks!

  • Sign in to reply
  • Cancel
Parents
  • element14jamie
    0 element14jamie over 12 years ago

    Hello Andriyanto,

    Thank you for posting this question and to shabaz for helping!

     

    I will move this over to the BeagleBone Black area as it is a better fit

     

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • element14jamie
    0 element14jamie over 12 years ago

    Hello Andriyanto,

    Thank you for posting this question and to shabaz for helping!

     

    I will move this over to the BeagleBone Black area as it is a better fit

     

    Jamie