Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum I cannot flash BBB eMMC
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 2 answers
  • Subscribers 61 subscribers
  • Views 2672 views
  • Users 0 members are here
  • beagleboneblack
  • bbb
Related

I cannot flash BBB eMMC

gihu
gihu over 12 years ago

Hi all,

 

I am wroting down here these lines beacause I am quite confused, and maybe I am doing something wrong and I still don't know it.

I have a BBB revision A6. As far as I though, BBB boots from internal eMMC, and can not boot from SD, but

I doanloaded and Android image from here:

Beagleboard:Android - eLinux.org

The first thing it seems extrange for me is that eMMC is 2-GB while Android image is almost 4GB

I have used WIN32 disk imager to write the image in the SD card (I tried on winXP and win8), but when I try to flash the BBB I have no succes, I think I am following all the steps, unplug everything, plug SD card, hold down boot button (I have checked I am holding the write button) and power on while boot button is pressed, but nothing happens, 4 user LEDs are off. I have tried many times (about 20 times), I have changed the power supply, firstly that could be the problem, now I am using 5V 2.1A power supply, over the power connector.

 

But, what is even more extrange, is that if I power on the BBB with the SD card (with build-in Android image), and without presing any button, the BBB boots from SD card and starts Android, and If I power down, remove SD card and power on again, Angstrom distribution is still on BBB.

 

Has anyone seen this behave before?

Is it not posible flash this Android  image because it is larger than eMMC?

So, if BBB can`t boot from SD, what I see when I power on the BBB with the SD card, is a wrong booting?

 

I am very confused and I really appreciate your help

 

Regards,

Miguel

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to rantalbott +3 verified
    Ran Talbott wrote: Interestingly, I accidentally discovered that I don't need to push the "user" switch during power-up to boot from SD. I believe this is because the SD cards have a uEnv.txt file in…
  • rantalbott
    rantalbott over 12 years ago +2 suggested
    My A6 just came in yesterday, but I'm assuming that it'll be able to boot from SD just like my A5s do. Interestingly, I accidentally discovered that I don't need to push the "user" switch during power…
  • e14 Contributor
    e14 Contributor over 12 years ago +1 suggested
    The Android image from the site you reference is a stand-alone Android image for use booting from the SD card only .. it does not, and will not program the on-board eMMC as you desire. For that you will…
Parents
  • alamorobotics
    0 alamorobotics over 12 years ago

    I came across this little blurb on Beagleboard:Updating The Software - eLinux.org,

    To force a boot from the microSD card, delete the MLO file in the FAT partition of the eMMC.

    You can access this when the board is connected over the USB cable and it appears as a thumbdrive.

     

    Has anyone given it a try ?

    I'll give it a try later tonight after work... ;-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to alamorobotics

    The table on page 6 of the schematics gives the boot order for normal boot and holding the button down during a power cycle. The idea being that if it doesn't find MLO on the first device, it moves on to the next etc.

     

    I spent some time building my own uSD image to use for flashing the eMMC (sorry, the angstrom one was too slow) and my experience was that it's all to easy to end up in a state that doesn't appear to match the stated boot order. Exactly how you get there isn't clear, holding the button tends to force the right thing.

    What's not always clear is that you need to hold the button during power-on, holding it during a reset or reboot does nothing.  Once you've held the button during a power-on, the change of boot order stays in effect until you power cycle again, so in that state you'll boot to uSD on a reboot or when you press the reset button.  This obviously has the potential to confuse matters if you don't realise what's happening.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to alamorobotics

    The table on page 6 of the schematics gives the boot order for normal boot and holding the button down during a power cycle. The idea being that if it doesn't find MLO on the first device, it moves on to the next etc.

     

    I spent some time building my own uSD image to use for flashing the eMMC (sorry, the angstrom one was too slow) and my experience was that it's all to easy to end up in a state that doesn't appear to match the stated boot order. Exactly how you get there isn't clear, holding the button tends to force the right thing.

    What's not always clear is that you need to hold the button during power-on, holding it during a reset or reboot does nothing.  Once you've held the button during a power-on, the change of boot order stays in effect until you power cycle again, so in that state you'll boot to uSD on a reboot or when you press the reset button.  This obviously has the potential to confuse matters if you don't realise what's happening.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • morgaine
    0 morgaine over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    What's not always clear is that you need to hold the button during power-on, holding it during a reset or reboot does nothing.

    Sometimes I really miss jumpers.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to morgaine

    image

    Not sure it would help here, the configuration pins are only sampled on power-up.  Yes, the days when this wasn't the case were in some ways preferable. Unless you'd just spilled a bag of 5000 jumpers on the floor image