Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum BB view, Can't boot TI SDK image to BBB
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 59 subscribers
  • Views 1330 views
  • Users 0 members are here
  • embedded_linux
  • bb-view
  • beaglebone_black
  • bbb
Related

BB view, Can't boot TI SDK image to BBB

e14 Contributor
e14 Contributor over 12 years ago

I am having trouble getting the TI SDK image to boot on BBB. I  wrote the image file,

bb-view-emmc-flasher-2013-09-09.img to a micro ad card and flashed the emmc accordingly. After Flashing the BBB (all LEDs steady lit after only 15 mins, vs the typical 30-45?)  I install the BB view cape and 7" LCD module, and reboot without the sd card.  I can see the backlight come on, but never displays anything. The pwr led on the BBB stays lit, but none of the other LEDs, on the BBB. However, One of the leds on the cape does blink. any help would be greatly appreciated.

  • Sign in to reply
  • Cancel
Parents
  • aaronpbrooks
    0 aaronpbrooks over 12 years ago

    Alright, I've got things working now.  If you have a 3.3v FTDI 232 serial cable/adaptor, you should be able to resolve this fairly easily.  Here are the steps that I took:

    • Shutdown/remove power from BBB
    • Remove cape from BBB
    • Plug in FTDI cable, and open/configure your favorite terminal application (I'm on a mac and really like CoolTerm (http://freeware.the-meiers.org/), but there are other options
    • Power BBB, and verify that bootup occurs (there will be no LED activity on the board, but you will see the bootup sequence via your terminal)
      • Login password for "am37x-evm" is "root"
    • Make changes described in the user manual (here: http://www.farnell.com/datasheets/1817212.pdf) in section 5.1.3, including removal of the 'pointercal' file
    • Perform shutdown ("shutdown now")
    • Remove power source
    • Place cape onto BBB
    • Supply power (through barrel jack is probably more reliable, but I have found that my USB port does actually supply enough current)
    • If all is well, the calibration screen will now appear!

     

    Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to aaronpbrooks

    I think it's related to powering the board from USB or external supply. I was unable to restore the BBB until I connected an external supply, and right now I have a 7'' LCD running directly from the uSD just as described in the manual for the old BB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to aaronpbrooks

    I think it's related to powering the board from USB or external supply. I was unable to restore the BBB until I connected an external supply, and right now I have a 7'' LCD running directly from the uSD just as described in the manual for the old BB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • aaronpbrooks
    0 aaronpbrooks over 12 years ago in reply to e14 Contributor

    Despite my claim that I got the board powered via USB, you are likely correct.  I got as far as the calibration before it started to draw too much current from my USB.  I switched to a 3A 5V supply and it worked swimmingly.  Hooked up to my variable power supply and measuring with a cheap multimeter, the BBB w/display attached draws just shy of 1A (~950mA), with peak somewhere around 1.2A.