Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Getting BB-View working on newer kernel (3.12.13) than 3.8.13
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 58 subscribers
  • Views 543 views
  • Users 0 members are here
  • bb-view
  • BeagleBone
Related

Getting BB-View working on newer kernel (3.12.13) than 3.8.13

e14 Contributor
e14 Contributor over 12 years ago

Hi

 

I have a BB white and a 7inch BB-View display that I got working with the 3.8.13 kernel using the instruction in this thread:

 

[How-to] BB-View on latest Debian

 

My goal is to get QT Quick 2 working on BBW, so I need the SGX-modules for the OpenGL ES2. I used the RobertCNelson scripts and used the 3.12.13-bone12 version, all successfully compiled and up working, except for the BB-View. When I try to transfer the steps from the thread above I can't get the display working. At start I get "of_resolve: Could not find symbol 'ocp'":

 

...

reading /dtbs/am335x-bone.dtb
27364 bytes read in 12 ms (2.2 MiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x358460 ]
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Using Device Tree in place at 88000000, end 88009ae3

Starting kernel ...

[    1.175739] omap_i2c 4819c000.i2c: Arbitration lost
[    3.227354] bone-capemgr bone_capemgr.6: slot #0: No cape found
[    5.263351] bone-capemgr bone_capemgr.6: slot #1: No cape found
[    7.299350] bone-capemgr bone_capemgr.6: slot #2: No cape found
[    9.335349] bone-capemgr bone_capemgr.6: slot #3: No cape found
[    9.345937] of_resolve: Could not find symbol 'ocp'
[    9.351159] bone-capemgr bone_capemgr.6: slot #4: Failed to resolve tree
[    9.358229] bone-capemgr bone_capemgr.6: loader: failed to load slot-4 BB-VIEW-LCD7-01:00A0 (prio 0)
[    9.370865] musb-hdrc musb-hdrc.0.auto: Falied to request rx1.
[    9.381404] musb-hdrc musb-hdrc.1.auto: Falied to request rx1.
[    9.459242] /cpus/cpu@0: could not find phandle
[    9.467582] tilcdc 4830e000.fb: no encoders/connectors found
[    9.473606] tilcdc 4830e000.fb: failed to initialize mode setting
Loading, please wait...
modprobe: chdir(3.12.13-bone12): No such file or directory

...

 

I found a page (Converting Device tree overlays to Kernel 3.12 on BeagleBone Black | Thing-Printer.comThing-Printer.com) about this problem and changed the "ocp" string to "baseboard_beaglebone" in the BB-View dts file. Recompile and now I got kernel panic instead, of course it wasn't that simple image. Any help?

 

...
reading /dtbs/am335x-bone.dtb
27364 bytes read in 12 ms (2.2 MiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x358aa0 ]
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Using Device Tree in place at 88000000, end 88009ae3

Starting kernel ...

[    1.175780] omap_i2c 4819c000.i2c: Arbitration lost
[    3.227341] bone-capemgr bone_capemgr.6: slot #0: No cape found
[    5.263340] bone-capemgr bone_capemgr.6: slot #1: No cape found
[    7.299338] bone-capemgr bone_capemgr.6: slot #2: No cape found
[    9.335338] bone-capemgr bone_capemgr.6: slot #3: No cape found
[    9.350332] OF: no ranges; cannot translate
[    9.357926] musb-hdrc musb-hdrc.0.auto: Falied to request rx1.
[    9.364294] OF: no ranges; cannot translate
[    9.373030] musb-hdrc musb-hdrc.1.auto: Falied to request rx1.
[    9.380605] OF: no ranges; cannot translate
[    9.385165] OF: no ranges; cannot translate
[    9.448161] pinctrl-single 44e10800.pinmux: pin 44e10978.0 already requested by 4819c000.i2c; cannot claim for gpio-leds-cape-lcd.9
[    9.460637] pinctrl-single 44e10800.pinmux: pin-94 (gpio-leds-cape-lcd.9) status -22
[    9.468811] pinctrl-single 44e10800.pinmux: could not request pin 94 (44e10978.0) from group pinmux_bb_view_lcd_cape_led_pins  on device pinctrl-single
[    9.483065] leds-gpio gpio-leds-cape-lcd.9: Error applying setting, reverse things back
[    9.504250] /cpus/cpu@0: could not find phandle
[    9.512702] tilcdc 4830e000.fb: no encoders/connectors found
[    9.518765] tilcdc 4830e000.fb: failed to initialize mode setting
[    9.527188] tilcdc fb.12: failed to get memory resource

...

[    9.907511] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b

  • Sign in to reply
  • Cancel
Parents
  • razvanbbb
    0 razvanbbb over 12 years ago

    Hi,

    any luck with this? I am in the same situation trying to make LCD4 to work on 3.15 kernel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • razvanbbb
    0 razvanbbb over 12 years ago

    Hi,

    any luck with this? I am in the same situation trying to make LCD4 to work on 3.15 kernel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to razvanbbb

    No sorry. I haven't been working on this for a time.