Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Enabling TIMER4 output on Beaglebone Black
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 58 subscribers
  • Views 1960 views
  • Users 0 members are here
  • beagleboneblack
  • bbb
Related

Enabling TIMER4 output on Beaglebone Black

deker
deker over 12 years ago

Hi,

 

I'm trying to get things set up to use TIMER4 (or 5, 6, or 7) to provide an external clock source to another component and I'm having some trouble. For now I'm happy with just getting the standard 24khz clock, though I may want to be able to modify the frequency in the future.

 

I'm using the Yocto Project (Dora) to build my images and the straight TI kernels from the meta-ti layer (linux-ti-staging_3.12) with a static devicetree. I've customized my devicetree enough that I'm somewhat comfortable with devicetree configs, but I know I'm a long way from having real devicetree-fu. That said, I've added the following in an attempt to get TIMER4 to come up:

 

In the am33xx_pinmux section:

 

        timer4_pins: pinmux_timer4_pins {
          pinctrl-single,pins = <
            0x90 0x12  /* gpmc_advn_ale as TIMER4, OUTPUT_PULLUP | MODE2 */
          >;
        };

 

And further down (note: I'm not certain this is necessary or correct, but it was a shot in the dark):


&timer4_fck {
        pinctrl-names = "default";
        pinctrl-0 = <&timer4_pins>;
        status = "okay";
};

 

I sadly don't have a scope to verify clock on the TIMER4 pin, but my guess is that something's not qorking right from the following reported in /sys/kernel/debug/clk/clk_

summary (note: I clipped bit after the relevant part):

 

root@beaglebone:/sys/kernel/debug/clk# more clk_summary
   clock                        enable_cnt  prepare_cnt  rate
---------------------------------------------------------------------
tclkin_ck                      0           0            12000000 
virt_26000000_ck               0           0            26000000 
virt_25000000_ck               0           0            25000000 
virt_24000000_ck               1           1            24000000 
    sys_clkin_ck                9           23           24000000 
       dpll_mpu_ck              1           1            300000000
          dpll_mpu_m2_ck        4           4            300000000
       timer6_fck               0           1            24000000 
       timer3_fck               0           1            24000000 
       dbg_sysclk_ck            0           1            24000000 
       timer7_fck               0           1            24000000 
       timer5_fck               0           1            24000000 
       timer4_fck               0           1            24000000 
       timer2_fck               1           1            24000000 
       timer1_fck               1           1            24000000 

I also haven't seen the device that needs the clocking initialize properly yet, so that's another tipoff.

 

Maybe related, I'm also seeing the following in the dmesg:

 

[    0.132509] platform mpu.1: FIXME: clock-name 'fck' DOES NOT exist in dt!

 

Any help or pointers would be appreciated. I've tried looking at section 20 in the AM335x TRM and I get the feeling there's just a register setting or two that need to be done, but I'm just beginning to learn the hardware end of the universe after many years as a UN*X guy, so I got a bit lost in trying to figure out how to do it.

 

Thanks,

 

-d

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    from that error in dmesg, I suspect that either there's something missing in the driver, or that you're missing some relevant attribute in your devicetree.

     

    Documentation/devicetree/bindings/crypto/omap-des.txt contains the only mention of 'fck' that I can see, but that could just mean it's not documented properly as that one appears to be for a different driver.

     

    In the vanilla 3.13 kernel source, I don't see a timer4_fck label in the devicetree files anywhere, so you'll have to dig out that label and see what it refers to before you can look up the binding in the documentation to see how to use it.

     

    There is some stuff related to timer4_fck in arch/arm/mach-omap2/cclock33xx_data.c but I can't tell from that how to properly set it up in devicetree.

     

    Unfortunately when you're using something like yocto you have no idea what they've patched into what sort of mess, but it probably bears little resembelance to either Roberts BBB kernels or to vanilla kernel.org kernels. So you end up very much on your own unless you can find someone else using the same config who wants to enable the same things.

    I've had reasonable results enabling stuff in kernel.org kernels on the BBB, but have never tried to setup a timer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • deker
    0 deker over 12 years ago in reply to e14 Contributor

    Thanks for the reply Selsinork.

     

    As far as I"ve been able to tell, the "fck" clock device being missing isn't unique to me, but then again, I'm also not certain that it's particularly relevant.

     

    As far as the kernel goes, the reason I chose to go the yocto route is exactly because I was trying to avoid the kernels that have a whole slew of patches. While I know that Robert's kernels or the Angstrom kernels work just fine, the "mess" of patches as you put it is far more prevalent there. I'm using yocto so that I can use the kernel sources that come direct from Texas Instruments through their official meta-ti layer for openembedded/yocto. The rest of the yocto distribution has not a thing to do with the kernel or devicetree and is actually much more simplistic and trimmed down than just about anything else. Once you wrap your head around bitbake (which you have to do for Angstrom anyway), yocto really is pretty nice to deal with and will allows a level of customization and control of the "mess" that I can't get by using a canned distro and kernel.

     

    That being said, there are definitions for timer4_fck in the DT sources from TI in arch/arm/boot/dts/am33xx-clocks.dtsi:

     

    timer4_fck: timer4_fck@44e00510 {

            #clock-cells = <0>;

            compatible = "mux-clock";

            clocks = <&tclkin_ck>, <&sys_clkin_ck>, <&clkdiv32k_ick>;

            reg = <0x44e00510 0x4>;

            bit-mask = <0x3>;

    };

     

    also in arch/arm/boot/dts/am33xx.dtsi:

     

    timer4: timer@48044000 {

            compatible = "ti,am335x-timer";

            reg = <0x48044000 0x400>;

            interrupts = <92>;

            ti,hwmods = "timer4";

            clocks = <&timer4_fck>;

            clock-names = "fck";

            ti,timer-pwm;

    };

     

     

    So, I can tie this back to how it sits in the clk_summary tree (and also to the "fck" name reference) from my post above, and I believe I've got the pin assignment bits correct, but what I'm lacking is the mechanism to take that defined clock and set the "enabled" bit for it in the kernel. Again, I'm still kind of a devicetree newb, so there may be something I'm missing in the definitions above, so any help is appreciated.

     

     

    Thanks,

     

    -d

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • deker
    0 deker over 12 years ago in reply to deker

    One other thing that I forgot to mention. For my specific application, I can't really use the more popular bbb kernels because I have need of pins reserved for capemgr, which AFAIK is implemented as patches on top of the mainline kernel, and it would be more of a pain than I would like to deal with to excise the entire capemgr (and would put me right back into custom kernels anyways).

     

    -d

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • deker
    0 deker over 12 years ago in reply to deker

    One other thing that I forgot to mention. For my specific application, I can't really use the more popular bbb kernels because I have need of pins reserved for capemgr, which AFAIK is implemented as patches on top of the mainline kernel, and it would be more of a pain than I would like to deal with to excise the entire capemgr (and would put me right back into custom kernels anyways).

     

    -d

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to deker

    capemgr itself shouldn't be reserving any pins, it does however come with a load of assumptions, some of which might.

     

    However IMHO, capemgr is an all or nothing proposition, you either buy into it fully or reject it fully and live with the consequences of that decision.

    The decision is coulded by things like BB-View which assume you've bought the concept and then don't provide all the pieces (the i2c eeprom is missing) which gives you the worst of both worlds.

     

    Haven't tried it, but theoretically you can use the same kernel as everyone else but just put a status = "disabled"; line into the devicetree in the right place and it won't load capemgr. Or just build your own devicetree that doesn't reference capemgr at all..

    There's an effort going on in the mainline kernel that should lead to us being able to build a single kernel that runs across a wide range of boards, all you need is to load the correct dtb for your board and only the required drivers are enabled.  So run that same kernel on a Cubieboard and we need to be able to be able to disable capemgr since the concept isn't valid for the different board. Same applies to something like a network controller that may simply not exist on a different board.