Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Starting LXDE on latest Debian Build with BB-View
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 57 subscribers
  • Views 1275 views
  • Users 0 members are here
  • lxde
  • bb-view
  • beaglebone_black
  • bbb
  • linux
Related

Starting LXDE on latest Debian Build with BB-View

e14 Contributor
e14 Contributor over 12 years ago

I've just downloaded the latest Debian build and added the patches to use BB-View but can't seem to get the desktop from the windows manager to appear on the LCD display. During the boot process the tux logo appears together with other startup messages and finally a welcome message but after that the screen is blank.

 

The touchscreen is working because the calibration screen appears on the first boot and displays the cursor and waits for a touch at each coordinate.

 

I've been starting LXDE which is the window manager used in the distribution by starting tightvncserver which appears to call a script in /root/.vnc/xstartup. I can see the desktop from my vnc client but nothing appears on the lcd display.

 

I guess I'm starting LXDE incorrectly so would welcome any suggestions on how to start LXDE correctly and fix this problem.

 

The debian distribution loaded was this BBB-eMMC-flasher-debian-7.5-2014-05-14-2gb.img

 

Before adding the BB-View patches uname returned this

uname –a

Linux beaglebone 3.8.13-bone50 #1 SMP Tue May 13 13:24:52 UTC 2014 armv7l GNU/Linux


After adding the patches uname returned this

Linux beaglebone 3.8.13 #1 SMP Mon Apr 21 11:45:02 CST 2014 armv7l GNU/Linux

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Can you try by logging into the console (on the LCD with locally attached keyboard/mouse) and typing startx ?

     

    I've not used vnc in a long time, but there used to be options in some variants to keep the local screen blanked while connected remotely. If that's the case then there may be a setting you can change to prevent this.  Other similar remote desktop software, like freeNX, never start a desktop on the local screen, they just use a 'virtual' xserver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Can you try by logging into the console (on the LCD with locally attached keyboard/mouse) and typing startx ?

     

    I've not used vnc in a long time, but there used to be options in some variants to keep the local screen blanked while connected remotely. If that's the case then there may be a setting you can change to prevent this.  Other similar remote desktop software, like freeNX, never start a desktop on the local screen, they just use a 'virtual' xserver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Sorry for not replying earlier but I'm coming to the conclusion that the installation of system did not go smoothly when flashing the mmc. It seems there are files missing to start LXDE like startx and .xinitrc files so I'm looking to start the installation all over again. I'll also see whether the installation works properly before I patch it for BB-VIEW.

     

    Thanks for you help

     

    Tony