Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Is the Gizmo2 suitable for high speed data acquistion?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 60 subscribers
  • Views 2089 views
  • Users 0 members are here
  • high_speed_data_acquisition
  • fpga
  • gizmo2
  • adc
Related

Is the Gizmo2 suitable for high speed data acquistion?

e14 Contributor
e14 Contributor over 11 years ago

Hello.

My area of interest is high speed data acquisition.I'd like to connect a quad or octal high speed ADC (serial LVDS output) running at speeds from say 25 MSPS to 125 MSPS per channel.

For the quad serial LVDS output ADC , need about 20 output lines. I saw on the following link (http://www.gizmosphere.org/wp-content/uploads/2014/11/AMD_GIZMO2_Development_Board_Schematic.pdf) a block diagram of the Gizmo2, which appears to have only 8 GPIO lines.

wonder how it might be possible to use the PCIe edge connectors or SATA connectors to interface the ADC to the Gizmo2.

Maybe it's simply not possible to interface such ADCs directly to Gizmo2 and instead will require a seperate FPGA board, some high speed ADC board custom design to interface with the FGPA board and then try and interface the combined FPGA + ADC  module to the Gizmo. Getting rather complicated.

I would appreciate your thoughts on this please.

Thanks.

Regards,

Will.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 11 years ago

    An 8 channel ADC at 125Ms/S = 1Gbyte/S at 8 bits or 2 Gbyte/S at 16 bits. That's equivalent to one or two 10Gbit Ethernet ports - you are not going to make sense of this amount of data (or do anything with it) with a tiny processor like the Gizmo.

     

    About the only way to get this amount of data from ADC into memory and then computer is by using an FPGA for the glue and multi-lane PCIe or possibly multiple 10Gbit ethernet ports.

    At the bottom end of your speed range it's only 200Mbyte/S - still too much for tiny processors and Gbit Ethernet but easier on PCIe or possibly UltraSpeed USB. At this lower rate SATA is possible but difficult - because now your ADC and FPGA have to pretend to be a disk drive.

     

    Think in terms of medium size FPGA, more than £10k on FPGA design tools, buying in some IP for UltraSpeed USB or Gbit Ethernet and  2000 hours of development effort.

     

    If you only want one just buy it. https://www.picotech.com/oscilloscope/4824/8-channel-oscilloscope

     

    If you want to pay for a  design ..............

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Thank you MK for those comments. Makes sense.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Thank you MK for those comments. Makes sense.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    Gizmo 2 is more like a small Windows or Linux PC, more abilities than a PI but mot as much as a full blown PC

     

     

     

    So for fast data accusation it would depend on what “FAST” is. As there is a multi tasking OS that will make it difficult to maintain critical timing

     

     

     

    You may want to use an Arduino or Launchpad type device as the capture device and the Gizmo as a very powerful HUB providing security, aggregation and analysis for the collected data

     

     

     

    Peter