Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Is the Gizmo2 suitable for high speed data acquistion?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 60 subscribers
  • Views 2059 views
  • Users 0 members are here
  • high_speed_data_acquisition
  • fpga
  • gizmo2
  • adc
Related

Is the Gizmo2 suitable for high speed data acquistion?

e14 Contributor
e14 Contributor over 11 years ago

Hello.

My area of interest is high speed data acquisition.I'd like to connect a quad or octal high speed ADC (serial LVDS output) running at speeds from say 25 MSPS to 125 MSPS per channel.

For the quad serial LVDS output ADC , need about 20 output lines. I saw on the following link (http://www.gizmosphere.org/wp-content/uploads/2014/11/AMD_GIZMO2_Development_Board_Schematic.pdf) a block diagram of the Gizmo2, which appears to have only 8 GPIO lines.

wonder how it might be possible to use the PCIe edge connectors or SATA connectors to interface the ADC to the Gizmo2.

Maybe it's simply not possible to interface such ADCs directly to Gizmo2 and instead will require a seperate FPGA board, some high speed ADC board custom design to interface with the FGPA board and then try and interface the combined FPGA + ADC  module to the Gizmo. Getting rather complicated.

I would appreciate your thoughts on this please.

Thanks.

Regards,

Will.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    If you really want to play with these speeds, I recommend the Mojo FPGA package as a relatively low cost yet capable processor. Usually with that rate, a trigger should be setup to record only the necessary data or output it as a scope. @wf215 please let us know how you go with this interesting project

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to clem57

    The OP wants to run his ADCs at 125 Msamples per second - that's a minimum of 1Gbit/s per ADC and he wants 8 of them. The Mojo is a simple low cost FPGA board and doesn't have the necessary high speed impedance controlled IO to connect to this kind of ADC,

    The FPGA on the Mojo is a low end cheapy - moving Gbytes of data per second takes a bit more than that.

     

    @Peter,

     

    The OP defined FAST - and at speeds of the order of 1GBbyte per second it's out of Arduino, Launchpad or Gizmo range.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to clem57

    The OP wants to run his ADCs at 125 Msamples per second - that's a minimum of 1Gbit/s per ADC and he wants 8 of them. The Mojo is a simple low cost FPGA board and doesn't have the necessary high speed impedance controlled IO to connect to this kind of ADC,

    The FPGA on the Mojo is a low end cheapy - moving Gbytes of data per second takes a bit more than that.

     

    @Peter,

     

    The OP defined FAST - and at speeds of the order of 1GBbyte per second it's out of Arduino, Launchpad or Gizmo range.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 11 years ago in reply to michaelkellett

    He will need more than 1 board I admit!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to clem57

    It'll be worse than that - it isn't easy to pipe 1GHz LVDS from an ADC to an FPGA though any kind of connector. The connectors on the Mojo won't do it.

    Using multiple FPGAs to gain performance is usually only worth doing when you've run out of the performance you can get on one FPGA.

     

    A typical high speed data acquisition architecture would have the ADCs connected directly to the FPGA and as close to it as possible, the FPGA will need a buffer memory which could be 32 bit wide DDRAM. You need to budget for  a memory bandwidth about three times that of the ADCs if you want to stream and about 1.5x if you just want to capture and then read. So that's 750MHz data rate for streaming or a modest 400MHz for capture.

     

    To get the data out of the buffer you'll need an interface that can sustain 1Gbyte/s for streaming (10Gb Ethernet ?)  or less if you just need to read the data in non real time (USB3 ?).

     

    It's a difficult job - in my first post I didn't mention the scope/logic-analyser you would need to get this working - think £20k minimum, but more likely up to £50k.

     

    I'm planning a more modest system for  a client - 2 or 4 channels (not sure yet) 8bit, 50 - 100Msamples/sec, capture only, some real time processing on the FPGA, Gbit Ethernet control/data interface.

    It'll need a custom board, will use 64 bit data path to ram, probably a Lattice ECP3-70 FPGA but we will consider a switch to Xilinx.

     

    MK