Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Need help getting started
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 60 subscribers
  • Views 2324 views
  • Users 0 members are here
Related

Need help getting started

e14 Contributor
e14 Contributor over 11 years ago

I have built a small C# windows service application and need to build a small windows OS computer to run the application. The only requirements I need are Mic input, Audio output, Ethernet and I guess monitor, and usb ports for mouse and keyboard for setting up system. Once complete, no need for monitor, keyboard and mouse. The only other requirement I may need is to host a small web application to modify small configurations of the C# windows application.  This is not absolute. 

 

I am not sure what I really need to use or where to start. I can only assume the bare minimal, cost needs to be as low as possible.  Any help would be appreciated.

 

Thanks,
Shawn

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago +1
    You could look at the Brix Ultra Compact Celeron PC, SB0565041 from CPC (One of Farnell's alter egos). £79 but you need to add RAM, hard drive and OS - very neat and small but possibly no cheaper than…
Parents
  • xever
    0 xever over 11 years ago

    Shawn,

     

    Seems like you want to build an emergency response system-like commercial product that would act as a hands-free module, as what I can interpret from your requirements and the kits you have ordered.  And if so, as what MK has mentioned, the rPi was never designed to be used in such application, so I would be really cautious about using it as your platform.  Also, you have established that you are not that well-versed in Linux, makes it even difficult to sell the idea of a product that can be life or death critical when used.

     

    All the best,

     

    Christever

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to xever

    Thanks to everyone for their input, suggestions and help.  Well, I guess I am back to square one again.

    - Shawn

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to xever

    Thanks to everyone for their input, suggestions and help.  Well, I guess I am back to square one again.

    - Shawn

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • xever
    0 xever over 11 years ago in reply to e14 Contributor

    I don't think you are back to square one.  You can continue building the product, and can use the rPi to validate your software and application, this is your prototyping stage anyway.  However, what is being implied with the reply is that you should be cautious on deciding the final platform.  There are strict standards and regulations for such critical systems, and the product should be robust in all its aspects.  The rPi was built as an educational platform, and since you are at this stage, I think using it is not a bad starting point.  Just don't fall into the trap of prototypes ending as final products.

     

    Christever