Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Need help getting started
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 60 subscribers
  • Views 2313 views
  • Users 0 members are here
Related

Need help getting started

e14 Contributor
e14 Contributor over 11 years ago

I have built a small C# windows service application and need to build a small windows OS computer to run the application. The only requirements I need are Mic input, Audio output, Ethernet and I guess monitor, and usb ports for mouse and keyboard for setting up system. Once complete, no need for monitor, keyboard and mouse. The only other requirement I may need is to host a small web application to modify small configurations of the C# windows application.  This is not absolute. 

 

I am not sure what I really need to use or where to start. I can only assume the bare minimal, cost needs to be as low as possible.  Any help would be appreciated.

 

Thanks,
Shawn

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago +1
    You could look at the Brix Ultra Compact Celeron PC, SB0565041 from CPC (One of Farnell's alter egos). £79 but you need to add RAM, hard drive and OS - very neat and small but possibly no cheaper than…
Parents
  • clem57
    0 clem57 over 11 years ago

    tspatrick

         Sorry, but you do not start with the software and build the computer for it unless you are IBM or HP. Why not start with a Raspberry Pi 2 and install C# on Linux (Raspbian). Change your program to use Linux not Windows. Not knowing what your program does, cannot fill in details.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Ok, I must have not have communicated my message well enough. I'm NOT developing a new OS. I am writing a small C# windows based service application to run on some flavor of windows, either embedded or full version.  I was just looking for ideas on what type of hardware should I be looking for with the requirements that I needed.  I like writing software but not that much to write an entire OS.  Funny!   Hopefully that was clear enough.  Thanks for the input though.

     

    -Shawn

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Ok, I must have not have communicated my message well enough. I'm NOT developing a new OS. I am writing a small C# windows based service application to run on some flavor of windows, either embedded or full version.  I was just looking for ideas on what type of hardware should I be looking for with the requirements that I needed.  I like writing software but not that much to write an entire OS.  Funny!   Hopefully that was clear enough.  Thanks for the input though.

     

    -Shawn