Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Need help getting started
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 60 subscribers
  • Views 2313 views
  • Users 0 members are here
Related

Need help getting started

e14 Contributor
e14 Contributor over 11 years ago

I have built a small C# windows service application and need to build a small windows OS computer to run the application. The only requirements I need are Mic input, Audio output, Ethernet and I guess monitor, and usb ports for mouse and keyboard for setting up system. Once complete, no need for monitor, keyboard and mouse. The only other requirement I may need is to host a small web application to modify small configurations of the C# windows application.  This is not absolute. 

 

I am not sure what I really need to use or where to start. I can only assume the bare minimal, cost needs to be as low as possible.  Any help would be appreciated.

 

Thanks,
Shawn

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago +1
    You could look at the Brix Ultra Compact Celeron PC, SB0565041 from CPC (One of Farnell's alter egos). £79 but you need to add RAM, hard drive and OS - very neat and small but possibly no cheaper than…
Parents
  • DAB
    0 DAB over 11 years ago

    Hi Shawn,

     

    As I understand it, you are writing a C# program to run under windows.

     

    Before we can help you further, we need so background information on your project.

     

    I sounds like you want to do an embedded task that uses audio input and output, plus you want it to support Ethernet.

     

    What we need to understand is audio sampling rates, audio output quality, and how much data/speed over Ethernet.

     

    Do you need the embedded computer to run windows?

     

    Have you looked at Windows CE, which might support your needs.

     

    You might also want to look at the new Gizmo 2 board as an easy way to run your windows code.

     

    The more information you can provide enables us to give you better suggestions.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to DAB

    depending in the C# program, it may well happily run under MONO on Linux as mentioned above

     

    it is the application you need to run if I am understanding you correctly, it is not windows that is the critical factor here

     

    So you are looking for a vheap and chearful machine to run it on, if you really insist on windows then your pretty much looking for a second hand laptop or desktop machine or buying a microATX based board with an INTEL ATOM or something similar, all this is possibly way over kill for what you may need so, this is why Clem, Michael and DAB are suggesting alternatives

     

    the 30$ RPI 2 with C# for Linux installed may well do perfectly for what you trying to do

     

    Regards

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to DAB

    depending in the C# program, it may well happily run under MONO on Linux as mentioned above

     

    it is the application you need to run if I am understanding you correctly, it is not windows that is the critical factor here

     

    So you are looking for a vheap and chearful machine to run it on, if you really insist on windows then your pretty much looking for a second hand laptop or desktop machine or buying a microATX based board with an INTEL ATOM or something similar, all this is possibly way over kill for what you may need so, this is why Clem, Michael and DAB are suggesting alternatives

     

    the 30$ RPI 2 with C# for Linux installed may well do perfectly for what you trying to do

     

    Regards

     

    Peter