Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Is it possible to add more RAM?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 2 answers
  • Subscribers 64 subscribers
  • Views 4277 views
  • Users 0 members are here
Related

Is it possible to add more RAM?

Former Member
Former Member over 10 years ago

Looking to buy a relatively cheap SBC to set up as a server running a memory intensive application. Been looking at a bunch, but it seems most are limited to just 1gb of RAM. Ideally I'd like to have 4GB if not more. This is the reason for my question.

 

Any suggestions?

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago in reply to balearicdynamics +1
    balearicdynamics I just saw the video and the compute module is 512MB Ram and 4GB eMMC storage. Sorry to differ. Clem
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to clem57 +1
    Mmmhhh... It's true, and it's a detail I have not noted following the enthusiasm seeing the 4G 1600 DDR ... Sure that this can't be used as extra-memory ? But we don't know yet the details of the project…
  • crjeder
    crjeder over 10 years ago +1
    How about that little beauty? https://www.solid-run.com/product/cubox-i-4x4/
Parents
  • Former Member
    0 Former Member over 9 years ago

    E.g. my most heavily used frankenstein at home:

        - Assembled 2016-05-04

        - Mini-ITX enclosure: Thermaltake Cube V1

        - Biostar NM70I-1037U Mini-ITX motherboard

           * Intel Celeron Processor 1037U (Dual Core 1.8 GHz)

           * Intel HD Graphics 2500

           * Chipset NM70

        - RAM: 8GB DDR3

        - Graphics support auto-selected:

           * Kernel module - i915

           * Xorg video driver - intel

        - Permanent storage: SSD 120GB

        - RJ45 Ethernet: r8169 kernel module

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago

    E.g. my most heavily used frankenstein at home:

        - Assembled 2016-05-04

        - Mini-ITX enclosure: Thermaltake Cube V1

        - Biostar NM70I-1037U Mini-ITX motherboard

           * Intel Celeron Processor 1037U (Dual Core 1.8 GHz)

           * Intel HD Graphics 2500

           * Chipset NM70

        - RAM: 8GB DDR3

        - Graphics support auto-selected:

           * Kernel module - i915

           * Xorg video driver - intel

        - Permanent storage: SSD 120GB

        - RJ45 Ethernet: r8169 kernel module