Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Is it possible to add more RAM?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 2 answers
  • Subscribers 65 subscribers
  • Views 5265 views
  • Users 0 members are here
Related

Is it possible to add more RAM?

e14 Contributor
e14 Contributor over 11 years ago

Looking to buy a relatively cheap SBC to set up as a server running a memory intensive application. Been looking at a bunch, but it seems most are limited to just 1gb of RAM. Ideally I'd like to have 4GB if not more. This is the reason for my question.

 

Any suggestions?

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 11 years ago in reply to balearicdynamics +1
    balearicdynamics I just saw the video and the compute module is 512MB Ram and 4GB eMMC storage. Sorry to differ. Clem
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to clem57 +1
    Mmmhhh... It's true, and it's a detail I have not noted following the enthusiasm seeing the 4G 1600 DDR ... Sure that this can't be used as extra-memory ? But we don't know yet the details of the project…
  • crjeder
    crjeder over 11 years ago +1
    How about that little beauty? https://www.solid-run.com/product/cubox-i-4x4/
Parents
  • clem57
    0 clem57 over 11 years ago

    Got one with 2GB: Hardkernel Unveils $59 ODROID-U3 Board Powered by Exynos 4412 Prime Quad Core SoC

     

    Clem

    PS. All these have RAM built on the board. No chance to change.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    This seems promising, thank you for the find! I was also looking at the MarsBoard so I'm gonna have to pick b/w the two.

     

    As for the OS, I was hoping to run some flavour of Linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    This seems promising, thank you for the find! I was also looking at the MarsBoard so I'm gonna have to pick b/w the two.

     

    As for the OS, I was hoping to run some flavour of Linux.