Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Hello everyone! Tell me to choose a single board computer
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 61 subscribers
  • Views 1752 views
  • Users 0 members are here
  • Single Board Computer
Related

Hello everyone! Tell me to choose a single board computer

ealltech
ealltech over 10 years ago

Local government increases electricity charges so i have to shift to low power computer solution. My requirements are very simple. I currently use my computer to Browse web (Google chrome) including watching online videos (flash) etc Download torrents (ktorrent) And watch movies (vlc player)

  1. VGA output
  2. Sub woofer need 3.5 mm output
  3. Ps/2 keyboard and mouse
  4. 1 Ghz or more processor and 1 GB DDR3

If you know a device which fulfills above please put the link below Thank-you!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to ealltech +1
    For PS/2 devices, you'll need a USB adapter. If you live in the Dallas Fort Worth Texas USA area, you can come buy and I'll give you one that I do not use anymore. On the other hand, they are not expensive…
Parents
  • e14 Contributor
    e14 Contributor over 9 years ago

    Mini-ITX boards are a step up in price from SoCs like RPi & BB but offer more expandability and flexibility.  For example, one of my home-built PCs is using a Biostar motherboard NM70I-1037U with a built-in dual-core Celeron @ 1.8GHz.  Fast enough for me as a developer.  The total price including an SSD disk, Thermaltake cube case (splurged on this), power supply, keyboard, and mouse was $300.  The Linux distribution was legally-free, donation-ware (Ubuntu MATE).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 9 years ago

    Mini-ITX boards are a step up in price from SoCs like RPi & BB but offer more expandability and flexibility.  For example, one of my home-built PCs is using a Biostar motherboard NM70I-1037U with a built-in dual-core Celeron @ 1.8GHz.  Fast enough for me as a developer.  The total price including an SSD disk, Thermaltake cube case (splurged on this), power supply, keyboard, and mouse was $300.  The Linux distribution was legally-free, donation-ware (Ubuntu MATE).