Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Switch ONLY when powered off
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 61 subscribers
  • Views 1250 views
  • Users 0 members are here
Related

Switch ONLY when powered off

atmn
atmn over 9 years ago

Hi!

 

I wonder if there are any curcuits that allow me to only switch when device is powered off.

 

I select between 2 chips with their 5V pin and I want to prevent to be able to "hot swap". If I would toggle the switch when power on it will stay on the state it was when the system was powered on.

 

Is there any solution, any chip I could use?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 9 years ago in reply to atmn +6
    This is a quick example that doesn't need any chips... Q1 and Q3 are P channel FETs like BSS84, Q2 and Q4 are N channel FETs like BSS138. With the switch in the capacitor position, Q2 will turn on Q1 and…
  • dougw
    dougw over 9 years ago +2
    You could use an DPST switch to select which chip gets power on power-up. The DPST switch state gets latched on power-up by a D-flip-flop. The D-flip-flop clock can be a simple capacitor to the power rail…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1
    OK, so a slightly more complicated approach would be to use a very low cost microcontroller (ATTiny or similar), have two power transistors, one for each unit and a button. When you press the button, the…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    OK, so a slightly more complicated approach would be to use a very low cost microcontroller (ATTiny or similar), have two power transistors, one for each unit and a button. When you press the button, the micro will power off the first device, wait a period of time, then power on the other. this approach can be applied to more than two devies in this case.

     

    Yes you can do it with simple ttl chips and passives but it will take just as long and less fun. A clunky switch will give no time for one to power off before the other starts powering up. You could also include a GPIO signal to the target device to tell it to go to sleep or some other pre-defined condition prior to the power being removed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    OK, so a slightly more complicated approach would be to use a very low cost microcontroller (ATTiny or similar), have two power transistors, one for each unit and a button. When you press the button, the micro will power off the first device, wait a period of time, then power on the other. this approach can be applied to more than two devies in this case.

     

    Yes you can do it with simple ttl chips and passives but it will take just as long and less fun. A clunky switch will give no time for one to power off before the other starts powering up. You could also include a GPIO signal to the target device to tell it to go to sleep or some other pre-defined condition prior to the power being removed.