Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Suggestion to send sensor data to internet cloud in remote location
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 58 subscribers
  • Views 1959 views
  • Users 0 members are here
  • cloud computing
  • vibration sensor
  • sensor
Related

Suggestion to send sensor data to internet cloud in remote location

lukegar56
lukegar56 over 8 years ago

Hello, there are some machinery system in color chemical firms  which uses high power motor and to know the health status of these machines I am thinking to use some new IOT friendly device name wireless vibration sensor interface with raspberry pi to connect it with Amazon cloud but the industry is at a remote location and we are not able to use the internet here, so looking for best way to send the data of sensor to cloud without any issue.  Any suggestion makes this process happen will be very helpful.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +1
    Hi Garry, If you're using that sensor/transmitter then it needs a receiver too, plugged into something that can upload to the cloud, and that same manufacturer offers a USB device for that according to…
  • Jan Cumps
    Jan Cumps over 8 years ago +1
    I've used SigFox for such scenarios. Including the Amazon Cloud integration. Check if it has coverage for your area: https://www.sigfox.com/en/coverage
  • lukegar56
    lukegar56 over 8 years ago +1
    Hey, shabaz Thanks for the reply, actually I have the transmitter as well as the receiver but interfacing it with Raspberry Pi model 3B I am searching out for some sample codes to make it connected and…
Parents
  • lukegar56
    lukegar56 over 8 years ago

    Hey,

    shabaz Thanks for the reply, actually I have the transmitter as well as the receiver but interfacing it with Raspberry Pi model 3B I am searching out for some sample codes to make it connected and send the readings of the sensor to  cloud using inbuilt wifi, any suggestion for that will be good.

     

    And Jan Cumps is it possible to connect these kinds of the sensor directly with Sigfox seems great idea but need to more about it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to lukegar56

    With the WiFi, you can connect to a local WiFi point. That point then needs to have access to the internet. Connecting a Raspberry Pi directly to the internet is not possible.

     

    For sigfox, chech the link that I provided above. If the remote area you’re going to place the device is covered by sigfox, you can use that. Else there’s no point to choose that solution.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to lukegar56

    With the WiFi, you can connect to a local WiFi point. That point then needs to have access to the internet. Connecting a Raspberry Pi directly to the internet is not possible.

     

    For sigfox, chech the link that I provided above. If the remote area you’re going to place the device is covered by sigfox, you can use that. Else there’s no point to choose that solution.