Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Sensing Skin is present
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 62 subscribers
  • Views 1936 views
  • Users 0 members are here
Related

Sensing Skin is present

hasher
hasher over 8 years ago

Hi guys

 

I am working on a project that  involves detection of skin (and hair). The sensor should be in such a way that it should differentiate human skin from other objects like wood,dirt . Is there a commercial sensor on the market that does this ?

 

 

Thanks Paul

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago in reply to hasher +4
    You should be able to combine with detecting a change in the relative chest position. Either tilt switch or accelerometer to detect both the accelration vertically and then the change in it's position…
  • hasher
    hasher over 8 years ago in reply to Fred27 +3
    Well I want to know when two animals push against each other to trigger a data point. So the sensor is mounted on the animals chest and I want to know when they mate. Obviously there is a lot hair in the…
  • Fred27
    Fred27 over 8 years ago in reply to hasher +3
    I think that would work, although there is still the chance of false positives. There are plenty of microcontrollers that do capacitive sensing - you won't even need something as powerful as a SBC. I'm…
Parents
  • genebren
    genebren over 8 years ago

    Capacitive sensing is a good way to go.  I have used multiple capactive sensors in an array to detect proper (full) contact with skin in a medical product.  The idea was to require multiple contact points to verify a verified contact.  If the fur does get in the way (which should not be too much of a problem), you could augment the detection with an I/R sensor to provide an added component of heat to the equation to assist in eliminating false/casual contact.

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 8 years ago

    Capacitive sensing is a good way to go.  I have used multiple capactive sensors in an array to detect proper (full) contact with skin in a medical product.  The idea was to require multiple contact points to verify a verified contact.  If the fur does get in the way (which should not be too much of a problem), you could augment the detection with an I/R sensor to provide an added component of heat to the equation to assist in eliminating false/casual contact.

     

    Gene