Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Sensing Skin is present
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 62 subscribers
  • Views 1936 views
  • Users 0 members are here
Related

Sensing Skin is present

hasher
hasher over 8 years ago

Hi guys

 

I am working on a project that  involves detection of skin (and hair). The sensor should be in such a way that it should differentiate human skin from other objects like wood,dirt . Is there a commercial sensor on the market that does this ?

 

 

Thanks Paul

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago in reply to hasher +4
    You should be able to combine with detecting a change in the relative chest position. Either tilt switch or accelerometer to detect both the accelration vertically and then the change in it's position…
  • hasher
    hasher over 8 years ago in reply to Fred27 +3
    Well I want to know when two animals push against each other to trigger a data point. So the sensor is mounted on the animals chest and I want to know when they mate. Obviously there is a lot hair in the…
  • Fred27
    Fred27 over 8 years ago in reply to hasher +3
    I think that would work, although there is still the chance of false positives. There are plenty of microcontrollers that do capacitive sensing - you won't even need something as powerful as a SBC. I'm…
Parents
  • Fred27
    Fred27 over 8 years ago

    The standard way of detecting touch as capacitive sensing. This doesn't specifically discriminate between skin and other objects, but there are ways to ignore non-specific contact - e.g. a whole hand or water/dirt over a panel of buttons. Does this meet your needs? You may need to be a bit more specific about what you're trying to achieve.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • hasher
    hasher over 8 years ago in reply to Fred27

    Well  I want to know when two animals push against each other to trigger a data point. So the sensor is mounted on the animals chest and I want to know when they mate. Obviously there is a lot hair in the way. Think of a cow or a horse. If it was a pressure sensor it might trigger whilst laying on the ground or rubbing against something.

     

    I can only mount my sensor on the male . Not both animals

     

    Even a combination of pressure and skin detection might reduce error. Plus I don't know if skin detection will work with so much hair.

     

    I know this is quirky but has application in farming

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 8 years ago in reply to hasher

    I think that would work, although there is still the chance of false positives. There are plenty of microcontrollers that do capacitive sensing - you won't even need something as powerful as a SBC. I'm familiar with TI's MSP430 range and there was even a project14 episode on using a MSP430FR2633 dev board as a proximity sensor.

     

    Episode 356: Bank to the Future with Arduino & TI

    hasher  wrote:

    I know this is quirky but has application in farming

    I'm glad you cleared that up! Otherwise it would have just been weird.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • hasher
    hasher over 8 years ago in reply to Fred27

    Thanks David

     

    I will check out the youtube video !! Maybe have questions after that.

     

     

    Fred27  wrote:

    I'm glad you cleared that up! Otherwise it would have just been weird.

    Haha yeah I added it as it was getting weird image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to hasher

    You should be able to combine with detecting a change in the relative chest position.

    Either tilt switch or accelerometer to detect both the accelration vertically and then the change in it's position for a period of time.

     

    Here they simply use different coloured marker bags ... image

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 8 years ago in reply to hasher

    You should be able to combine with detecting a change in the relative chest position.

    Either tilt switch or accelerometer to detect both the accelration vertically and then the change in it's position for a period of time.

     

    Here they simply use different coloured marker bags ... image

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down